6.1. TI Apps Launcher - User Guide¶
6.1.1. Overview¶
TI Apps Launcher is a QT Based Application launcher for TI Platforms. Currently, TI Apps Launcher incorparates following applications,
Industrial HMI
Live Camera
ARM Analytics
Benchmarks
GPU Performance
Seva Store
Firefox
3D Demo
Settings
All of the necessary equipment requirement and instructions are provided here.
Note
Not all of the above set of applications are supported by each platform. So there will be differences between each.
6.1.2. Hardware Prerequisites¶
TI AM62x SK / TI AM62x-LP SK / TI AM62xSIP SK
PC (Windows or Linux, to use serial terminal console)
HDMI Monitor (to view the Demo on Display)
Ethernet Cable (to connect AM62x SK to internet)
USB Camera or OV5640 camera sensor module (for Live Camera)
Keyboard & Mouse (to control the TI Apps Launcher)
SD card (minimum 16GB)
6.1.3. Launching and Using the TI Apps Launcher¶
The TI Apps Launcher launches on Linux startup. Follow the below instructions to use it.
Flash an SD card with tisdk-default-image-am62xx-evm.wic.xz. User can download the tisdk-default-image-am62xx-evm.wic.xz image from here. Please follow the instructions from here to Flash an SD card.
Note
Images may vary between each platform based on the number of supported applications.
Insert the flashed SD card to the board, connect the display, mouse, ethernet cable, keyboard and power on the TI AM62x SK. The TI Apps Launcher will launch automatically when the device is fully booted.
6.1.3.1. Launching the Industrial HMI¶
Note
Industrial HMI on AM62xSIP SK varies from the one documented here. This is only valid for AM62x SK and AM62x-LP SK.
To launch the Industrial HMI demo, click on the Industrial HMI button on the left panel.
Note
It takes around 3-5 seconds for Industrial HMI to start.
By default, the Industrial HMI demo starts in Auto mode as shown below.
You can click on the Auto-Manual slider button to switch modes.
In Manual mode, you can use the ^ and v buttons of each motor to control the RPM.
6.1.3.2. Launching the Live Camera¶
Ensure you have enabled the camera sensors which you have connected to TI AM62x SK. Refer this to know the list of camera modules supported and how to enable the sensor overlays for them.
To launch the Live Camera demo, click on the Live Camera button on the left panel.
Note
It takes around 3-5 seconds for Live Camera to start.
The Live Camera demo starts streaming the output of the camera connected in the centre window of TI Apps Launcher. The image below is captured using USB Camera.
6.1.3.3. Launching the ARM Analytics Demo¶
Note
ARM Analytics Demo is only supported on AM62x SK and AM62x-LP SK. AM62xSIP doesn’t support it.
AM62x SDK now supports ARM Analytics with pre-existing demos showcasing Object Detection, Face Detection and Image Classification.
To launch the ARM Analytics demo, click on the ARM Analytics button on the left panel.
By default, the ARM Analytics demo shows the results of Object Detection Model on existing data.
Click on the Face Detection button to check the results of Face Detection Model on existing data.
Click on the Image Classification button to check the results of Image Classification Model on existing data.
6.1.3.4. Launching the Benchmarks Demo¶
Note
Benchmarks Demo is not supported on AM62xSIP because it depends on weston-terminal. AM62xSIP uses EGLFS to run the ti-apps-launcher.
The Benchmarks Demo includes various System Benchmarks like dhrystone, linpack, nbench, etc. and GPU benchmarks like glmark2.
Click on the Benchmarks button on the left panel.
User will now see the list of Benchmarks available to test on TI AM62x. Click on the play button infront of the benchmark you like to test. The image below is captured while running the glmark2.
You will see the updated values of FPS & Score metrices getting populated.
6.1.3.5. Launching the GPU Performance Demo¶
Note
GPU Performance Demo is not supported on AM62xSIP because it depends on weston or requires the ownership of EGLFS context.
The GPU Performance demo allows users to vary the GPU loads using glmark2. Click on the GPU Performance button on the left panel.
Now you can vary the GPU Loads by clicking on the various numbers you see on GPU Load Levels Bar.
The image below is captured while running the glmark2 with GPU Load Level as 1.
You will see the updated values of FPS & Score metrices getting populated.
6.1.3.6. Launching the Seva Store¶
Note
Seva Store is not supported on AM62xSIP due to it’s memory constraints.
AM62x SDK now supports Seva Store. Seva Store is TI developed Demo Gallery Tool which allows users to Download and Install demos on the go. Developers can host their Demos as Docker Images on any public Docker Registry and link them to Seva Design Gallery. Refer Seva Store - User Guide to know more about Seva Store.
6.1.3.7. Launching the Firefox Browser¶
Note
Firefox Browser is not supported on AM62xSIP due to it’s memory constraints.
AM62x SDK now supports Firefox ESR Browser. Click on the Firefox button on the left panel.
Click Launch button to launch the Firefox Browser. The Browser launches with TI Arm-based processors page as the first tab by default.
Note
It takes approximately 10-12 seconds for Firefox ESR browser to launch.
Click x to close the Firefox Browser.
6.1.3.8. Launching the 3D Demo¶
Note
3D Demo requires weston to be running or EGLFS context to run. ti-apps-launcher is run on EGLFS so it is not supported on AM62xSIP.
Click on the 3D Demo button on the left panel.
Click Launch button to launch the 3D Demo by Imagination. By default, you would see the Skinning Model running on the screen.
You can use mouse buttons or spacebar to pause the 3D Demo and press ESC to exit & go back to TI Apps Launcher.
6.1.4. Building the TI Apps Launcher¶
The TI Apps Launcher is enabled by default in yocto for AM62x Linux and RT-Linux.
The source code is available at TI Apps Launcher and can be re-compiled with the following steps
To setup the environment, from the root of the SDK installation directory, source environment-setup script.
$ source linux-devkit/environment-setup
Go to the root of TI Apps Launcher repository and run the following command to build the application.
$ qmake "SOURCES += configs/am62xx-evm.cpp" "DEFINES += SOC_AM62"; make # For AM62x SK $ qmake "SOURCES += configs/am62xx-lp-evm.cpp" "DEFINES += SOC_AM62_LP"; make # For AM62x LP SK $ qmake "SOURCES += configs/am62xxsip-evm.cpp" "DEFINES += SOC_AM62_LP"; make # For AM62xSIP SK
Copy the compiled binary to /usr/bin directory of the device
$ scp ti-apps-launcher root@<ip-addr-of-device>:/usr/bin/
If you have modified the scripts under the ti-apps-launcher scripts directory then copy the same to the device
$ scp -r scripts/ root@<ip-addr-of-device>:/opt/ti-apps-launcher/