2.3. Migration Guide¶
Overview
This page covers migration information for applications built on top of the Processor SDK Linux AM62X.
2.3.1. Processor SDK Linux AM62X 08.xx Releases¶
2.3.1.1. Processor SDK Sitara 08.06¶
- This is the fourth release of Processor SDK Linux AM62X on 2021 LTS 5.10 kernel, 2021.01 U-Boot
- ATF 2.8+
- OPTEE 3.20
- Yocto Dunfell/3.1
- Platforms Supported : AM62x (GP, HS-FS, HS-SE) with default boot on HS-FS
2.3.1.2. Processor SDK 08.05¶
- This is the third release of Processor SDK Linux AM62X on 2021 LTS 5.10 kernel, 2021.01 U-Boot
- ATF 2.7+
- OPTEE 3.19+
- Yocto Dunfell/3.1
- Platforms Supported : AM62x
2.3.1.3. Processor SDK 08.04¶
- This is the second release of Processor SDK Linux AM62X on 2021 LTS 5.10 kernel, 2021.01 U-Boot
- ATF 2.7
- OPTEE 3.18
- Yocto Dunfell/3.1
- Platforms Supported : AM62x
2.3.1.4. Processor SDK 08.03¶
- This is the first release of Processor SDK Linux AM62X.
2.3.2. AM62 SD UHS Speed modes Enable¶
In 08.03 release, SD card enumeration failures were observed on a few U1 class of SD cards. These include but not limited to,
- Microcenter U1 class cards
- Kingston U1 class cards
- HP U1 class cards
A conservative approach was taken to disable UHS modes by default, and support wide range of SD cards. However if required they can be enabled by using the following steps,
Yocto build Flow
Revert the following commits, from meta-processor-sdk layer
Cleaning up U-Boot and Kernel repos
$MACHINE=am62x-evm bitbake -f linux-ti-staging-c do_cleansstate $MACHINE=am62x-evm bitbake -f u-boot-ti-staging -c do_cleansstateRebuild the wic image
$MACHINE=am62x-evm bitbake -f tisdk-default-imageBuilding from source tree
Run the following commands in respective src tree directories to revert UHS disable patches.
<SDK_INSTALL_PATH>/board-support/linux-5.10.109+gitAUTOINC+9e58028f94-g9e58028f94
patch -p1 -R < patches/0001-arm64-dts-ti-k3-am62-main-Disable-UHS-speed-modes-on.patch<SDK_INSTALL_PATH>/board-support/u-boot-2021.01+gitAUTOINC+74fc69c889-g74fc69c889
patch -p1 -R < patches/0001-Revert-arm-dts-k3-am625-sk-u-boot-Add-u-boot-tag-to-.patch patch -p1 -R < patches/0002-Revert-configs-am62x_evm_a53_defconfig-Enable-config.patchRecompile dtb
make linux-dtbsRecompile the kernel Image
make linuxRecompile the bootloaders
make u-boot