3.7.1. Introduction¶
AM62x device is enabled with 3D graphics accelerator based on the A-Series AXE-1-16M from Imagination Technologies Inc. It enables the support of 3D graphics rendering using OpenGL® ES API’s. The OpenGL® ES API’s up to and including version 3.1 with render surfaces upto 4k and input textures upto 8k sizes are supported by the hardware.
The following extensions are supported:
| EGL_EXT_client_extensions |
| EGL_EXT_device_base |
| EGL_EXT_device_enumeration |
| EGL_EXT_device_query |
| EGL_EXT_platform_base |
| EGL_KHR_client_get_all_proc_addresses |
| EGL_KHR_debug EGL_EXT_platform_device |
| EGL_EXT_platform_wayland |
| EGL_KHR_platform_wayland |
| EGL_MESA_platform_gbm |
| EGL_KHR_platform_gbm |
| EGL_MESA_platform_surfaceless |
| EGL_ANDROID_native_fence_sync |
| EGL_EXT_buffer_age |
| EGL_EXT_create_context_robustness |
| EGL_EXT_image_dma_buf_import |
| EGL_EXT_image_dma_buf_import_modifiers |
| EGL_EXT_image_gl_colorspace |
| EGL_EXT_swap_buffers_with_damage |
| EGL_EXT_yuv_surface |
| EGL_IMG_context_priority |
| EGL_KHR_cl_event2 |
| EGL_KHR_config_attribs |
| EGL_KHR_create_context |
| EGL_KHR_fence_sync |
| EGL_KHR_get_all_proc_addresses |
| EGL_KHR_gl_colorspace |
| EGL_KHR_gl_renderbuffer_image |
| EGL_KHR_gl_texture_2D_image |
| EGL_KHR_gl_texture_3D_image |
| EGL_KHR_gl_texture_cubemap_image |
| EGL_KHR_image_base |
| EGL_KHR_no_config_context |
| EGL_KHR_partial_update |
| EGL_KHR_reusable_sync |
| EGL_KHR_surfaceless_context |
| EGL_KHR_swap_buffers_with_damage |
| EGL_EXT_pixel_format_float |
| EGL_KHR_wait_sync |
| EGL_MESA_configless_context |
| EGL_MESA_drm_image |
| EGL_MESA_image_dma_buf_export |
| EGL_WL_bind_wayland_display |
| EGL_WL_create_wayland_buffer_from_image |
| EGL_IMG_cl_image |
| GL_APPLE_texture_format_BGRA8888 |
| GL_EXT_blend_minmax |
| GL_EXT_buffer_storage |
| GL_EXT_clip_control |
| GL_EXT_color_buffer_float |
| GL_EXT_color_buffer_half_float |
| GL_EXT_compressed_ETC1_RGB8_sub_texture |
| GL_EXT_conservative_depth |
| GL_EXT_copy_image |
| GL_EXT_discard_framebuffer |
| GL_EXT_draw_buffers |
| GL_EXT_draw_buffers_indexed |
| GL_EXT_draw_elements_base_vertex |
| GL_EXT_EGL_image_array |
| GL_EXT_float_blend |
| GL_EXT_gpu_shader5 |
| GL_EXT_memory_object |
| GL_EXT_memory_object_fd |
| GL_EXT_multi_draw_arrays |
| GL_EXT_multisampled_render_to_texture |
| GL_EXT_multisampled_render_to_texture2 |
| GL_EXT_occlusion_query_boolean |
| GL_EXT_polygon_offset_clamp |
| GL_EXT_read_format_bgra |
| GL_EXT_robustness |
| GL_EXT_separate_shader_objects |
| GL_EXT_shader_framebuffer_fetch |
| GL_EXT_shader_group_vote |
| GL_EXT_shader_implicit_conversions |
| GL_EXT_shader_io_blocks |
| GL_EXT_shader_non_constant_global_initializers |
| GL_EXT_shader_pixel_local_storage |
| GL_EXT_shader_pixel_local_storage2 |
| GL_EXT_shader_texture_lod |
| GL_EXT_shadow_samplers |
| GL_EXT_sparse_texture |
| GL_EXT_sRGB_write_control |
| GL_EXT_texture_border_clamp |
| GL_EXT_texture_buffer |
| GL_EXT_texture_cube_map_array |
| GL_EXT_texture_format_BGRA8888 |
| GL_EXT_texture_format_sRGB_override |
| GL_EXT_texture_rg |
| GL_EXT_texture_shadow_lod |
| GL_EXT_texture_sRGB_decode |
| GL_EXT_texture_sRGB_R8 |
| GL_EXT_texture_sRGB_RG8 |
| GL_EXT_YUV_target |
| GL_IMG_framebuffer_downsample |
| GL_IMG_multisampled_render_to_texture |
| GL_IMG_program_binary |
| GL_IMG_read_format |
| GL_IMG_shader_binary |
| GL_IMG_texture_format_BGRA8888 |
| GL_IMG_texture_npot |
| GL_KHR_blend_equation_advanced |
| GL_KHR_blend_equation_advanced_coherent |
| GL_KHR_debug |
| GL_KHR_robustness |
| GL_OES_compressed_ETC1_RGB8_texture |
| GL_OES_depth24 |
| GL_OES_depth_texture |
| GL_OES_draw_buffers_indexed |
| GL_OES_draw_elements_base_vertex |
| GL_OES_EGL_image |
| GL_OES_EGL_image_external |
| GL_OES_EGL_image_external_essl3 |
| GL_OES_EGL_sync |
| GL_OES_element_index_uint |
| GL_OES_fragment_precision_high |
| GL_OES_get_program_binary |
| GL_OES_gpu_shader5 |
| GL_OES_mapbuffer |
| GL_OES_packed_depth_stencil |
| GL_OES_required_internalformat |
| GL_OES_rgb8_rgba8 |
| GL_OES_sample_shading |
| GL_OES_sample_variables |
| GL_OES_shader_image_atomic |
| GL_OES_shader_io_blocks |
| GL_OES_shader_multisample_interpolation |
| GL_OES_standard_derivatives |
| GL_OES_surfaceless_context |
| GL_OES_texture_border_clamp |
| GL_OES_texture_buffer |
| GL_OES_texture_cube_map_array |
| GL_OES_texture_float |
| GL_OES_texture_half_float |
| GL_OES_texture_npot |
| GL_OES_texture_stencil8 |
| GL_OES_texture_storage_multisample_2d_array |
| GL_OES_vertex_array_object |
| GL_OES_vertex_half_float |
For more information about the supported OpenGL® ES and EGL® extensions see:
- https://docs.imgtec.com/reference-manuals/open-gl-es-extensions/topics/overview.html
- https://registry.khronos.org/OpenGL/
Note
OpenCL® libraries are currently provided without support at https://git.ti.com
The OpenGL® ES and EGL® libraries are packaged with the Processor SDK Linux AM62x and are used by graphics stacks such as Wayland/Weston. The drivers run on an ARM core and programs the firmware running inside a GPU core with rendering commands submitted by the user applications.
Support for up to 2Kx2K render surfaces.
The rest of this page will cover the following topics:
- Software architecture of Graphics
- Instructions on how to run graphics demos
- Instructions on how to run DSS application
- Instructions on how launch Weston
- Instructions on how to run PVR tools
3.7.2. Software Architecture¶
The picture below shows the software architecture of Graphics in Processor SDK Linux AM62x.
Fig. 3.4 PSDK Linux Rogue Graphics Software Stack
Please note that RGX-KM in this context refers to the pvrsrvkm kernel module, which is currently provided at: https://git.ti.com/cgit/graphics/ti-img-rogue-driver
This is included by default in the SDK. The kernel module is located at:
target # /lib/modules/$(uname -r)/extra/pvrsrvkm.ko
It is loaded automatically by the rc.pvr init script in /etc/init.d/ .
3.7.3. Graphics Demos¶
Along with the graphics driver and userspace libraries, the SDK also includes example applications. Some of the demos are based on the IMG Native_SDK examples.
The following demos are available to run under the Wayland windowing system.
target # /usr/bin/SGX/demos/Wayland/OpenGLESDeferredShading
target # /usr/bin/SGX/demos/Wayland/OpenGLESGaussianBlur
target # /usr/bin/SGX/demos/Wayland/OpenGLESImageBasedLighting
target # /usr/bin/SGX/demos/Wayland/OpenGLESIntroducingPVRCamera
target # /usr/bin/SGX/demos/Wayland/OpenGLESIntroducingPVRUtils
target # /usr/bin/SGX/demos/Wayland/OpenGLESIntroducingUIRenderer
target # /usr/bin/SGX/demos/Wayland/OpenGLESNavigation2D
target # /usr/bin/SGX/demos/Wayland/OpenGLESNavigation3D
target # /usr/bin/SGX/demos/Wayland/OpenGLESParticleSystem
Additionally demos using the Null Window System / KMS / DRM / EGLFS are provided with Qt. By default EGLFS will use the eglfs_kms backend.
target # /usr/share/qt5/examples/opengl/hellogles3/hellogles3 -platform eglfs
target # /usr/share/qt5/examples/opengl/2dpainting/2dpainting -platform eglfs
target # /usr/share/qt5/examples/opengl/paintedwindow/paintedwindow -platform eglfs
The default eglfs_kms configuration file for Qt5 is located at:
target # /etc/qt5/eglfs_kms_cfg.json
For more information about Qt’s EGLFS and using Qt5 in embedded applications see:
3.7.4. Display¶
TI SoC’s are equipped with Display SubSystem (DSS) hardware to provide hardware
acceleration for alpha blending of overlays and color conversion. The DSS
hardware is exposed to the software drm API available through libdrm module.
Through this drm interface, a user space program can perform mode setting of
the display.
The drm module models the display hardware as a series of abstract hardware blocks and manages them through the API. The blocks are:
- CRTC[1]: represents a scanout engine that generates video timing signal from the data pointed to by the scanout buffer
- Connector: represents where the video timing signal is sent across to the display
- Encoder: transforms the video timing signal from CRTC to a format that is suitable for sending across the connector
- Plane: represents the overlay buffer that a CRTC can be fed with
A utility application modetest can be used to get the list of available drm
blocks. All the information available for the device can be displayed by using
it.
3.7.4.1. Finding Connector ID¶
Run the below modetest command:
Look for the display device for which the connector ID is required - such as HDMI, LCD etc.
Connectors:
id encoder status type size (mm) modes encoders
4 3 connected HDMI-A 480x270 20 3
modes:
name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
1920x1080 60 1920 2008 2052 2200 1080 1084 1089 1125 flags: phsync, pvsync; type: preferred, driver
...
16 15 connected unknown 0x0 1 15
modes:
name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
800x480 60 800 1010 1040 1056 480 502 515 525 flags: nhsync, nvsync; type: preferred, driver
The modes displayed are the various resolutions supported by the connected display.
3.7.4.2. Finding Plane ID¶
To find the Plane ID, run the modetest command:
which should show something like below:
Planes:
id crtc fb CRTC x,y x,y gamma size
19 0 0 0,0 0,0 0
formats: RG16 RX12 XR12 RA12 AR12 XR15 AR15 RG24 RX24 XR24 RA24 AR24 NV12 YUYV UYVY
props:
...
20 0 0 0,0 0,0 0
formats: RG16 RX12 XR12 RA12 AR12 XR15 AR15 RG24 RX24 XR24 RA24 AR24 NV12 YUYV UYVY
props:
...
3.7.5. Wayland/Weston¶
The supported Wayland/Weston version brings in the multiple display support in extended desktop mode and the ability to drag-and-drop windows from one display to the other.
To launch Weston, do the following:
On the target console:
target # unset WAYLAND_DISPLAY
On the default display:
target # weston --tty=1 --display=<default connector-id>
On the secondary display:
target # weston --tty=1 --display=<secondary connector-id>
On all connected displays (LCD and HDMI):
target # weston --tty=1
By default, the screensaver timeout is configured to 300 seconds. The user can change the screensaver timeout using a command line option:
--idle-time=<number of seconds>
For example, to set timeout of 10 minutes and Weston configured to display on all connectors, use the below command:
weston --tty=1 --idle-time=600
To disable the screen timeout and to configure Weston to display on all connectors, use the below command:
weston --tty=1 --idle-time=0
If you face any issues with the above procedure, please refer GLSDK_FAQs#Unable_to_run_Weston_on_the_GLSDK_release for troubling shooting tips.
The filesystem comes with a preconfigured weston.ini file which will be located in
/etc/weston.ini
3.7.5.1. Running Weston clients¶
# /usr/bin/weston-flower
# /usr/bin/weston-clickdot
# /usr/bin/weston-cliptest
# /usr/bin/weston-dnd
# /usr/bin/weston-editor
# /usr/bin/weston-eventdemo
# /usr/bin/weston-image /usr/share/weston/terminal.png
# /usr/bin/weston-resizor
# /usr/bin/weston-simple-egl
# /usr/bin/weston-simple-shm
# /usr/bin/weston-simple-touch
# /usr/bin/weston-smoke
# /usr/bin/weston-info
# /usr/bin/weston-terminal
3.7.5.2. Running multimedia with Wayland sink¶
The GStreamer video sink for Wayland is the waylandsink. To use this video-sink for video playback:
target # gst-launch-1.0 playbin uri=file://<path-to-file-name> video-sink=waylandsink
3.7.5.3. Exiting Weston¶
Terminate all Weston clients before exiting Weston. If you have invoked Weston from the serial console, exit Weston by pressing Ctrl-C.
If Weston was started automatically by the init system then it can be stopped with:
target # /etc/init.d/weston stop
It is also possible to invoke Weston from the native console, exit Weston by pressing Ctrl-Alt-Backspace.
3.7.5.4. Using IVI shell feature¶
The SDK also has support for configuring Weston ivi-shell. The default shell that is configured in the SDK is the desktop-shell.
To change the shell to ivi-shell, the user will have to add the following lines into the /etc/weston.ini.
To switch back to the desktop-shell can be done by commenting these lines in the /etc/weston.ini (comments begin with a ‘#’ at the start of line).
[core]
shell=ivi-shell.so
After the above configuration is completed, we can restart Weston by running the following commands
target# /etc/init.d/weston stop
target# /etc/init.d/weston start
Note
When Weston starts with ivi-shell, the default background is black, this is different from the desktop-shell that brings up a window with background.
With ivi-shell configured for Weston, Wayland client applications use ivi-application protocol to be managed by a central HMI window management.
Applications must support the ivi_application Wayland protocol to be managed by the HMI central controller with an unique numeric ID.
Some important references to Weston IVI-shell can be found at the following link:
3.7.5.4.1. Running QT applications with IVI shell¶
To run the QT application with ivi-shell, set the QT_WAYLAND_SHELL_INTEGRATION environment variable to ivi-shell.
export QT\_WAYLAND\_SHELL\_INTEGRATION=ivi-shell
3.7.6. Using the PowerVR Tools¶
The suite of PowerVR Tools is designed to enable rapid graphics application development. It targets a range of areas including asset exporting and optimization, PC emulation, prototyping environments, on-line and off-line performance analysis tools and many more. Please refer to PowerVR-SDK for additional details on the tools and detailed documentation.
The target file system includes a subset of PowerVR tools such as PVRScope and PVRTrace recorder libraries from Imagination PowerVR SDK to profile and trace GFX activities. In addition, it also includes PVRPerfServerDeveloper tool.
Note
If you are experiencing issues with any of the tools try updating to the latest provided by Imagination at https://developer.imaginationtech.com/
3.7.6.1. PVRTune¶
The PVRTune utility is a real-time GPU performance analysis tool. It captures hardware timing data and counters which facilitate the identification of performance bottlenecks. PVRPerfServerDeveloper should be used along with the PVRTune running on the PC to gather data on the SGX loading and activity threads. You can invoke the tool with the below command:
target # /opt/img-powervr-sdk/PVRHub/PVRPerfServer/PVRPerfServerDeveloper
3.7.6.2. PVRTrace¶
The PVRTrace is an OpenGL® ES API recording and analysis utility. PVRTrace GUI provides off-line tools to inspect captured data, identify redundant calls, highlight costly shaders and many more. The default filesystem contains helper scripts to obtain the PVRTrace of the graphics application. This trace can then be played back on the PC using the PVRTrace Utility.
To start tracing, use the below commands as reference:
target # cp /opt/img-powervr-sdk/PVRHub/Scripts/start_tracing.sh ~/.
target # ./start_tracing.sh <log-filename> <application-to-be-traced>
Example:
target # ./start_tracing.sh westonapp weston-simple-egl
The above command will do the following:
- Setup the required environment for the tracing
- Create a directory under the current working directory called pvrtrace
- Launch the application specified by the user
- Start tracing the PVR Interactions while recording the traces to a file under the current directory
To end the tracing, the user can invoke the Ctrl-C and the trace file path will be displayed.
The trace file can then be transferred to a PC, and we can visualize the application using the host side PVRTrace utility. Please refer PowerVR-SDK for more details.
| [1] | CRTC stands for cathode-ray tube controller, a throw back to the old cathode-ray tubes TV’s which had a controller that generated video timings based on the data it is being fed by a buffer. |