3.5.2.5.2.4.1. Initializing the PRU from a TI-RTOS Core (Legacy)ΒΆ
Note
The PRU Getting Started Labs do not cover TI-RTOS cores controlling the PRU. TI-RTOS SDKs are available for the following processors: AM335x, AM437x, AM57x, AM65x. Some legacy information is provided here for AM335x, AM437x, AM57x customers using PROCESSOR-SDK-RTOS 6.3. HOWEVER, this information has not been tested or validated in several years. These steps are provided as-is. TI cannot answer questions about these steps. Because of the lack of support, These sections are marked as legacy.
TI no longer provides support for TI-RTOS / baremetal SW development for AM335x & AM437x. See this notice for more information.
- Launch CCS and open a Workspace
- Go to File > New > CCS Project
- Select your Target in the first dropdown menu and your Board in the second dropdown menu. Select your Connection in the third dropdown menu.
- Select the Cortex A [ARM] tab and give your project a name. Select the GNU (Linaro) compiler.
- Under Project templates and examples select SYS/BIOS and then GNU Target Examples and finally Typical.
- Select Next >. Under Products and Repositories select <processor> PDK, SYS/BIOS, and XDAIS.
- Select the Platform that you’re using from the drop down menu.
- Right click the project folder in the Project Explorer. Select Properties from the drop down menu. Select CCS Build > GNU Linker > Libraries
- Select Add... in the top bar of the Libraries box. Click Browse. Navigate to: <PDK Directory>/packages/ti/osal/lib/tirtos/<processor>/<ARM core>/release. You should see a file titled ti.osal.a<ARM core>fg. If you don’t see the file, make sure you’re browsing all file types. Select that file.
Note
For AM335x / AM437x / AM572x, ARM core is a8 / a9 / a15, and the file is named ti.osal.aa8fg / ti.osal.aa9fg / ti.osal.aa15fg.
- Open your app.cfg file in the project. Copy the code found in pru-software-support-package/Getting_Started_Labs/PRU_FROM_RTOS/app<processor>.cfg into your app.cfg:
There are a few things that should be noted in this configuration file. Jump to the section for the processor that you are using:
- pru_getting_started_labs_initialize_from_rtos_am335x_code
- pru_getting_started_labs_initialize_from_rtos_am437x_code
- pru_getting_started_labs_initialize_from_rtos_am572x_code
AM335x Configuration File
var Mmu = xdc.useModule('ti.sysbios.family.arm.a8.Mmu');
Mmu.enableMMU = true;
/* Force peripheral section to be NON cacheable strongly-ordered memory */
var peripheralAttrs = {
type : Mmu.FirstLevelDesc_SECTION, // SECTION descriptor
tex: 1,
bufferable : false, // bufferable
cacheable : false, // cacheable
shareable : false, // shareable
noexecute : true, // not executable
};
/* Define the base address of the 1 Meg page the peripheral resides in. */
var peripheralBaseAddr = 0x4A300000;
/* Configure the corresponding MMU page descriptor accordingly */
Mmu.setFirstLevelDescMeta(peripheralBaseAddr,
peripheralBaseAddr,
peripheralAttrs);
In the above code: Mmu.enableMMU = true; enables the MMU. Mmu.setFirstLevelDescMeta sets the page of memory starting at peripheralBaseAddr to be non cacheable as described in peripheralAttrs.
var socType = "am335x";
/* Load the PRUSS package */
var Pruss = xdc.loadPackage('ti.drv.pruss');
Pruss.Settings.socType = socType;
/* Load the uart package */
var Uart = xdc.loadPackage('ti.drv.uart');
Uart.Settings.socType = socType;
/*use CSL package*/
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
/* Load the board package */
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "<YOUR_BOARD_HERE>";
The above configuration code loads in the modules neccesary to load the PRU from the A8.
Click here to move on to the next step: pru_getting_started_labs_initialize_from_rtos_continue.
AM437x Configuration File
var Mmu = xdc.useModule('ti.sysbios.family.arm.a8.Mmu');
Mmu.enableMMU = true;
var peripheralAttrs = {
type : Mmu.FirstLevelDesc_SECTION, // SECTION descriptor
tex: 0,
bufferable : false, // bufferable
cacheable : false, // cacheable
shareable : false, // shareable
noexecute : true, // not executable
};
/* Define the base address of the 1 Meg page the peripheral resides in. */
var peripheralBaseAddr = 0x54400000;
/* Configure the corresponding MMU page descriptor accordingly */
Mmu.setFirstLevelDescMeta(peripheralBaseAddr,
peripheralBaseAddr,
peripheralAttrs);
System.SupportProxy = SysMin;
Mmu.enableMMU = true; enables the MMU. Mmu.setFirstLevelDescMeta sets the page of memory starting at peripheralBaseAddr to be non cacheable as described in peripheralAttrs. There is a quirk here where the A9 uses the A8’s MMU configuration. This is intended.
var socType = "am437x";
/* Load the PRUSS package */
var Pruss = xdc.loadPackage('ti.drv.pruss');
Pruss.Settings.socType = socType;
/* Load the uart package */
var Uart = xdc.loadPackage('ti.drv.uart');
Uart.Settings.socType = socType;
/*use CSL package*/
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
/* Load the board package */
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "<YOUR_BOARD_HERE>";
The above configuration code loads in the modules neccesary to load the PRU from the A9.
Click here to move on to the next step: pru_getting_started_labs_initialize_from_rtos_continue.
AM572x Configuration File
var socType = "am572x";
/* Load the PRUSS package */
var Pruss = xdc.loadPackage('ti.drv.pruss');
Pruss.Settings.socType = socType;
/* Load the uart package */
var Uart = xdc.loadPackage('ti.drv.uart');
Uart.Settings.socType = socType;
/*use CSL package*/
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
/* Load the board package */
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "<YOUR_BOARD_HERE>";
The above configuration code loads in the modules neccesary to load the PRU from the A15.
Continue
- Board options for <YOUR_BOARD_HERE> can be found in <PDK>/Packages/ti/board/src. Change <YOUR_BOARD_HERE> to be one of those options listed.
- You will need the PRU program that you wish to load to be in hex array format as a .h file that is included in your project folder. Instructions on how to do that can be found above in the Compiling to a Hex Array File section.
- You’ll need to create a target configuration file in order to launch your board
and initialize PRU-ICSS. You can do this by navigating to Window > Show Viewv > Target Configurations. Then select New Target Configuration File. Select your Board and Connection type and select save.
Right-click the newly created .ccxml file and select Launch selected configuration
Connect to the Cortex A core, Reset the CPU, and then navigate to Scripts > PRU_ICSS > PRU_ICSS_INIT for AM335x & AM437x, or Scripts > AM572X MULTICORE Initialization > AM572X_MULTICORE_EnableAllCores for AM572x. Select the init script.
Load the PRU program and run it.
- Connect to the PRU (for AM335x), or to a PRU in PRU-ICSS0 (for AM437x &
AM572x). Pause the PRU. Navigate to Window > Show View > Disassembly and select it.
- The PRU Program that you compiled into a hex array should now appear in the IRAM of the PRU.