3.10.1. Jailhouse

3.10.1.1. Overview

Jailhouse is a static partitioning hypervisor that runs bare metal binaries. It cooperates closely with Linux. Jailhouse doesn’t emulate resources that don’t exist. It splits existing hardware resources into isolated compartments called “cells” that are wholly dedicated to guest software programs called “inmates”. One of these cells runs the Linux OS and is known as the “root cell”. Other cells borrow CPUs and devices from the root cell as they are created.

  • The picture below shows the Jailhouse on a system before the Jailhouse is enabled

../../../_images/arch_native.png
  • After the Jailhouse is enabled

../../../_images/enable_jailhouse.png
  • After a cell is created

../../../_images/root_inmate_new.png

Jailhouse consists of three parts:

  • A Kernel module

  • A Hypervisor firmware

  • Tools

The tools helps in enabling the hypervisor on the device at runtime, in creating a cell, to load inmate a binary, to run the inmate binary and to stop the hypervisor itself.

3.10.1.2. Enabling hypervisor on AM62Px platform

Jailhouse is an example of Asynchronous Multiprocessing (AMP) architecture. When we boot Linux on a multi-core ARM processor, Linux initially utilizes all availabale cores. After enabling the hypervisor, it moves Linux to the root-cell which continues to use all ARM cores. When a new cell is created (ex. for linux-demo), hypervisor calls cpu_down() for subset of ARM cores from the root cell, typically reserving one core for Linux and assigning the remaining cores to the new cell. The new cell will use the allocated ARM cores and hardware resources, dedicated for this cell in the cell configuration file.

The open source Jailhouse project from https://github.com/siemens/jailhouse is integrated in Yocto build environment.

  • Yocto recipe (master) for Jailhouse can be found here: meta-ti.

  • Jailhouse kernel patches are integrated with TI Linux Kernel (v6.18) and hosted here Linux git.ti. This repository includes Jailhouse module, uio_ivshmem module for shared-memory and device tree changes for Jailhouse.

  • U-Boot port for Jailhouse can be found here U-Boot git.ti. This repository contains the fix for error message during boot after memory for Jailhouse is reserved in device tree.

3.10.1.3. Building Jailhouse Image for AM62Px platform

The list of components which should be built to get Jailhouse Image for AM62Px are:

  • U-Boot ( tiboot3.bin, tispl.bin, u-boot.img ).

  • Kernel ( with Jailhouse and shared memory module ).

  • Filesystem for root cell and RAM filesystem for inmate.

There are two options to build Jailhouse Image, one is using open source Yocto build environment with public repositories mentioned above or the other method is to use sources and makefile from TI Processors SDK installer.

3.10.1.3.1. Building Jailhouse Image using Yocto

Refer to prerequisites for Yocto build for an Ubuntu host: Host Setup - Ubuntu (Recommended).

The steps to download and build the AM62Px wic Image containing Jailhouse (tisdk- jailhouse-image) using Yocto build environment are as listed below :

$ git clone https://git.ti.com/git/arago-project/oe-layersetup.git tisdk
$ cd tisdk
$ ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-<version>-config.txt
$ cd build
$ . conf/setenv
$ echo 'TI_EXTRAS="tie-jailhouse"' >> conf/local.conf
$ MACHINE=<machine> bitbake -k tisdk-jailhouse-image

The bitbake command mentioned in the last line above builds the tisdk-jailhouse-image, the image can be located at tisdk/build/deploy-ti/images/am62pxx-evm.

This image includes a host cell filesystem Image based on arago ‘default’ filesystem, boot partition with bootloader binaries and kernel Image with Jailhouse components and uio_ivshmem kernel module for shared memory applications. The filesystem image also contains a RAM filesystem (cpio) which gets mounted by kernel booting on an inmate cell.

3.10.1.3.2. Building Jailhouse using TI SDK Installer

The latest Processor SDK Linux AM62Px installer is available on AM62Px-SDK-Download-page.

The installer should be downloaded on a Linux ubuntu host machine. The steps to install the sources using installer are:

$ chmod +x ./ti-processor-sdk-linux-<machine>-<version>-Linux-x86-Install.bin
$ ./ti-processor-sdk-linux-<machine>-<version>-Linux-x86-Install.bin

Create an SD card with prepackaged filesystem image by following instructions from the link Create SD Card with custom images.

The Jailhouse kernel sources, Jailhouse firmware and u-boot bootloader sources can be customized or modified and then built using the steps given below.

Jailhouse sources are located at $TI_SDK_PATH/board-support/extra-drivers/jailhouse directory. The top level SDK Makefile has the jailhouse_clean, jailhouse and jailhouse_install targets which can be used to clean, build and install Jailhouse to the target file system using the default configs or after making any required changes.

Following are the additional dependencies needed to be installed in host PC for jailhouse build.

$ sudo apt-get install device-tree-compiler python3-dev

Python package:
$ pip3 install Mako

The exact commands are:

$ make jailhouse_clean
$ make jailhouse
$ make jailhouse_install DESTDIR=<root partition of target>

These commands can be used to install Jailhouse kernel module, firmware and management tools in the target filesystem.

The kernel and u-boot sources for Jailhouse image are located at $TI_SDK_PATH/board-support/linux-extras-* and $TI_SDK_PATH/board-support/uboot-extras-*. These targets can be build and installed using top-level Makefile.

Below commands can be used to install kernel image and modules to root of the target filesystem.

$ make linux-extras
$ make linux-extras_install DESTDIR=<root partition of target>

Below commands can be used to install bootloader binaries to the boot partition of target.

$ make u-boot-extras
$ make u-boot-extras_install DESTDIR=<boot partition of target>

3.10.1.4. Generate SD Card Image for Jailhouse

You can download the tisdk-jailhouse-image-am62pxx-evm.rootfs.wic.xz from here AM62Px-SDK-Download-page.

After that you need to flash the tisdk-jailhouse-image-am62pxx-evm.rootfs.wic.xz to a SD Card. Various ways to flash wic image on SD card are mentioned here Create SD Card.

3.10.1.5. Booting the SD Card Image

After the tisdk-jailhouse-image-am62pxx-evm.rootfs.wic.xz is flashed to SD Card. Change the boot mode pins in AM62Px board for SD Card boot.

SW1[1:8] = 11000010 and SW2[1:8] = 01000000

Insert the SD Card in SD Card slot in AM62Px board. Use a USB Micro-B cable to connect the host PC to the USB Micro-B interface for UART on the EVM then power on the board, the following logs can be observed on the terminal window:

Trying to boot from MMC2
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Starting ATF on ARM64 core...

...


 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project am62pxx-evm -

Arago 2025.01 am62pxx-evm -

am62pxx-evm login:

Note

Jailhouse module is not autoloaded during boot-up. To load the jailhouse module after boot, run following commands:

root@am62pxx-evm: modprobe jailhouse

3.10.1.6. Pre-built components in Jailhouse Image

The target filesystem on AM62Px platform will consists of the following Jailhouse components:

  1. jailhouse.ko : kernel module at /lib/modules/<linux_kernel_version>/extra/driver directory;

  2. jailhouse.bin : hypervisor at /lib/firmware directory;

  3. Jailhouse management tools: /usr/local/libexec/jailhouse and /usr/sbin directories;

In order to create the root-cell and an inmate cell we need to provide cell configuration files. Those configuration files and example binaries are located at /usr/share/jailhouse/cells and /usr/share/jailhouse/inmates.

3.10.1.7. Jailhouse Interface

Jailhouse provides several user-space interfaces. Some important ones are listed below:

  • Enable Jailhouse

root@am62pxx-evm: jailhouse cell enable <root cell config>
  • To create a new cell

root@am62pxx-evm: jailhouse cell create <inmate cell config>
  • To list the running cell(s)

root@am62pxx-evm: jailhouse cell list
  • Stop inmate cell

root@am62pxx-evm: jailhouse cell shutdown <id or name of inmate cell>
  • Destroy cell

root@am62pxx-evm: jailhouse cell destroy <id or name of inmate cell>
  • Disable Jailhouse

root@am62pxx-evm: jailhouse disable

3.10.1.8. Running Jailhouse Demos on AM62Px

3.10.1.8.1. Host Setup

Flash tisdk-jailhouse-image-am62pxx-evm.rootfs.wic.xz to SD card using balena and boot AM62Px from the SD card. As we will be running two instances ,two terminals are required. Connect one terminal to the primary UART (e.g. /dev/ttyUSB0) and the other to the secondary UART (e.g. /dev/ttyUSB1).

3.10.1.8.2. Running Linux Demo

The goal of this demo is to partition the CPU cores and run a second instance of the Linux kernel with a RAM filesystem. The inmate kernel will use the secondary UART to provide a login shell to the user. The steps to run the demo are:

  • First enable Jailhouse

root@am62pxx-evm: jailhouse enable /usr/share/jailhouse/cells/k3-am62p5-sk.cell
  • Create an inmate cell for linux

root@am62pxx-evm: jailhouse cell create /usr/share/jailhouse/cells/k3-am62p5-sk-linux-demo.cell
  • Load the required inmate binaries

linux-loader.bin is a small application provided and built by Jailhouse source tree to run inmates. As you can see (-a 0x0) it is loaded to virtual address 0x0. “-s “kernel=0x9e0200000 dtb=0x9e0000000” -a 0x1000” - is the linux_loader argument loaded as string to virtual address 0x1000, which instructs the linux-loader to branch to the those addresses. Kernel Image is loaded to the virtual address 0x9e0200000, jailhouse inmate ramfs to 0x9e2b4a000 and device tree for inmate to 0x9e0000000.

root@am62pxx-evm: jailhouse cell load k3-am62p5-sk-linux-demo /usr/libexec/jailhouse/linux-loader.bin -a 0x0 -s "kernel=0x9e0200000 dtb=0x9e0000000" -a 0x1000 /boot/Image -a 0x9e0200000 /boot/tisdk-jailhouse-inmate-am62pxx-evm.cpio -a 0x9e2b4a000 /usr/share/jailhouse/inmate-k3-am62p5-sk.dtb -a 0x9e0000000
  • Start inmate cell

root@am62pxx-evm: jailhouse cell start k3-am62p5-sk-linux-demo
  • Now, on the secondary terminal, verify that the inmate kernel has booted with RAM filesystem. Also note that the /dev/ttySX number used for root cell and inmate may or may not match.

[  OK  ] Finished Record Runlevel Change in UTMP.

|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project am62pxx-evm -

Arago 2025.01 am62pxx-evm -

am62pxx-evm login: root

The Linux demo (i.e Two Guest VMs) can be started using the linux-demo.sh script in that folder. There is no such script for the bare-metal demos but the commands are very similar (all the needed pieces are in the filesystem already).

3.10.1.8.3. Run Crash Test To Detect Inmate Failure

The Jailhouse image also packages crash-test application, designed to detect crashes in the inmate Linux system by sending ICMP packets at regular intervals from the root side. If the application fails to receive ICMP echo reply packets within the expected timeframe, it prints “No response received for packet x” on the console which signifies a potential crash in the inmate Linux system.

It utilizes network interface created on both root and inmate side using the ivshmem net module to facilitate communication between the root side and the inmate Linux system. It ensures continuous monitoring for effective crash detection.

Crash test application can be run by using the linux-demo.sh script present in /usr/share/jailhouse.

To start crash test after linux demo

root@<machine>: ./usr/share/jailhouse/linux-demo.sh -c

To start crash test in background mode

root@<machine>: ./usr/share/jailhouse/linux-demo.sh -c -b

To skip crash test and only start linux demo

root@<machine>: ./usr/share/jailhouse/linux-demo.sh

3.10.1.8.4. Adding custom demos or applications in Inmate Filesystem

Custom demos can also be run in inmate after copying the required files in RAM filesystem. This can be done using following steps:-

  • Extract the tisdk-jailhouse-inmate-am62pxx-evm.rootfs.cpio file in a separate folder(ex. temp) in linux host PC. This file is present in /media/$USER/root/boot/ or from output from yocto build.

$ cpio -iv < <path to cpio>/tisdk-jailhouse-inmate-image-<machine>.rootfs.cpio
  • Copy the your demo/app to folder where cpio is extracted

$ cp <TI-SDK-PATH>/board-support/extra-drivers/jailhouse/tools/demos/ivshmem-demo <path to extracted cpio>
  • Generate a new cpio file

$ find . | sort | cpio --reproducible -o -H newc -R root:root > <path you want to save your new cpio>/tisdk-jailhouse-inmate-<machine>.rootfs.cpio

3.10.1.8.5. Running Shared Memory Demo

The Jailhouse image contains modules for userspace I/O system (UIO) and Inter-VM shared memory (IVSHMEM). This allows VMs to communicate with each other via a shared memory mechanism.The IVSHMEM device is emulated in the hypervisor, and the shared memory regions are reserved in the DTB for cross-cell communication.

For shared-memory demo we can use ivshmem-demo application located at tools/demos in Jailhouse source directory. ivshmem-demo application is already packaged in root and inmate.

Boot the Jailhouse image and run the linux demo script. After both root and linux inmate are is started to check whether the device node exists run

root@<machine>: ls /dev/uio0
root@<machine>: cat /proc/interrupts | grep uio.

Run ivshmem-demo on both root and inmate cell

  • Root cell

root@am62pxx-evm:/usr/share/jailhouse# ivshmem-demo
ID = 0
Maximum peers = 3
state[0] = 1
state[1] = 0
state[2] = 3
rw[0] = 0
rw[1] = -1
rw[2] = 1
in@0x0000 = 0
in@0x2000 = -1
in@0x4000 = -1

Sending interrupt 1 to peer 1

Sending interrupt 1 to peer 1

Sending interrupt 1 to peer 1

Sending interrupt 1 to peer 1

Interrupt #1
state[0] = 1
state[1] = 0
state[2] = 0
rw[0] = 1
rw[1] = -1
rw[2] = 1
in@0x0000 = 10
in@0x2000 = -1
in@0x4000 = -1
  • Inmate cell

root@am62pxx-evm:/home# ./ivshmem-demo
main program startedID = 2
Maximum peers = 3
state[0] = 0
state[1] = 0
state[2] = 3
rw[0] = -1
rw[1] = -1
rw[2] = 0
in@0x0000 = �
in@0x2000 = -1
in@0x4000 = -1

Sending interrupt 3 to peer 0

Sending interrupt 3 to peer 0

Interrupt #1
state[0] = 1
state[1] = 0
state[2] = 3
rw[0] = 0
rw[1] = -1
rw[2] = 1
in@0x0000 =
in@0x2000 = -1
in@0x4000 = -1

Sending interrupt 3 to peer 0

Sending interrupt 3 to peer 0

Sending interrupt 3 to peer 0

Sending interrupt 3 to peer 0
^C

You can see interrupts will be received in both inmate and root cell. Also, check the values using

root@<machine>:~# cat /proc/interrupts | grep uio

Below changes in ivshmem-demo.c can be done to send characters from root to inmate and vice versa.

diff --git a/tools/demos/ivshmem-demo.c b/tools/demos/ivshmem-demo.c
index f9ef438e..4e1d26db 100644
--- a/tools/demos/ivshmem-demo.c
+++ b/tools/demos/ivshmem-demo.c
@@ -75,7 +75,9 @@ static void print_shmem(void)
    printf("rw[0] = %d\n", rw[0]);
    printf("rw[1] = %d\n", rw[1]);
    printf("rw[2] = %d\n", rw[2]);
-   printf("in@0x0000 = %d\n", in[0/4]);
+   //printf("in@0x0000 = %d\n", in[0/4]);
+   char *s = (char *)in;
+   printf("in@0x0000 = %c\n", s[0]);
    printf("in@0x2000 = %d\n", in[0x2000/4]);
    printf("in@0x4000 = %d\n", in[0x4000/4]);
}
@@ -193,7 +195,8 @@ int main(int argc, char *argv[])
                             error(1, errno, "read(uio)");

                    rw[id] = int_count;
-                   out[0] = int_count * 10;
+                   //out[0] = int_count * 10;
+                   memcpy((void *)out, "H", sizeof("H"));
                    printf("\nInterrupt #%d\n", int_count);
                    print_shmem();

It will send character (here “H”) to root to inmate or vice versa when an interrupt is received.

Note

You may shutdown and start the same binary multiple times. Every time you start the binary, it starts from the beginning.

If you have different binaries which use the same cell resources, you may reuse the created cell to run them. You need just shutdown the cell, load another binary and start it. If you need to run different binaries that requires different resources, you need to shutdown the running cell, destroy it, create a new one with required resources, load a new binary and start it.

3.10.1.8.6. Running Ethernet Demo

This application demonstrates how to use IVSHMEM Ethernet to communicate with another linux inmate cell in the Jailhouse hypervisor. Configure the eth2 in root cell and eth0 in inmate cell and ping.

  • In inmate cell

root@<machine>: ip addr add 192.168.0.3 dev eth0
root@<machine>: ip link set eth0 up
  • In root cell

root@<machine>: ip addr add 192.168.0.2 dev eth2
root@<machine>: ip link set eth2 up

Ping eth0 using eth2 #ping 192.168.0.2 in root cell or ping eth2 using eth0 ping 192.168.0.3 in inmate cell.

Ex. ping to inmate cell from root cell

root@<machine>:~# ping -c 4 192.168.0.3
PING 192.168.0.3 (192.168.0.3) 56(84) bytes of data.
64 bytes from 192.168.0.3: icmp_seq=1 ttl=64 time=0.780 ms
64 bytes from 192.168.0.3: icmp_seq=2 ttl=64 time=0.413 ms
64 bytes from 192.168.0.3: icmp_seq=3 ttl=64 time=0.407 ms
64 bytes from 192.168.0.3: icmp_seq=4 ttl=64 time=0.415 ms

--- 192.168.0.3 ping statistics ---
4 packets transmitted, 4 received, 0% packet loss, time 3057ms
rtt min/avg/max/mdev = 0.407/0.503/0.780/0.159 ms

3.10.1.8.7. Running Baremetal Demos

Jailhouse comes with inmate demos located at the inmates/demos directory. We will see the working of two demo inmates: gic-demo and uart-demo. Those are very simple bare-metal applications that demonstrate a uart and arm-timer interrupt. These demos are common for all Jailhouse platforms.

3.10.1.8.7.1. Running UART Demo

  • Enable Jailhouse

root@am62pxx-evm: jailhouse enable /usr/share/jailhouse/cells/k3-am62p5-sk.cell
  • Create a inmate cell

root@am62pxx-evm: jailhouse cell create /usr/share/jailhouse/cells/k3-am62p5-sk-inmate-demo.cell
  • load uart-demo.bin in inmate cell

root@am62pxx-evm: jailhouse cell load inmate-demo /usr/share/jailhouse/inmates/uart-demo.bin
  • Start inmate cell

root@am62pxx-evm: jailhouse cell start inmate-demo
  • You will see UART demo running in secondary terminal for inmate

Hello 1 from cell!
Hello 2 from cell!
Hello 3 from cell!
Hello 4 from cell!
Hello 5 from cell!
Hello 6 from cell!
Hello 7 from cell!
Hello 8 from cell!

3.10.1.8.7.2. Running GIC Demo

  • Enable Jailhouse

root@am62pxx-evm: jailhouse enable /usr/share/jailhouse/cells/k3-am62p5-sk.cell
  • Create a inmate cell

root@am62pxx-evm: jailhouse cell create /usr/share/jailhouse/cells/k3-am62p5-sk-inmate-demo.cell
  • Load gic-demo.bin in inmate cell

root@am62pxx-evm: jailhouse cell load inmate-demo /usr/share/jailhouse/inmates/gic-demo.bin
  • Start inmate cell

root@am62pxx-evm: jailhouse cell start inmate-demo
  • You will see GIC demo running in secondary terminal inmate

Initializing the GIC...
Initializing the timer...
Timer fired, jitter:   9324 ns, min:   9324 ns, max:   9324 ns
Timer fired, jitter:   4794 ns, min:   4794 ns, max:   9324 ns
Timer fired, jitter:   4289 ns, min:   4289 ns, max:   9324 ns
Timer fired, jitter:   4249 ns, min:   4249 ns, max:   9324 ns
Timer fired, jitter:    739 ns, min:    739 ns, max:   9324 ns
Timer fired, jitter:   4489 ns, min:    739 ns, max:   9324 ns
Timer fired, jitter:   4184 ns, min:    739 ns, max:   9324 ns
Timer fired, jitter:   4184 ns, min:    739 ns, max:   9324 ns
Timer fired, jitter:   5034 ns, min:    739 ns, max:   9324 ns

3.10.1.9. Memory Reservation

Linux kernel has to reserve some memory for Jailhouse hypervisor and for inmate. This memory has to be reserved statically.

Following example shows reservation of 518MB physical memory for hypervisor, inmates and also shared memory region for cross-cell communication.

hyp_mem: jailhouse@9dfa00000 {
      reg = <0x00000009 0xdfa00000 0x0 0x20600000>;
      alignment = <0x1000>;
      no-map;
};

3.10.1.10. Hardware Modules Reservation

Jailhouse is a partitioning hypervisor. This means a HW peripheral is in exclusive control of one of the cells. Jailhouse cell config file defines this ownership to ensure that all accesses to peripherals are isolated between different cells. Access to any peripheral outside of the owned will be treated as violation, and Jailhouse will park that cell. To ensure that Linux uses only the assigned peripheral, we can disable the peripherals which are owned by the other cell.

Following nodes describe an example of how devices are disabled in the root cell device tree.

/* Disable uart used by inmate cell */
&main_uart1 {
     status = "disabled";
};

/* Disable emmc instance used by inmate cell */
&sdhci0 {
     status = "disabled";
 };

3.10.1.11. Root-cell configuration

When hypervisor is being enabled it creates a cell for Linux and moves it to that cell. The cell is called as “root-cell”. The cell configuration as a “.c” which gets compiled to “.cell” file. The hypervisor uses the “cell” file to create a cell. The cell configuration describes memory regions and their attributes which will be used by the cell,

.mem_regions = {
/* IVSHMEM shared memory regions for 00:00.0 (demo)
{
      .phys_start = 0x9dfa00000,
      .virt_start = 0x9dfa00000,
      .size = 0x10000,
      .flags = JAILHOUSE_MEM_READ,
},
{
      .phys_start = 0x9dfa10000,
      .virt_start = 0x9dfa10000,
      .size = 0x10000,
      .flags = JAILHOUSE_MEM_READ | JAILHOUSE_MEM_WRITE,
},
/* Peer 0 {
      .phys_start = 0x9dfa20000,
      .virt_start = 0x9dfa20000,
      .size = 0x10000,
      .flags = JAILHOUSE_MEM_READ | JAILHOUSE_MEM_WRITE,
},
/* Peer 1 {
      .phys_start = 0x9dfa30000,
      .virt_start = 0x9dfa30000,
      .size = 0x10000,
      .flags = JAILHOUSE_MEM_READ,
},
/* Peer 2 {
      .phys_start = 0x9dfa40000,
      .virt_start = 0x9dfa40000,
      .size = 0x10000,
      .flags = JAILHOUSE_MEM_READ,
},
/* IVSHMEM shared memory region for 00:01.0
JAILHOUSE_SHMEM_NET_REGIONS(0x9dfb00000, 0),
{
      .phys_start = 0x01810000,
      .virt_start = 0x01810000,
      .size = 0x00070000,
      .flags = JAILHOUSE_MEM_READ | JAILHOUSE_MEM_WRITE |
      JAILHOUSE_MEM_IO,
},
{
      .phys_start = 0x018a0000,
      .virt_start = 0x018a0000,
      .size = 0x00060000,
      .flags = JAILHOUSE_MEM_READ | JAILHOUSE_MEM_WRITE |
      JAILHOUSE_MEM_IO,
},
/* RAM {
      .phys_start = 0x80000000,
      .virt_start = 0x80000000,
      .size = 0x80000000,
      .flags = JAILHOUSE_MEM_READ | JAILHOUSE_MEM_WRITE |
      JAILHOUSE_MEM_EXECUTE,
},
/* RAM {
      .phys_start = 0x880000000,
      .virt_start = 0x880000000,
      .size = 0x15fa00000,
      .flags = JAILHOUSE_MEM_READ | JAILHOUSE_MEM_WRITE |
      JAILHOUSE_MEM_EXECUTE,
},
/* RAM. Reserved for inmates {
      .phys_start = 0x9e0000000,
      .virt_start = 0x9e0000000,
      .size = 0x20000000,
      .flags = JAILHOUSE_MEM_READ | JAILHOUSE_MEM_WRITE |
      JAILHOUSE_MEM_EXECUTE,
},

bitmap of CPU cores dedicated for the cell,

.cpus = {
      0xf,
},

bitmap of interrupt controller SPI interrupts

.irqchips = {
     {
         .address = 0x01800000,
         .pin_base = 32,
         .pin_bitmap = {
         0xffffffff, 0xffffffff, 0xffffffff, 0xffffffff,
         },
     },
     {
         .address = 0x01800000,
         .pin_base = 160,
         .pin_bitmap = {
         0xffffffff, 0xffffffff, 0xffffffff, 0xffffffff,
         },
     },
     {
         .address = 0x01800000,
         .pin_base = 288,
         .pin_bitmap = {
         0xffffffff, 0xffffffff, 0xffffffff, 0xffffffff,
         },
     },
     {
         .address = 0x01800000,
         .pin_base = 416,
         .pin_bitmap = {
         0xffffffff, 0xffffffff, 0xffffffff, 0xffffffff,
         },
     },
     {
         .address = 0x01800000,
         .pin_base = 544,
         .pin_bitmap = {
         0xffffffff, 0xffffffff, 0xffffffff, 0xffffffff,
         },
     },
},

and some other parameters.

In addition to this, the root cell also allocates the physical memory for the hypervisor.

.hypervisor_memory = {
      .phys_start = 0x9dfc00000,
      .size = 0x400000,
},

The “memory regions” section is used by hypervisor to create the second stage MMU translation table.

3.10.1.12. Performance

3.10.1.12.1. Cache Benchmark

In the Jailhouse hypervisor environment, cache benchmarking involves executing cache-intensive operations, like the dd command, on the root side, while simultaneously employing the perf tool on the inmate side to measure cache performance metrics. This setup ensures that the cache activity generated on the root side is monitored in real-time on the inmate side, allowing user to analyze cache hit rates, misses, and other relevant metrics. Both the root and inmate system share one instance of L2 cache. It’s important to emphasize that the performance observed during cache benchmarking in a Jailhouse hypervisor environment may vary due to several factors. These include workload characteristics, cache utilization patterns, system resource availability, and potential interference from other processes or system activities.

Root

root@am62pxx-evm:/usr/share/jailhouse# dd if=/dev/zero of=large_file bs=1M count=2000
2000+0 records in
2000+0 records out
2097152000 bytes (2.1 GB, 2.0 GiB) copied, 26.8668 s, 78.1 MB/s

Inmate

root@am62pxx-evm:~# perf stat -B -e cache-references,cache-misses,cycles,instructions,branches,faults,migrations sleep 5

Performance counter stats for 'sleep 5':

      342780      cache-references
        9929      cache-misses                     #    2.90% of all cache refs
     3417097      cycles
      911493      instructions                     #    0.27  insn per cycle
      103554      branches
          58      faults
           0      migrations

5.004324530 seconds time elapsed

0.000000000 seconds user
0.004692000 seconds sys

root@am62pxx-evm:~# perf stat -B -e cache-references,cache-misses,cycles,instructions,branches,faults,migrations sleep 5

Performance counter stats for 'sleep 5':

      342453      cache-references
        9657      cache-misses                     #    2.82% of all cache refs
     2729625      cycles
      908783      instructions                     #    0.33  insn per cycle
      102995      branches
          58      faults
           0      migrations

5.003581220 seconds time elapsed

0.003911000 seconds user
0.000000000 seconds sys