3.8.8. OpenCL
The OpenCL™ libraries in the Processor SDK Linux AM62Px allow offloading tasks to the GPU for compute centric libraries without the GPU or CPU usage incurred by managing displays or creating a offscreen context. The drivers run on an ARM core and programs the firmware running inside a GPU core with commands submitted by the user applications.
OpenCL™ differs from OpenGL® in that it makes use of a predefined Installable Client Driver (ICD) Loader to allow applications to query and pick the device it deems necessary instead of relying on a predefined mapping between a chosen display and backing vendor acceleration implementation. This means that typically an application that wants to use OpenCL™ should link against an ICD loader library instead of directly using a specific library.
Note
Some tools dynamically load their respective OpenCL™ library at
runtime by using dlopen, which can fail in Yocto based environments. This is
usually the result of a clash in philosophies between Yocto and Application
developers over the usage of devlinks (also know in Yocto as “dev-so”s). It
is Yocto’s belief that, for the most part, applications should not try to use
dev links directly and should instead open the specific version of the
library they need. You can patch the application to do this or create the
devlink from /usr/lib/libOpenCL.so to /usr/lib/libOpenCL.so.1
manually. Tools provided by Yocto will are already patched.
A useful tool for debugging OpenCL™ ICD Loaders and devices is clinfo. This command, when run without any arguments will present a list of all supported devices, associated parameters, and supported extensions.
For more information about OpenCL™ extensions see: