6.1. TI Apps Launcher - User Guide
6.1.1. Overview
TI Apps Launcher is a QT Based Application launcher for TI Platforms. Currently, TI Apps Launcher incorporates following applications across all supported platforms,
Industrial HMI
Live Camera
Benchmarks
GPU Performance
Seva Store
Chromium
Settings
All of the necessary equipment requirement and instructions are provided here.
Note
Not all of the above set of applications are supported by each platform. So there will be differences between each.
6.1.2. Hardware Prerequisites
PC (Windows or Linux, to use serial terminal console)
HDMI Monitor (to view the Demo on Display)
Ethernet Cable (to connect AM62Px SK to internet)
USB Camera or OV5640 camera sensor module (for Live Camera)
Keyboard & Mouse (to control the TI Apps Launcher)
SD card (minimum 16GB)
6.1.3. Launching and Using the TI Apps Launcher
The TI Apps Launcher launches on Linux startup. Follow the below instructions to use it.
Flash an SD card with the
tisdk-default-image. User can download thetisdk-default-imagewic image from AM62Px-SDK-Download-page. Please follow the instructions from here to Flash an SD card.
Note
Images may vary between each platform based on the number of supported applications.
Insert the flashed SD card to the board, connect the display, mouse, ethernet cable, keyboard and power on the SK-EVM. The TI Apps Launcher will launch automatically when the device is fully booted.
6.1.3.1. Launching the Industrial HMI
To launch the Industrial HMI demo, click on the Industrial HMI button on the left menu.
You can click on the Auto-Manual slider button to switch modes.
In Manual mode, you can use the ^ and v buttons of each motor to control the RPM.
6.1.3.2. Launching the Camera App
AM62Px has hardware codecs which are capable of encoding and decoding H.246 and H.265 Videos.
The Camera app supports recording and playback of video in H264 and H265 formats.
Click on the ‘Camera’ button on the left menu to start the app.
If a camera is detected, it will start previewing by default.
By default, the Codec chosen for recording and playback is H264. If you want to use H265 instead, just toggle the switch on the bottom left corner.
If there are multiple cameras connected, you can switch between them by selecting the preferred camera from Cameras Dropdown.
Once a camera is selected and the preview is visible, you can start recording by clicking on the Record/Stop button right next to the Cameras Dropdown. The Camera preview will still be available while recording.
The status message on the top right will display the filename into which the video is being recorded.
Press the Record/Stop button again to Stop Recording.
To play the recorded videos, Select a video file from the Gallery Dropdown, and click Play Button. The info about the file being played will be displayed on the top left corner.
This player can be used to play any .h264, .h265 and .mp4 (h264 and h265 only) files. To test with other files instead of recorded videos, copy the test files to
/opt/ti-apps-launcher/gallery/.
Note
The Gallery Dropdown filters files based on the name of the file. So the filename must have “h264” or “h265” as substring.
To delete the recorded files, after selecting the file from Dropdown, click Delete Button next to the Play Button.
6.1.3.3. Launching the ARM Analytics Demo
Note
ARM Analytics Demo is only supported on AM62x SK, AM62x-LP SK, AM62PX and BeaglePlay. AM62SIP doesn’t support it.
This app tries to showcase the ARM optimized models for Object Detection, Face Detection and Image Classification.
To launch the ARM Analytics demo, click on the ARM Analytics button on the left panel.
By default, the ARM Analytics demo shows the results of Object Detection Model on existing data.
To test Face Detection or Image Classification, Click on the respective buttons available at the bottom of the main window.
6.1.3.4. Launching the Benchmarks Demo
The Benchmarks Demo includes various System Benchmarks like dhrystone, linpack, nbench, etc. and GPU benchmarks like glmark2.
Click on the Benchmarks button on the left panel.
User will now see the list of Benchmarks available to test on SK-EVM. Click on the play button infront of the benchmark you like to test. The image below is captured while running the glmark2.
Once after the entire benchmark has been run, the FPS & Score will get populated in the table.
6.1.3.5. Launching the GPU Performance Demo
The GPU Performance demo allows users to vary the GPU loads using glmark2. Click on the GPU Performance button on the left panel.
Now you can choose the GPU Load Level from the buttons available on the right. Choose from ‘0’ which is no load to ‘4’ max load.
You will see the updated values of FPS & Score metrices getting populated in the table.
6.1.3.6. Launching the Seva Store
Note
Seva Store is not supported on AM62xSIP due to it’s memory constraints.
Processor SDK Linux AM62Px now supports Seva Store. Seva Store is a TI developed demo gallery which allows users to download and install demos on the go. Developers can host their demos as Docker Images on any public Docker Registry and link them to Seva Design Gallery.
Refer Seva Store - User Guide to know more about Seva Store.
6.1.3.7. Launching the Chromium Browser
Note
Chromium Browser is not supported on AM62xSIP due to it’s memory constraints.
Processor SDK Linux AM62Px now supports GPU Accelarated Chromium Browser. Click on the Chromium button on the left panel.
Click Launch button to launch the Chromium Browser. The Browser launches with WebGL Aquarium as the first tab by default.
Refer Chromium Browser - User Guide to know more about Chromium Browser.
6.1.3.8. Launching the 3D Demo
Note
3D Demo requires weston to be running or EGLFS context to run. ti-apps-launcher is run on EGLFS so it is not supported on AM62xSIP.
Click on the 3D Demo button on the left panel.
Click Launch button to launch the 3D Demo by Imagination. By default, you would see the Skinning Model running on the screen.
You can use mouse buttons or spacebar to pause the 3D Demo and press ESC to exit & go back to TI Apps Launcher.
6.1.3.10. Using terminal
The terminal button on the left panel can be used to open a terminal application, which is based on QMLtermwidget.
6.1.3.11. Using Wi-Fi Demo
The Wifi button on the left panel allows you to connect to an external Wi-Fi network.
Ensure the required overlay is applied and the M.2 Wi-Fi card is connected to SK-EVM. For more information, refer to How to Enable M.2-CC33x1 in Linux.
Click the toggle button to turn on Wi-Fi.
Click on the Refresh button to scan for available SSIDs.
Select an SSID from the list, then enter the passphrase and Wi-Fi security type.
For certain security types, you may need to provide additional details.
After entering all the required info, click on Connect.
If the all entered details are correct, device will be connected to the selected Wi-Fi network. If needed, click Disconnect to disconnect from the network and return to SSID selection menu.
6.1.4. Compiling TI Apps Launcher
The ideal way to compile TI Apps Launcher is to trigger a Yocto build. But for a quicker way to do it, especially during development, TI provides a debian-arm64 Docker image. This image already has all dependencies required for compiling ti-apps-launcher.
First, clone TI Apps Launcher on host:
git clone https://github.com/texasinstruments/ti-apps-launcher.git
export TI_APPS_LAUNCHER_REPO="$(pwd)/ti-apps-launcher"
cd ti-apps-launcher
Then, add the following line in CMakeLists.txt:
add_compile_definitions(SOC_AM62=1) # if target is AM62x or AM62SIP
add_compile_definitions(SOC_AM62_LP=1) # if target is AM62x-LP
add_compile_definitions(SOC_AM62P=1) # if target is AM62P
Then, install the QEMU user mode emulators for enabling cross-architecture execution on host system:
sudo apt-get install qemu-user-static
Then, pull TI’s debian-arm64 Docker image and run it:
docker pull ghcr.io/texasinstruments/debian-arm64:latest
docker run -it -v ${TI_APPS_LAUNCHER_REPO}:/root/ti-apps-launcher ghcr.io/texasinstruments/debian-arm64 bash
Finally, run:
cd /root/ti-apps-launcher/
cmake -B build -S . -DRT_BUILD=0 # if target is RT image, make -DRT_BUILD=1
make -C build
The compiled binary should be build/ti-apps-launcher.
Copy the compiled binary to /usr/bin/ directory of the target:
scp ${TI_APPS_LAUNCHER_REPO}/build/ti-apps-launcher root@<ip-addr-of-device>:/usr/bin
If you have modified the scripts in the scripts/ directory, then copy them too:
scp -r ${TI_APPS_LAUNCHER_REPO}/scripts root@<ip-addr-of-device>:/opt/ti-apps-launcher
Note
This is a quick and easy way to compile ti-apps-launcher during development, but it is a good idea to validate with Yocto builds often. There is a possibility that compiler mismatch could present issues in the run up to production.