2.2. Yocto Layer Configuration
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.
Config File |
Description |
Supported machines/platforms |
---|---|---|
processor-sdk-kirkstone-chromium-09.02.01.10-config.txt |
Processor SDK 09.02.01.10 Release |
am62pxx-evm |