2.3. Yocto Layer Configuration

Processor SDK uses oe-layersetup configuration files to initialize the Yocto build environment. Configure your build with the following command:

$ ./oe-layertool-setup.sh -f <config>

Replace <config> with one of the following configuration files.

The oe-layersetup git repository has the following configuration files in the configs/processor-sdk directory.

Table 2.2 Yocto Layer Configuration

Config File

Description

Supported machines/platforms

processor-sdk-scarthgap-chromium-11.02.08.02-config.txt

Used for building chromium browser enabled Yocto based filesystem

am62pxx-evm

processor-sdk-scarthgap-11.02.08.02-config.txt

Used for building Yocto based filesystem

am62pxx-evm

processor-sdk-scarthgap-selinux-11.02.08.02-config.txt

Used for building SELinux enabled Yocto based filesystem

am62pxx-evm

The oe-layersetup configuration, as defined in processor-sdk-scarthgap-chromium-11.02.08.02-config.txt, is used for configuring the meta layers in the yocto SD card image available on AM62Px-SDK-Download-page.