6.1. How to Enable M.2-CC33x1 in Linux
Processor SDK 10.0 introduces support for the CC33XX family of devices. These devices feature Wi-Fi 6 (802.11ax) for the 2.4 and 5GHz frequency bands, and can be attached to embedded linux devices communicating over SDIO. The CC3351 supports both 2.4 and 5GHz frequencies, while the CC3301 supports only 2.4GHz. Find more information about the CC3301 here.
Because the AM6x starter kits now feature an M.2 Key-E connector, an M.2 card has been developed for evaluation purposes. Order the M.2-CC3301 board from here. The M.2-CC3351 is also interchangeable and uses the exact same instructions below.
By default, the Processor SDK includes support for the M.2-CC33x1 on the following starter kits:
SK-AM62B-P1
SK-AM62A-LP
SK-AM62P-LP
AM62L-EVM
6.1.1. Hardware Installation
To install the M.2-CC33x1, remove the screw from the Starter Kit’s M.2 connector. Place the M.2-CC33x1 into the Key-E slot. Place the M.2 card into the Starter Kit’s slot, and insert the screw such that the edge of the M.2 card is held down by the screw. The end result should be as shown in the image below.
6.1.2. Enable DT Overlay for M.2-CC33x1
After flashing the SD card with the tisdk-debian-trixie-image, mount the SD card onto a host computer, if not done already.
On the boot partition of the SD card, add one of the following variables, corresponding to the starter kit,
into the uEnv.txt file. This will let u-boot enable the m.2-cc33x1 devicetree overlay. The uEnv.txt file can be found on the boot
partition of the SD card.
For SK-AM62B-P1:
name_overlays=ti/k3-am625-sk-m2-cc3351.dtbo
For SK-AM62A-LP:
name_overlays=ti/k3-am62a7-sk-m2-cc3351.dtbo
For SK-AM62P-LP:
name_overlays=ti/k3-am62p5-sk-m2-cc3351.dtbo
For AM62L-EVM:
name_overlays=ti/k3-am62l3-evm-m2-cc3351.dtbo
Note
Though the name of the file ends with m2-cc3301.dtbo, the same file applies for the M.2-CC3351 board.
Do not change the name of this file in the uEnv.txt regardless of which M.2 card that is being used.
6.1.3. Connect to Wi-Fi
TI’s Debian SDK uses NetworkManager to connect to wifi. To connect, ensure that NetworkManager.service is running with the following command:
systemctl status NetworkManager.service
It should show status as “active”. If it isn’t active, activate it by running the following:
systemctl restart NetworkManager.service
Then, to actually connect to wifi, use nmcli as follows:
nmcli device wifi list
nmcli device wifi connect "<SSID>" password "<password>"
Note
The following command also works and will prompt for a password:
nmcli device wifi connect --ask "<SSID>"
For more information on the Wi-Fi capabilities of the CC33xx devices, please see the documentation that can be found in the CC33xx SDK.