2.5.1. RT-linux 11.01 Performance Guide
Read This First
All performance numbers provided in this document are gathered using following Evaluation Modules unless otherwise specified.
Name |
Description |
|---|---|
AM62Px SK |
AM62Px Starter Kit rev E1 with ARM running at 1.4GHz, DDR data rate 3200 MT/S |
Table: Evaluation Modules
About This Manual
This document provides performance data for each of the device drivers which are part of the Processor SDK Linux package. This document should be used in conjunction with release notes and user guides provided with the Processor SDK Linux package for information on specific issues present with drivers included in a particular release.
If You Need Assistance
For further information or to report any problems, contact https://e2e.ti.com/ or https://support.ti.com/
2.5.1.1. System Benchmarks
Stress-ng and Cyclic Test
stress-ng (next-generation) will stress test a embedded platform in various selectable ways. It was designed to exercise various physical subsystems as well as the various operating system kernel interfaces. stress-ng can also measure test throughput rates; this can be useful to observe performance changes across different operating system or types of hardware.
Cyclictest is most commonly used for benchmarking RT systems. It is one of the most frequently used tools for evaluating the relative performance of real-time systems. Some performance tests which use Cyclictest are System benchmarking, Latency debugging with tracing and approximating application performance.
Test commands used for running stress-ng and cyclictest together
stress-ng --cpu-method=all -c 4 &
cyclictest -m -Sp80 -D6h -h400 -i200 -M -q
The following summarizes the latencies observed using the yocto based default SDK image
Note
Using the OP-TEE TRNG driver can impact this benchmark’s performance due to frequent context switching between Normal World (Linux) and Secure World (OP-TEE), that occurs when the kernel’s hardware random number generator interface (hwrng) requests entropy from the secure TRNG to replenish the Linux entropy pool.
The Linux TRNG driver can mitigate these latency spikes. This involves enabling the Pseudo RNG driver in OP-TEE as documented in the Foundational Components section: Building OP-TEE with Pseudo RNG drivers, and enabling the RNG node in the Linux kernel device tree. This way the HW TRNG is accessed from the kernel itself.
Latencies |
CPU 0 |
CPU 1 |
CPU 2 |
CPU 3 |
|---|---|---|---|---|
Minimum (usec) |
5 |
5 |
5 |
5 |
Average (usec) |
6 |
6 |
7 |
6 |
Maximum (usec) |
36 |
34 |
37 |
34 |