3.2.2.13. OSPI/QSPI NOR/NAND

Introduction

Octal Serial Peripheral Interface (OSPI) and Quad Serial Peripheral Interface (QSPI) are SPI modules that have x8 IO lines and x4 IO lines respectively. These controllers are mainly used to interface with Octal and Quad SPI flashes. OSPI is backward compatible with QSPI. These modules can also work in dual (x2) and single (x1) modes. OSPI and QSPI controllers on TI SoCs support memory mapped IO interfaces, which provide a direct interface for accessing data from the external SPI flash, thereby simplifying software requirements. These controllers work only in master mode.

SoC Family

Capability

Driver

AM62Px/J7200

OSPI NOR

drivers/spi/spi-cadence-quadspi.c

Note

Not all OSPI flashes can be supported. Users are recommended to check whether or not the OSPI flash part chosen for custom board designs meets all the criteria listed at https://e2e.ti.com/support/processors/f/791/t/946418

Driver Features

OSPI controllers supports Double Data Rate (DDR) mode for OSPI/QSPI NOR flashes in Octal configuration wherein data can be read on both edges of the clock, and Single Data Rate (SDR) mode for OSPI/QSPI NAND flashes in Quad and Octal configuration.

Memory mapped read support

Once the controller is configured in memory map mode, the whole flash memory is made available as a memory region at an SoC specific address. This region can be accessed using normal memcpy() (or mem-to-mem dma copy). Controller hardware will internally communicate with SPI flash over SPI bus and get the requested data. This mode provides the best throughput and is the default mode in the SDK.

Supported SPI modes

The spi-cadence-quadspi.c driver supports standard SPI mode 0 only.

DMA support

The driver uses mem-to-mem DMA copy on top of an OSPI/QSPI memory mapped port during flash read operations for maximum throughput and reduced CPU load.

Driver Architecture

../../../../_images/linux_qspi.png

Fig. 3.2 OSPI/QSPI NOR/NAND software stack

The OSPI Controller does not support interfacing with non-flash SPI slaves.

Driver Configuration

Source Location

OSPI driver is at: drivers/spi/spi-cadence-quadspi.c under Linux kernel source tree. This driver also supports QSPI version of the same IP.

Kernel Configuration Options

The driver can be built into the kernel or can be compiled as module and loaded into the kernel dynamically.

Enabling OSPI/QSPI Driver Configurations

Following needs to be enabled to access OSPI/QSPI flash: TI QSPI controller driver, Cadence OSPI controller driver, SPI NOR framework, and/or SPI NAND framework in the kernel via menuconfig.

Note

OSPI/QSPI drivers and their dependencies are enabled by default in the SDK images. So this section can be skipped in that case.

Start the Linux Kernel Configuration tool:

$ make menuconfig ARCH=<architecture_name>

To enable QSPI controller driver:

Device Drivers  --->
[*] SPI support  --->
   <*>   DRA7xxx QSPI controller support

To enable SPI NOR framework:

Device Drivers  --->
   <*> Memory Technology Device (MTD) support  --->
   <*>   SPI-NOR device support  --->

To enable SPI NAND framework:

Device Drivers  --->
   <*> Memory Technology Device (MTD) support  --->
   <*>   NAND  --->
      <*>   SPI NAND device Support  --->

To enable spi-cadence-quadspi driver:

Device Drivers  --->
   [*] SPI support --->
   <*>   Cadence Quad SPI controller

To enable them as modules, make <*> as <M>.

Enabling UBIFS filesystem support:

File systems  --->
   [*] Miscellaneous filesystems  --->
   <*>   UBIFS file system support

DT Configuration

For spi-cadence-quadspi controller refer to Documentation/devicetree/bindings/spi/cdns,qspi-nor.yaml for DT bindings and their usage.

To configure OSPI/QSPI NOR/NAND flash partitions and flash related DT bindings refer to Documentation/devicetree/bindings/mtd/jedec,spi-nor.yaml, Documentation/devicetree/bindings/mtd/spi-nand.yaml and Documentation/devicetree/bindings/mtd/partitions/partition.yaml.

The following is an example device-tree node for an OSPI NOR device

&ospi0 {

   flash@0{
      compatible = "jedec,spi-nor";
      reg = <0x0>;
      spi-tx-bus-width = <8>;
      spi-rx-bus-width = <8>;
      spi-max-frequency = <25000000>;
      cdns,tshsl-ns = <60>;
      cdns,tsd2d-ns = <60>;
      cdns,tchsh-ns = <60>;
      cdns,tslch-ns = <60>;
      cdns,read-delay = <4>;

      partitions {
         compatible = "fixed-partitions";
         #address-cells = <1>;
         #size-cells = <1>;
         bootph-all;

         partition@0 {
            label = "ospi.tiboot3";
            reg = <0x00 0x80000>;
         };

         partition@80000 {
            label = "ospi.tispl";
            reg = <0x80000 0x200000>;
         };

         // other partitions
      };
   };
};

Flash properties:

  1. compatible: specifies the compatible string for the device, the operating system uses this string to identify and the match the driver for the device. Use ‘jedec,spi-nor’ for OSPI/QSPI NOR flashes and ‘spi-nand’ for OSPI/QSPI NAND flashes.

  2. spi-tx-bus-width and spi-rx-bus-width: specifies the bus width in bits for SPI transactions when transmitting (tx) and receiving (rx) data. Set for ‘8’ for OSPI flashes and ‘4’ for QSPI flashes.

  3. spi-max-frequency: defines the maximum frequency in Hertz at which the SPI bus can operate. Set 1/4th or 1/8th of ‘assigned-clocks’ value of ‘ospi0’ node for SDR and DDR mode respectively.

  4. cdns,read-delay: specifies the delay in clock cycles between the fetch of a command and responding to that command by the flash devices. This differs with flashes, try with different read delays starting from 0 and find the minimum read-delay at which the flash driver probes correctly.

Driver Usage

Note

Although OSPI/QSPI NOR/NAND are different at hardware level, from Linux point of view, they are managed in the same way and are exposed as /dev/mtdX devices to the user space. Therefore, there is virtually no difference to end user even though OSPI/QSPI NOR/NAND use different drivers underneath. Therefore this section applies to both OSPI/QSPI NOR/NAND.

Load UBI module for using ubi commands:

$ modprobe ubi

This should create /dev/mtdX entries for every partition defined in DT or via command line arguments. MTD abstracts all types of flashes and, therefore, both OSPI/QSPI NOR/NAND appear as MTD devices. To see all MTD partitions in the system run:

$ cat /proc/mtd

Here is an example output (name varies depending on what is passed in DT or via command line arguments):

dev:    size   erasesize  name
mtd0: 00080000 00010000 "QSPI.U_BOOT"
mtd1: 00080000 00010000 "QSPI.U_BOOT.backup"
mtd2: 00010000 00010000 "QSPI.U-BOOT-SPL_OS"
mtd3: 00010000 00010000 "QSPI.U_BOOT_ENV"
mtd4: 00010000 00010000 "QSPI.U-BOOT-ENV.backup"
mtd5: 00800000 00010000 "QSPI.KERNEL"
mtd6: 036d0000 00010000 "QSPI.FILESYSTEM"

Testing

Using mtd-utils

$ cat /proc/mtd # Should list OSPI/QSPI partitions
$ flash_erase  /dev/mtd6 0 0 # Erase entire /dev/mtd6
$ dd if=/dev/random of=tmp_write.txt bs=1 count=num # num = bytes to write to flash
$ mtd_debug write /dev/mtd6 0 num tmp_write.txt # write to num bytes to flash
$ mtd_debug read /dev/mtd6 0 num tmp_read.txt # read to num bytes to flash
$ diff tmp_read.txt tmp_write.txt # should be NULL

Using dd command

$ cat /proc/mtd # Should list OSPI/QSPI partitions
$ flash_erase  /dev/mtd6 0 0 # Erase entire /dev/mtd6
$ dd if=/dev/random of=tmp_write.txt bs=1 count=num # num = bytes to write to flash
$ dd if=tmp_write.txt of=/dev/mtd6 bs=num count=1 # write to num bytes to flash
$ dd if=/dev/mtd6 of=tmp_read.txt bs=num count=1 # read to num bytes to flash
$ diff tmp_read.txt tmp_write.txt # should be NULL

Note

Make sure UBIFS filesystem is enabled in the kernel (refer to this section for more information).

Refer here for UBIFS.

root~# ubiformat /dev/mtd9
ubiformat: mtd9 (nor), size 23199744 bytes (22.1 MiB), 354 eraseblocks of 65536 bytes (64.0 KiB), min. I/O size 1 bytes
libscan: scanning eraseblock 353 -- 100% complete
ubiformat: 354 eraseblocks are supposedly empty
ubiformat: formatting eraseblock 353 -- 100% complete
root:~# ubiattach -p /dev/mtd9
[  270.874428] ubi0: attaching mtd9
[  270.914131] ubi0: scanning is finished
[  270.921788] ubi0: attached mtd9 (name "QSPI.file-system", size 22 MiB)
[  270.928405] ubi0: PEB size: 65536 bytes (64 KiB), LEB size: 65408 bytes
[  270.935210] ubi0: min./max. I/O unit sizes: 1/256, sub-page size 1
[  270.941491] ubi0: VID header offset: 64 (aligned 64), data offset: 128
[  270.948102] ubi0: good PEBs: 354, bad PEBs: 0, corrupted PEBs: 0
[  270.954215] ubi0: user volume: 0, internal volumes: 1, max. volumes count: 128
[  270.961602] ubi0: max/mean erase counter: 0/0, WL threshold: 4096, image sequence number: 2077421476
[  270.970887] ubi0: available PEBs: 350, total reserved PEBs: 4, PEBs reserved for bad PEB handling: 0
[  270.980204] ubi0: background thread "ubi_bgt0d" started, PID 863
UBI device number 0, total 354 LEBs (23154432 bytes, 22.1 MiB), available 350 LEBs (22892800 bytes, 21.8 MiB), LEB size 65408 bytes (63.9 KiB)
root:~# ubimkvol /dev/ubi0 -N flash_fs -s 20MiB
Volume ID 0, size 321 LEBs (20995968 bytes, 20.0 MiB), LEB size 65408 bytes (63.9 KiB), dynamic, name "flash_fs", alignment 1
root:~# mkdir /mnt/flash
root:~# mount -t ubifs ubi0:flash_fs /mnt/flash/
[  326.002602] UBIFS (ubi0:0): default file-system created
[  326.008309] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 866
[  326.027530] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "flash_fs"
[  326.035157] UBIFS (ubi0:0): LEB size: 65408 bytes (63 KiB), min./max. I/O unit sizes: 8 bytes/256 bytes
[  326.044615] UBIFS (ubi0:0): FS size: 20341888 bytes (19 MiB, 311 LEBs), journal size 1046528 bytes (0 MiB, 16 LEBs)
[  326.055123] UBIFS (ubi0:0): reserved for root: 960797 bytes (938 KiB)
[  326.061610] UBIFS (ubi0:0): media format: w4/r0 (latest is w4/r0), UUID 828AA98E-3A51-4B35-AD50-9E90144AD4C7, small LPT model
root:~#

Now you can access filesystem at /mnt/flash/.

Using Micron MT35XU512ABA1G12-0AAT flash on AM62x and AM62P

The AM62x and AM62P-LP Starter Kits (SK) by default come with the Cypress S28HS512TGABHM010 flash. But the Micron MT35XU512ABA1G12-0AAT flash can also be used with some slight modifications to the device tree properties. The patch below should allow to use the Micron flash. Note that applying it will likely make the Cypress flash unusable.

diff --git a/arch/arm64/boot/dts/ti/k3-am625-sk.dts b/arch/arm64/boot/dts/ti/k3-am625-sk.dts
index f353db3664ac..bb2ef6a88455 100644
--- a/arch/arm64/boot/dts/ti/k3-am625-sk.dts
+++ b/arch/arm64/boot/dts/ti/k3-am625-sk.dts
@@ -253,7 +253,7 @@ flash@0 {
               cdns,tsd2d-ns = <60>;
               cdns,tchsh-ns = <60>;
               cdns,tslch-ns = <60>;
-              cdns,read-delay = <4>;
+              cdns,read-delay = <0>;

               partitions {
                        bootph-all;
@@ -291,10 +291,10 @@ partition@800000 {
                              reg = <0x800000 0x37c0000>;
                        };

-                       partition@3fc0000 {
+                       partition@3fe0000 {
                              bootph-pre-ram;
                              label = "ospi.phypattern";
-                             reg = <0x3fc0000 0x40000>;
+                             reg = <0x3fe0000 0x20000>;
                        };
               };
      };

Runtime Power Management

The OSPI Controller supports runtime power management where it can suspend when there is no activity concerning the OSPI peripheral.

It suspends after a certain period of inactivity based on the value of CQSPI_AUTOSUSPEND_TIMEOUT which is set to 2000 ms in it’s driver spi-cadence-quadspi.c

root@am62xx-evm:~# head /sys/bus/platform/devices/fc40000.spi/power/*
==> /sys/bus/platform/devices/fc40000.spi/power/autosuspend_delay_ms <==
2000

==> /sys/bus/platform/devices/fc40000.spi/power/control <==
auto

==> /sys/bus/platform/devices/fc40000.spi/power/runtime_active_time <==
5808

==> /sys/bus/platform/devices/fc40000.spi/power/runtime_status <==
suspended

==> /sys/bus/platform/devices/fc40000.spi/power/runtime_suspended_time <==
112684

To increase the auto suspend delay value, one can write into the autosuspend_delay_ms sysfs entry like below,

echo <delay> > /sys/bus/platform/devices/fc40000.spi/power/autosuspend_delay_ms

One can verify that OSPI has actually suspended by also looking at the k3conf output as shown below.

root@am62xx-evm:~# k3conf dump device 75
|------------------------------------------------------------------------------|
| VERSION INFO                                                                 |
|------------------------------------------------------------------------------|
| K3CONF | (version 0.3-nogit built Thu Jul 25 14:13:02 UTC 2024)              |
| SoC    | AM62X SR1.0                                                         |
| SYSFW  | ABI: 4.0 (firmware version 0x000a '10.0.8--v10.00.08 (Fiery Fox))') |
|------------------------------------------------------------------------------|

|------------------------------------------------------|
| Device ID | Device Name           | Device Status    |
|------------------------------------------------------|
|    75     | AM62X_DEV_FSS0_OSPI_0 | DEVICE_STATE_OFF |
|------------------------------------------------------|

This shows that the OSPI controller is physically turned off and thus no longer contributing to active power consumed by the system.

When a transaction is initiated from userspace or otherwise, the driver resumes the OSPI controller automatically.