3.1.1.7. DDRSS ECC
3.1.1.7.1. Overview
The DDR subsystem (DDRSS) comprises DDR controller, DDR PHY and wrapper logic to integrate these blocks in the device. For SDRAM data integrity, the DDRSS bridge supports inline ECC on the data written to or read from the SDRAM. ECC is stored together with the data so that a dedicated SDRAM device for ECC is not required. The 8-bit single error correction double error detection (SECDED) ECC data is calculated over 64-bit data quanta. For every 256-byte data block 32 bytes of ECC is stored inline. Thus 1/9th of the total SDRAM space is used for ECC storage and the remaining 8/9th of the SDRAM data space are seen as consecutive byte addresses. Even if there are non-ECC protected regions the previously described 1/9th-8/9th rule still applies and consecutive byte addresses are seen from system point of view. AM62Px supports up to 3 ECC protected non-overlapping memory ranges. The current U-Boot release supports a single region covering the entire SDRAM space.
ECC is calculated for all accesses that are within the address ranges protected by it. 1-bit error is correctable by ECC, but multi-bit and multiple 1-bit errors are not correctable and will be treated as an uncorrectable error. Any uncorrectable error will cause a bus abort. There are three ways to handle it:
By default, it is reported as a synchronous data abort to software
Enable ESM pin corresponding to DDRSS ECC uncorrectable error
DDR*SS0_DDRSS_DRAM_ECC_UNCORR_ERR_LVL_0
which routes an ECC uncorrectable error to ESMTrap it using
HANDLE_EA_EL3_FIRST_NS
and with help of a custom handlerplat_ea_handler()
in trusted-firmware-a report the cause
Note
Options 1 and 2 doesn’t report the reason. So, if there is a need to report the reason behind uncorrectable error handle it the third way.
3.1.1.7.1.1. DDRSS ECC handling
Note
The ECC feature of DDRSS is not enabled by default in U-Boot.
Note
Apply the patch on top of ti-u-boot (tag: 09.02.00.009).
This patch is to fix up the RAM size correctly if ECC is enabled.
Patch: https://git.ti.com/cgit/ti-u-boot/ti-u-boot/patch/?id=26c81a4d5b31b0ca6a57bcd30d115f458cb98192
3.1.1.7.1.1.1. Enabling ECC
The ECC feature of DDRSS can be enabled by the following two steps:
Add
ti,ecc-enable
boolean property to thememorycontroller
node// u-boot/arch/arm/dts/k3-*-ddr.dtsi &memorycontroller { power-domains = <&k3_pds 170 TI_SCI_PD_SHARED>, <&k3_pds 55 TI_SCI_PD_SHARED>; clocks = <&k3_clks 170 0>, <&k3_clks 16 4>; ti,ecc-enable; };Re-build U-Boot with
CONFIG_K3_INLINE_ECC
enabled# u-boot/configs/*_r5_defconfig CONFIG_PINCTRL_SINGLE=y CONFIG_POWER_DOMAIN=y CONFIG_TI_POWER_DOMAIN=y CONFIG_K3_INLINE_ECC=y CONFIG_K3_SYSTEM_CONTROLLER=y CONFIG_REMOTEPROC_TI_K3_ARM64=y CONFIG_RESET_TI_SCI=y
3.1.1.7.1.1.2. Priming with BIST Engine
The bootloader has the responsibility to pre-load the ECC protected region with known data before functional reads and writes are performed. During the ECC initialization, the R5 SPL fills the entire memory with zeros using the BIST engine in the DDR controller. The BIST engine method allows priming the entire region with zeros in much less time.
3.1.1.7.1.1.3. Simulating ECC error
U-Boot command ‘ddrss’ can be used to simulate the ECC error by generating bit errors in SDRAM data at certain address. The ECC check can be tested by:
Enabling ECC
Shrinking the protected range
Modifying a value
Restoring range to original and
Reading the value will cause the ECC error
The command syntax is
ddrss ecc_err <addr in hex> <bit_err in hex>
The command will read data from addr
and write data ^ bit_err
back to
addr
.
3.1.1.7.1.1.3.1. Single bit error
The following example generates a 1-bit error on bit 0 of the data at address 0x82400000.
=> ddrss ecc_err 82400000 1 Testing DDRSS ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400000, read data 0x0, written data 0x1, err pattern: 0x1, read after write data 0x1 ECC test: Enabled DDR ECC ... ECC test: addr 0x82400000, read data 0x0 ECC test: DDR ECC 1-bit error ECC test: 1-bit ECC err count: 1 ECC test: 1-bit error in [0x2400000:0x2400008]
Reading from 0x82400000 returns a corrected value, the 1-bit error counter is incremented, and the offset of the error in the physical memory is reported in 8-byte range.
The following example flips the bit back, which clears the error state.
=> ddrss ecc_err 82400000 1 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400000, read data 0x1, written data 0x0, err pattern: 0x1, read after write data 0x0 ECC test: Enabled DDR ECC ... ECC test: addr 0x82400000, read data 0x0
3.1.1.7.1.1.3.2. Multi bit error and Multiple single bit error
3.1.1.7.1.1.3.2.1. Synchronous Abort (default)
The following example generates a 2-bit error on bits 0 and 1 of the data at address 0x82400000.
=> ddrss ecc_err 82400000 3 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400000, read data 0x0, written data 0x3, err pattern: 0x3, read after write data 0x3 ECC test: Enabled DDR ECC ... "Synchronous Abort" handler, esr 0x96000210 elr: 0000000080825450 lr : 0000000080825450 (reloc) elr: 00000000fff03450 lr : 00000000fff03450 x0 : 0000000000000000 x1 : 0000000000000000 x2 : 000000000000000a x3 : 0000000002800000 x4 : 0000000002800000 x5 : 00000000fde9132f x6 : 00000000fffa6762 x7 : 00000000fde91770 x8 : 00000000fffffff0 x9 : 0000000000000008 x10: 0000000000000010 x11: 0000000000000002 x12: 0000000000000002 x13: 00000000fde91948 x14: 00000000fde91a50 x15: 0000000000000000 x16: 00000000fff40520 x17: 0000000000000000 x18: 00000000fde9ddb0 x19: 0000000000000004 x20: 0000000082400000 x21: 0000000000000000 x22: 000000000000023f x23: 0000000000000003 x24: 0000000000000000 x25: 0000000000000000 x26: 000000000f300134 x27: 000000000000dfff x28: 0000000000000000 x29: 00000000fde91770 Code: 9402415d 90000520 9120c400 940020da (b9400282) Resetting CPU ... resetting ... U-Boot SPL 2023.04-00017-gc0a4f47f8365 (Feb 16 2024 - 12:18:21 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') ECC is enabled, priming DDR which will take several seconds. ECC: priming DDR completed in 1356 msec
The following example generates a 1-bit error on bit 0 of the data at addresses 0x82400000 and 0x82400008.
=> ddrss ecc_err 82400000 1 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400000, read data 0x0, written data 0x1, err pattern: 0x1, read after write data 0x1 ECC test: Enabled DDR ECC ... ECC test: addr 0x82400000, read data 0x0 ECC test: DDR ECC 1-bit error ECC test: 1-bit ECC err count: 1 ECC test: 1-bit error in [0x2400000:0x2400008] => ddrss ecc_err 82400008 1 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400008, read data 0x0, written data 0x1, err pattern: 0x1, read after write data 0x1 ECC test: Enabled DDR ECC ... "Synchronous Abort" handler, esr 0x96000210 elr: 0000000080825450 lr : 0000000080825450 (reloc) elr: 00000000fff03450 lr : 00000000fff03450 x0 : 0000000000000000 x1 : 0000000000000000 x2 : 000000000000000a x3 : 0000000002800000 x4 : 0000000002800000 x5 : 00000000fde9132f x6 : 00000000fffa6762 x7 : 00000000fde91770 x8 : 00000000fffffff0 x9 : 0000000000000008 x10: 0000000000000010 x11: 0000000000000002 x12: 0000000000000002 x13: 00000000fde91948 x14: 00000000fde91a50 x15: 0000000000000000 x16: 00000000fff40520 x17: 0000000000000000 x18: 00000000fde9ddb0 x19: 0000000000000004 x20: 0000000082400008 x21: 0000000000000000 x22: 000000000000023f x23: 0000000000000001 x24: 0000000000000000 x25: 0000000000000000 x26: 000000000f300134 x27: 000000000000dfff x28: 0000000000000000 x29: 00000000fde91770 Code: 9402415d 90000520 9120c400 940020da (b9400282) Resetting CPU ... resetting ... U-Boot SPL 2023.04-00017-gc0a4f47f8365 (Feb 16 2024 - 12:18:21 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') ECC is enabled, priming DDR which will take several seconds. ECC: priming DDR completed in 1356 msec
3.1.1.7.1.1.3.2.2. Error Signaling Module (ESM)
The Error Signaling Module (ESM) aggregates events and/or errors from throughout the device into one location. It can signal both low and high priority interrupts to a processor to deal with an event and/or manipulate an I/O error pin to signal an external hardware that an error has occurred. Therefore an external controller is able to reset the device or keep the system in a safe, known state.
The ESM pin corresponding to DDRSS ECC uncorrectable error
DDR32SS0_DDRSS_DRAM_ECC_UNCORR_ERR_LVL_0
is 175.
So, enable it by adding 175 to the ti,esm-pins
property of
main-esm
node.
// u-boot/arch/arm/dts/k3-am62p-*.dts main_esm: esm@420000 { compatible = "ti,j721e-esm"; reg = <0x00 0x420000 0x00 0x1000>; ti,esm-pins = <160>, <161>, <162>, <163>, <175>, <177>, <178>; bootph-pre-ram; };
The following example generates a 2-bit error on bits 0 and 1 of the data at address 0x82400000.
=> ddrss ecc_err 82400000 3 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400000, read data 0x0, written data 0x3, err pattern: 0x3, read after write data 0x3 ECC test: Enabled DDR ECC ...� U-Boot SPL 2023.04-00017-gc0a4f47f8365-dirty (Feb 16 2024 - 12:07:41 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') ECC is enabled, priming DDR which will take several seconds. ECC: priming DDR completed in 1357 msec
The following example generates a 1-bit error on bit 0 of the data at addresses 0x82400000 and 0x82400008.
=> ddrss ecc_err 82400000 1 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400000, read data 0x0, written data 0x1, err pattern: 0x1, read after write data 0x1 ECC test: Enabled DDR ECC ... ECC test: addr 0x82400000, read data 0x0 ECC test: DDR ECC 1-bit error ECC test: 1-bit ECC err count: 1 ECC test: 1-bit error in [0x2400000:0x2400008] => ddrss ecc_err 82400008 1 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400008, read data 0x0, written data 0x1, err pattern: 0x1, read after write data 0x1 ECC test: Enabled DDR ECC ...� U-Boot SPL 2023.04-00017-gc0a4f47f8365-dirty (Feb 16 2024 - 12:07:41 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') ECC is enabled, priming DDR which will take several seconds. ECC: priming DDR completed in 1357 msec
3.1.1.7.1.1.3.2.3. Trusted Firmware-A (TFA) custom handler
plat_ea_handler
is invoked by the runtime exception handling
framework for the platform to handle an External Abort received at
EL3 if HANDLE_EA_EL3_FIRST_NS
is enabled.
Add
plat_ea_handler
to report ECC uncorrectable error and callplat_default_ea_handler
// trusted-firmware-a/plat/ti/k3/common/k3_ea.c #include <inttypes.h> #include <stdint.h> #include <common/bl_common.h> #include <common/debug.h> #include <arch_helpers.h> #include <plat/common/platform.h> #include <bl31/ea_handle.h> #include <lib/mmio.h> #include <platform_def.h> void plat_ea_handler(unsigned int ea_reason, uint64_t syndrome, void *cookie, void *handle, uint64_t flags) { unsigned long v2a_int_stat_reg; v2a_int_stat_reg = mmio_read_32(K3_DDRSS_BASE + K3_DDRSS_V2A_INT_STAT_REG); ERROR_NL(); if(v2a_int_stat_reg & K3_DDRSS_V2A_INT_STAT_REG_ECC2BERR) ERROR("DDR ECC Multi-bit error detected\n"); else if(v2a_int_stat_reg & K3_DDRSS_V2A_INT_STAT_REG_ECCM1BERR) ERROR("DDR ECC Multiple 1-bit error detected\n"); console_flush(); plat_default_ea_handler(ea_reason, syndrome, cookie, handle, flags); }Define the DDRSS registers
K3_DDRSS_BASE
,K3_DDRSS_SIZE
andK3_DDRSS_V2A_INT_STAT_REG
// trusted-firmware-a/plat/ti/k3/include/platform_def.h #define K3_GIC_BASE 0x01800000 #define K3_GIC_SIZE 0x200000 #define K3_DDRSS_BASE 0x0F300000 #define K3_DDRSS_SIZE 0x200 #define K3_DDRSS_V2A_INT_STAT_REG 0xA4 #define K3_DDRSS_V2A_INT_STAT_REG_ECC2BERR BIT(4) #define K3_DDRSS_V2A_INT_STAT_REG_ECCM1BERR BIT(5) #if !K3_SEC_PROXY_LITE #define SEC_PROXY_DATA_BASE 0x32C00000Map
K3_DDRSS_BASE
andK3_DDRSS_SIZE
// trusted-firmware-a/plat/ti/k3/common/k3_bl31_setup.c /* Table of regions to map using the MMU */ const mmap_region_t plat_k3_mmap[] = { K3_MAP_REGION_FLAT(K3_USART_BASE, K3_USART_SIZE, MT_DEVICE | MT_RW | MT_SECURE), K3_MAP_REGION_FLAT(K3_GIC_BASE, K3_GIC_SIZE, MT_DEVICE | MT_RW | MT_SECURE), K3_MAP_REGION_FLAT(K3_GTC_BASE, K3_GTC_SIZE, MT_DEVICE | MT_RW | MT_SECURE), K3_MAP_REGION_FLAT(SEC_PROXY_RT_BASE, SEC_PROXY_RT_SIZE, MT_DEVICE | MT_RW | MT_SECURE), K3_MAP_REGION_FLAT(SEC_PROXY_SCFG_BASE, SEC_PROXY_SCFG_SIZE, MT_DEVICE | MT_RW | MT_SECURE), K3_MAP_REGION_FLAT(SEC_PROXY_DATA_BASE, SEC_PROXY_DATA_SIZE, MT_DEVICE | MT_RW | MT_SECURE), K3_MAP_REGION_FLAT(K3_DDRSS_BASE, K3_DDRSS_SIZE, MT_DEVICE | MT_RW | MT_SECURE), { /* sentinel */ } };Add
trusted-firmware-a/plat/ti/k3/common/k3_ea.c
toBL31_SOURCES
# trusted-firmware-a/plat/ti/k3/common/plat_common.mk BL31_SOURCES += \ ${PLAT_PATH}/common/k3_bl31_setup.c \ ${PLAT_PATH}/common/k3_helpers.S \ ${PLAT_PATH}/common/k3_topology.c \ ${PLAT_PATH}/common/k3_ea.c \ ${K3_GIC_SOURCES} \ ${K3_PSCI_SOURCES} \ ${K3_SEC_PROXY_SOURCES} \ ${K3_TI_SCI_SOURCES} \Enable
HANDLE_EA_EL3_FIRST_NS
# trusted-firmware-a/plat/ti/k3/common/plat_common.mk # Allow customizing the UART baud rate K3_USART_BAUD := 115200 $(eval $(call add_define,K3_USART_BAUD)) HANDLE_EA_EL3_FIRST_NS := 1 # Libraries include lib/xlat_tables_v2/xlat_tables.mk0
The following example generates a 2-bit error on bits 0 and 1 of the data at address 0x82400000.
=> ddrss ecc_err 82400000 3 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400000, read data 0x0, written data 0x3, err pattern: 0x3, read after write data 0x3 ECC test: Enabled DDR ECC ... ERROR: DDR ECC Multi-bit error detected ERROR: Unhandled External Abort received on 0x80000000 from EL2 ERROR: exception reason=1 syndrome=0x92000210 Unhandled Exception from lower EL. x0 = 0x0000000000000000 x1 = 0x0000000000000000 x2 = 0x000000000000000a x3 = 0x0000000002800000 x4 = 0x0000000002800000 x5 = 0x00000000fde9132f x6 = 0x00000000fffa6762 x7 = 0x00000000fde91770 x8 = 0x00000000fffffff0 x9 = 0x0000000000000008 x10 = 0x0000000000000010 x11 = 0x0000000000000002 x12 = 0x0000000000000002 x13 = 0x00000000fde91948 x14 = 0x00000000fde91a50 x15 = 0x0000000000000000 x16 = 0x00000000fff40520 x17 = 0x0000000000000000 x18 = 0x00000000fde9ddb0 x19 = 0x0000000000000004 x20 = 0x0000000082400000 x21 = 0x0000000000000000 x22 = 0x000000000000023f x23 = 0x0000000000000003 x24 = 0x0000000000000000 x25 = 0x0000000000000000 x26 = 0x000000000f300134 x27 = 0x000000000000dfff x28 = 0x0000000000000000 x29 = 0x00000000fde91770 x30 = 0x00000000fff03450 scr_el3 = 0x000000000000073d sctlr_el3 = 0x0000000030cd183f cptr_el3 = 0x0000000000000000 tcr_el3 = 0x0000000080803520 daif = 0x00000000000002c0 mair_el3 = 0x00000000004404ff spsr_el3 = 0x00000000000002c9 elr_el3 = 0x00000000fff03450 ttbr0_el3 = 0x000000009e793240 esr_el3 = 0x0000000092000210 far_el3 = 0x0000000082400000 spsr_el1 = 0x0000000000000000 elr_el1 = 0x0000000000000000 spsr_abt = 0x0000000000000000 spsr_und = 0x0000000000000000 spsr_irq = 0x0000000000000000 spsr_fiq = 0x0000000000000000 sctlr_el1 = 0x0000000030d00801 actlr_el1 = 0x0000000000000000 cpacr_el1 = 0x0000000000000000 csselr_el1 = 0x0000000000000000 sp_el1 = 0x0000000000000000 esr_el1 = 0x0000000000000000 ttbr0_el1 = 0x0000000000000000 ttbr1_el1 = 0x0000000000000000 mair_el1 = 0x0000000000000000 amair_el1 = 0x0000000000000000 tcr_el1 = 0x0000000000800080 tpidr_el1 = 0x0000000000000000 tpidr_el0 = 0x0000000000000000 tpidrro_el0 = 0x0000000000000000 par_el1 = 0x0000000000000000 mpidr_el1 = 0x0000000080000000 afsr0_el1 = 0x0000000000000000 afsr1_el1 = 0x0000000000000000 contextidr_el1 = 0x0000000000000000 vbar_el1 = 0x0000000000000000 cntp_ctl_el0 = 0x0000000000000002 cntp_cval_el0 = 0x0801e3088020c0b2 cntv_ctl_el0 = 0x0000000000000002 cntv_cval_el0 = 0xaefcc7a67dc999c0 cntkctl_el1 = 0x0000000000000000 sp_el0 = 0x000000009e78d6d0 isr_el1 = 0x0000000000000000 dacr32_el2 = 0x0000000000000000 ifsr32_el2 = 0x0000000000000000 cpuectlr_el1 = 0x0000000000000040 cpumerrsr_el1 = 0x00000000010405d7 l2merrsr_el1 = 0x0000000011005408 cpuactlr_el1 = 0x00001000090ca000 U-Boot SPL 2023.04-00017-gc0a4f47f8365 (Feb 16 2024 - 11:30:58 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') ECC is enabled, priming DDR which will take several seconds. ECC: priming DDR completed in 1356 msec
The following example generates a 1-bit error on bit 0 of the data at addresses 0x82400000 and 0x82400008.
=> ddrss ecc_err 82400000 1 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400000, read data 0x0, written data 0x1, err pattern: 0x1, read after write data 0x1 ECC test: Enabled DDR ECC ... ECC test: addr 0x82400000, read data 0x0 ECC test: DDR ECC 1-bit error ECC test: 1-bit ECC err count: 1 ECC test: 1-bit error in [0x2400000:0x2400008] => ddrss ecc_err 82400008 1 Testing DDR ECC: ECC test: Disabling DDR ECC ... ECC test: addr 0x82400008, read data 0x0, written data 0x1, err pattern: 0x1, read after write data 0x1 ECC test: Enabled DDR ECC ... ERROR: DDR ECC Multiple 1-bit error detected ERROR: Unhandled External Abort received on 0x80000000 from EL2 ERROR: exception reason=1 syndrome=0x92000210 Unhandled Exception from lower EL. x0 = 0x0000000000000000 x1 = 0x0000000000000000 x2 = 0x000000000000000a x3 = 0x0000000002800000 x4 = 0x0000000002800000 x5 = 0x00000000fde9132f x6 = 0x00000000fffa6762 x7 = 0x00000000fde91770 x8 = 0x00000000fffffff0 x9 = 0x0000000000000008 x10 = 0x0000000000000010 x11 = 0x0000000000000002 x12 = 0x0000000000000002 x13 = 0x00000000fde91948 x14 = 0x00000000fde91a50 x15 = 0x0000000000000000 x16 = 0x00000000fff40520 x17 = 0x0000000000000000 x18 = 0x00000000fde9ddb0 x19 = 0x0000000000000004 x20 = 0x0000000082400008 x21 = 0x0000000000000000 x22 = 0x000000000000023f x23 = 0x0000000000000001 x24 = 0x0000000000000000 x25 = 0x0000000000000000 x26 = 0x000000000f300134 x27 = 0x000000000000dfff x28 = 0x0000000000000000 x29 = 0x00000000fde91770 x30 = 0x00000000fff03450 scr_el3 = 0x000000000000073d sctlr_el3 = 0x0000000030cd183f cptr_el3 = 0x0000000000000000 tcr_el3 = 0x0000000080803520 daif = 0x00000000000002c0 mair_el3 = 0x00000000004404ff spsr_el3 = 0x00000000000002c9 elr_el3 = 0x00000000fff03450 ttbr0_el3 = 0x000000009e793240 esr_el3 = 0x0000000092000210 far_el3 = 0x0000000082400008 spsr_el1 = 0x0000000000000000 elr_el1 = 0x0000000000000000 spsr_abt = 0x0000000000000000 spsr_und = 0x0000000000000000 spsr_irq = 0x0000000000000000 spsr_fiq = 0x0000000000000000 sctlr_el1 = 0x0000000030d00801 actlr_el1 = 0x0000000000000000 cpacr_el1 = 0x0000000000000000 csselr_el1 = 0x0000000000000000 sp_el1 = 0x0000000000000000 esr_el1 = 0x0000000000000000 ttbr0_el1 = 0x0000000000000000 ttbr1_el1 = 0x0000000000000000 mair_el1 = 0x0000000000000000 amair_el1 = 0x0000000000000000 tcr_el1 = 0x0000000000800080 tpidr_el1 = 0x0000000000000000 tpidr_el0 = 0x0000000000000000 tpidrro_el0 = 0x0000000000000000 par_el1 = 0x0000000000000000 mpidr_el1 = 0x0000000080000000 afsr0_el1 = 0x0000000000000000 afsr1_el1 = 0x0000000000000000 contextidr_el1 = 0x0000000000000000 vbar_el1 = 0x0000000000000000 cntp_ctl_el0 = 0x0000000000000002 cntp_cval_el0 = 0x0801e1088020c0b2 cntv_ctl_el0 = 0x0000000000000002 cntv_cval_el0 = 0xaffcc7a67dc989c0 cntkctl_el1 = 0x0000000000000000 sp_el0 = 0x000000009e78d6d0 isr_el1 = 0x0000000000000000 dacr32_el2 = 0x0000000000000000 ifsr32_el2 = 0x0000000000000000 cpuectlr_el1 = 0x0000000000000040 cpumerrsr_el1 = 0x00000000000405b7 l2merrsr_el1 = 0x0000000011005808 cpuactlr_el1 = 0x00001000090ca000 U-Boot SPL 2023.04-00017-gc0a4f47f8365 (Feb 16 2024 - 11:30:58 +0530) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)') ECC is enabled, priming DDR which will take several seconds. ECC: priming DDR completed in 1356 msec
Note
ESM is a hardware logic to handle errors in the system. If both ESM and trusted-firmware-a logics are enabled, ESM takes charge and resets the device, before trusted-firmware-a handles.
The following example shows the message if the ECC is not enabled in DDRSS.
=> ddrss ecc_err 82400000 1 ECC not enabled. Please enable ECC any try again