3.2.2.12.5. Low Power Modes
3.2.2.12.5.1. Overview
The following sections describe a high-level description of the different low power modes of the device. If your application requires inactive power management, you must determine which low power mode described below satisfies your requirements. Each mode must be evaluated based on power consumption and latency (the time it takes to wakeup to Active mode) requirements. Specific values are detailed in the device-specific data sheet. As part of this SDK offering, Texas Instruments has added support for the following low power modes:
Deep Sleep
MCU Only
Partial I/O
3.2.2.12.5.2. Deep Sleep
Deep Sleep AKA Suspend-to-RAM is a low-power mode that allows an embedded device to retain its state in RAM while the processor is turned off. This can save a significant amount of power, especially in devices that are battery-powered.
The benefits of using deep sleep in embedded devices:
Faster wake-up: devices can wake up from this low-power state much faster than a complete power cycle.
Better efficiency: deep sleep can help to improve the efficiency of embedded devices by reducing the amount of time that the processor is idle. This is because the processor can be kept in a low-power state when it is not needed.
In order to enter deep sleep, use the following command:
root@evm:~# echo mem > /sys/power/state
[ 47.558246] PM: suspend entry (deep)
[ 47.562456] Filesystems sync: 0.000 seconds
[ 47.597364] remoteproc remoteproc1: stopped remote processor 79000000.r5f
[ 47.604640] Freezing user space processes
[ 47.614313] Freezing user space processes completed (elapsed 0.005 seconds)
[ 47.623448] OOM killer disabled.
[ 47.627420] Freezing remaining freezable tasks
[ 47.633363] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[ 47.640783] printk: Suspending console(s) (use no_console_suspend to debug)
[ 47.662936] omap8250 2800000.serial: PM domain pd:146 will not be powered off
[ 47.669305] Disabling non-boot CPUs ...
[ 47.671283] psci: CPU1 killed (polled 0 ms)
[ 47.674127] psci: CPU2 killed (polled 4 ms)
[ 47.676794] psci: CPU3 killed (polled 0 ms)
This partially indicates that linux has finished it’s deep sleep sequence. For further confirmation, one can take a look at the PMIC_LPM_EN pin on the EVM (after programming the PMCTRL_SYS register (0x43018080) to 0x15). Here, if the pin is 3.3V when active and 0V when in deep sleep.
Refer to the Wakeup Sources section for information on how to wakeup the device from Deep Sleep mode using one of the supported wakeup sources.
3.2.2.12.5.3. MCU Only
Similar to Deep Sleep, with the major distinction being that the MCU core is kept alive to run applications. The benefits of using MCU Only mode:
Low power consumption: MCU Only mode can save a significant amount of power, especially in battery-powered devices. This is because The rest of the SoC status is the same as Deep Sleep and DDR is in self-refresh.
Run background tasks: This mode can be used to run background tasks that do not require the full power of the system. For example, you could use the firmware on the MCU core to run a watchdog timer, a sensor polling loop, or a network communication task.
Respond to interrupts: This allows the system to still respond to external events, while it is in a low-power state.
To enter MCU Only mode, enable MCU R5 core as a wakeup source in linux:
root@evm:~# echo enabled > /sys/bus/platform/devices/79000000.r5f/power/wakeup
Now, the SoC can be suspended using the following command:
root@evm:~# echo mem > /sys/power/state
[ 175.651151] PM: suspend entry (deep)
[ 175.655444] Filesystems sync: 0.000 seconds
[ 175.667559] Freezing user space processes
[ 175.673951] Freezing user space processes completed (elapsed 0.002 seconds)
[ 175.681105] OOM killer disabled.
[ 175.684404] Freezing remaining freezable tasks
[ 175.690155] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[ 175.697574] printk: Suspending console(s) (use no_console_suspend to debug)
[ 175.722262] omap8250 2800000.serial: PM domain pd:146 will not be powered off
[ 175.954174] Disabling non-boot CPUs ...
[ 175.956374] psci: CPU1 killed (polled 0 ms)
[ 175.959326] psci: CPU2 killed (polled 0 ms)
[ 175.962024] psci: CPU3 killed (polled 4 ms)
Once the SoC enters MCU Only mode, the following log should be printed on the MCU UART (in most cases it will be /dev/ttyUSB3)
[IPC RPMSG ECHO] Suspend request to MCU-only mode received
[IPC RPMSG ECHO] Press any key on this terminal to resume the kernel from MCU only mode
Refer to the Wakeup Sources section for information on how to wakeup the device from MCU Only mode using one of the supported wakeup sources.
3.2.2.12.5.4. Partial I/O
In Partial I/O, only the I/O pins and a small digital logic in the CANUART I/O Bank are active, while the rest of the SoC is turned off. The user can use the I/O pins to aggregate multiple I/O wakeup events and toggle PMIC_LPM_EN pin to enable PMIC or discrete power solution when an I/O wakeup event is triggered.
Note
The system looses nearly all its state as DDR is also turned-off. Partial I/O is comparable with a Linux poweroff state.
The reference implementation in this SDK implements Partial I/O as a poweroff state. On poweroff, Linux ti_sci driver checks the potential Partial I/O wakeup sources for being enabled. If one of the wakeup sources is found to be enabled, Partial I/O is entered instead of poweroff.
The following wakeup sources have been configured for Partial I/O: mcu_uart0, mcu_mcan0, and mcu_mcan1. Partial I/O mode can only be tested when k3-am62x-sk-lpm-wkup-sources.dtso overlay is loaded. Please refer to How to enable DT overlays for more details.
After Linux boots, the MCAN wakeup for Partial I/O is enabled using the wake on PHY activity option of ethtool. For example, the following command enables mcu_mcan0 wakeup:
root@evm:~# ethtool -s mcu_mcan0 wol p
To enable mcu_mcan1 wakeup:
root@evm:~# ethtool -s mcu_mcan1 wol p
To enable UART wakeup:
root@evm:~# echo enabled > /sys/class/tty/ttyS0/device/power/wakeup
Note
UART wakeup from Partial I/O is currently being debugged on the EVM.
With at least one of the wakeup sources enabled, Partial I/O mode can be entered with the following command:
root@evm:~# poweroff
At this point, Linux kernel will go through its poweroff process and the console output will stop at the following lines:
[ 51.698039] systemd-shutdown[1]: Powering off.
[ 51.769478] reboot: Power down
The system has entered Partial I/O and can only be woken up with an activity on the I/O pin programmed for wakeup. For example, if mcu_mcan0 wakeup was enabled, grounding Pin 22 of J8 MCU Header will wakeup the system and it will go through a normal Linux boot process.
Note
The capability to detect whether system is resuming from Partial I/O or doing a normal cold boot will be added in future release.
3.2.2.12.5.5. Limitations
HWRNG support on GP devices is incompatible with Deep Sleep and MCU Only modes. To test LPM on GP devices, HWRNG has to be unloaded one-time before running the Suspend-to-RAM command:
root@evm:@~# modprobe -r optee_rng