3.2.2.9. CPSW Ethernet¶
3.2.2.9.1. Introduction¶
The CPSW Ethernet Subsystem is capable of supporting MAC mode, Switch mode, VLAN and the standard TSN features such as PTP, EST, CBS and IET.
Note
To operate in switch mode, at least two external ports are required.
3.2.2.9.2. Instances of the CPSW Subsystem¶
The TI AM62Px family of devices contain the following instances of the CPSW Ethernet Subsystem:
3.2.2.9.3. TSN Documentation and Testing¶
The CPSW Ethernet Subsystem supports TSN features in the following configurations:
For further details regarding the TSN features and testing, refer TSN with CPSW