3.4.2. Secure Boot

3.4.2.1. Introduction

Each device contains customer programmable keys used to authenticate, and optionally decrypt, code/data to be used on the device. A job for the Public Boot ROM of both General Purpose (GP) and High Security (HS) devices is to load the next stage of the boot process into memory. On High Security devices, Public ROM also checks the initial boot image for an attached header containing details about the image, including a signature used to verify the authorship of the image, and optionally encryption information. This header must be attached and the image must pass authentication for Public Boot ROM to continue boot. It is then the responsibility of the authors to maintain a Chain-of-Trust by ensuring each next stage is itself authenticated. One weak link and all lower trust levels could be compromised.

Note

Example: Forgetting to disable U-Boot console or environment loading means a non-secured linux can be loaded. The U-Boot console (or command line interface (CLI)) and environment are powerful features that make it great for creating a customized boot process. However, leaving either or them enabled in a production system allows non-secured software to be loaded and the Chain-of-Trust to be broken.

The following is an example list where Chain-of-Trust should be maintained.

  • Remove U-Boot uEnv.txt loading support.

  • Disable environment loading (the default built-in environment must be compiled to be the one you want).

  • Environment must not fallback to other boot modes.

  • Place firewalls in board-config to match the location of loaded artifacts (TF-A/OP-TEE).

  • Update debug sections of initial image cert.

  • Enable DM-verity/DM-crypt.

  • Set root password or disable root account.

  • Read the OP-TEE porting guide and turn off developer options

  • Disable kernel debug options

  • Disable/remove userspace debug tools, devmem disable, etc..

The U-Boot’s Secondary Program Loader (SPL) securely verifies the U-Boot proper. U-Boot uses its verified boot framework to do this (See: Secure boot using U-Boot verified boot framework). U-Boot proper then securely verifies and decrypts the kernel, Device Tree Blobs (DTB), and initramfs.

../_images/AM62L_KF.png

Secure boot has layers. Some layers are trusted more than others. Secure ROM has the highest trust and Runtime Execution Environment (REE) non-trustzone user-space applications have the least. If a lower trust entity must load a higher trust code, an even higher trust entity must verify it and not allow access by the lower trust entity after that point. Some such trust inversions are as follows:

  • A53 Public Boot ROM loading TF-A/OP-TEE

  • A53 Public Boot ROM loading TIFS

  • Linux loading Trusted applications (TA)

These are called out in the sequence as shown in the following image and their method of ensuring trust is explained.

3.4.2.2. Secure Boot Flow

../_images/AM62L_BF.png

ROM

On device startup, execution begins with the ROM bootloader (Secure ROM) running on SMS M4 core. After initial device security setup, the Secure ROM starts the Public ROM running on the A53 core. The Public ROM handles loading the first stage image tiboot3.bin from a peripheral as selected by the BOOTMODE pins. This image is placed into on-chip SRAM as external memory interfaces such as DDR are not yet enabled. The exact location is device dependent. More details can be found in the device “Technical Reference Manual”.

The contents of this first stage image are authenticated and decrypted by the Secure ROM. Contents include:

  • Texas Instruments Foundational Security (TIFS) firmware: After authentication/decryption, TIFS firmware replaces the Secure ROM as the authenticator entity executing on the M4 core in the 2nd phase of the boot.

  • BL-1: The pre-bootloader executed on the A53 core, initializes the console and DDR for the 2nd phase of the boot.

A53 SPL

Public ROM loads the second boot stage image tispl.bin from the peripheral as selected by the BOOTMODE pins. From this image, TF-A, OP-TEE, A53 SPL (U-Boot SPL) and SPL DTB are extracted and authenticated and/or decrypted by the Secure ROM. If authenticated, the Secure ROM resets the A53 core. TF-A, OP-TEE and U-Boot SPL begin execution on the A53 core.

U-Boot SPL then loads the U-Boot proper FIT image u-boot.img from the peripheral as selected by the BOOTMODE pins. The U-Boot SPL verifies the signed FIT image independently, without using TIFS. From this FIT image, the U-Boot bootloader and DTB are extracted before passing execution to U-Boot proper.

U-Boot SPL’s output will be similar to this: (notice the “Checking hash(es)” lines as U-Boot and DTB are authenticated).

U-Boot SPL 2026.01-ti-gee3048ee0822 (Apr 09 2026 - 00:09:07 +0000)
SPL initial stack usage: 1936 bytes
Trying to boot from DFU
######DOWNLOAD ... OK
Ctrl+C to exit ...
## Checking hash(es) for config conf-0 ... sha512,rsa4096:custMpk+ OK
## Checking hash(es) for Image uboot ... sha512+ OK
## Checking hash(es) for Image fdt-0 ... sha512+ OK

U-Boot

The boot flow continues as it does on a non-secure device, until loading the next FIT image named fitImage. This FIT image includes the Linux kernel, DTB, and other required boot artifacts. U-Boot verifies the signed images on boot independently, without using TIFS. U-Boot extracts each component from the FIT image and verifies its signature. Once U-Boot verifies all components, it starts Linux. For more information, see: U-Boot FIT Signature Documentation

U-Boot’s output will be similar to this:

U-Boot 2021.01-g2de57d278b (May 16 2022 - 14:28:40 +0000)

SoC:   AM64X SR1.0
Model: Texas Instruments AM642 EVM
Board: AM64-GPEVM rev A
DRAM:  2 GiB
NAND:  0 MiB
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from FAT... *** Warning - bad CRC, using default environment

In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Net:   eth0: ethernet@8000000port@1
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
1011 bytes read in 2 ms (493.2 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
7862647 bytes read in 328 ms (22.9 MiB/s)
## Loading kernel from FIT Image at 90000000 ...
Using 'k3-am642-evm.dtb' configuration
Trying 'kernel@1' kernel subimage
   Description:  Linux kernel
   Type:         Kernel Image
   Compression:  gzip compressed
   Data Start:   0x900000f8
   Data Size:    7743643 Bytes = 7.4 MiB
   Architecture: AArch64
   OS:           Linux
   Load Address: 0x80080000
   Entry Point:  0x80080000
Verifying Hash Integrity ... OK
## Loading fdt from FIT Image at 90000000 ...
Using 'k3-am642-evm.dtb' configuration
Trying 'k3-am642-evm.dtb' fdt subimage
   Description:  Flattened Device Tree blob
   Type:         Flat Device Tree
   Compression:  uncompressed
   Data Start:   0x90762a54
   Data Size:    56436 Bytes = 55.1 KiB
   Architecture: AArch64
   Load Address: 0x83000000
Verifying Hash Integrity ... OK
Loading fdt from 0x90762a54 to 0x83000000
Booting using the fdt blob at 0x83000000
Uncompressing Kernel Image
Loading Device Tree to 000000008ffef000, end 000000008ffff602 ... OK

Linux

If initramfs is included, we can trust our initial modules and tasks, but we cannot trust anything beyond this as the root file-system may have been modified. To allow trusted use of files outside of our initramfs we use dm-verity. With this we can authenticate a block device as we read from it. As any changes to this block-device will cause the authentication to fail, we cannot put any user-modifiable configurations or user installed programs here. Only important, read-only, files should be placed on this partition, such as static kernel and operating system files and configurations. All other files must be placed in a non-verifiable read/write user partition.

3.4.2.3. HS Boot Flow Tools

U-Boot:

The ti-u-boot source is a project used to create tiboot3.bin, tispl.bin, and u-boot.img. To create tiboot3.bin for K3 family devices, U-Boot builds BL-1 and binman packages it in a tiboot3.bin image. To build A53 SPL, binman takes TF-A (bl31.bin), OPTEE (bl32.bin), A53 SPL, and A53 DTBs and packages them in a tispl.bin image. U-Boot can then use the openssl library to sign each component as specified in k3-am62l3-evm-binman.dtsi.

$ git clone https://git.ti.com/git/ti-u-boot/ti-u-boot.git

$ # Example use:
$ make ARCH=arm CROSS_COMPILE=aarch64-none-linux-gnu- am62lx_evm_defconfig
$ make CROSS_COMPILE=aarch64-none-linux-gnu- BL1=bl1.bin BL31=bl31.bin TEE=tee-pager_v2.bin BINMAN_INDIRS=<path-to-tisdk>/board-support/prebuilt-images

Linux:

The ti-linux source is a TI project used to build Linux kernel, DTB, and other boot artifacts. Some of these components could be included in a verifiable image fitImage. For HS devices, only the fitImage will be allowed to boot once fitImage has been authenticated.

$ git clone https://git.ti.com/git/ti-linux-kernel/ti-linux-kernel.git

$ #Example use:
$ make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- defconfig ti_arm64_prune.config
$ make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- menuconfig
$ make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu-

TF-A:

The TF-A source (formerly called ATF) is used to build bl31.bin that gets packaged into tispl.bin. For HS devices, this binary needs to be signed.

$ git clone https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git

$ # Example use:
$ make ARCH=aarch64 CROSS_COMPILE=aarch64-none-linux-gnu- PLAT=k3 TARGET_BOARD=lite SPD=opteed

OPTEE:

The OPTEE source is used to build bl32.bin/tee-pager_v2.bin that gets packaged into tispl.bin. For HS devices, this binary needs to be signed.

$ git clone https://github.com/OP-TEE/optee_os.git

$ # Example use:
$ make CROSS_COMPILE64=aarch64-linux-gnu- PLATFORM=k3-<soc> CFG_ARM64_core=y

Ti-linux-firmware:

The ti-linux-firmware is a TI repository where all firmware releases are stored. Firmwares for a device family can also be found in the pre-built SDK under <path-to-tisdk>/board-support/prebuilt-images/<evm>. Binman expects to find the device firmware with the following appended to U-Boot build command: BINMAN_INDIRS=<path-to-tisdk>/board-support/prebuilt-images, and expects to find a ti-sysfw directory in this path.

$ git clone https://git.ti.com/git/processor-firmware/ti-linux-firmware.git
Branch: ti-linux-firmware.