3.1.1.1. Setup

3.1.1.1.1. Install host dependencies

To install host dependencies for building TI U-boot source (standalone) on Ubuntu 22.04+, run the following command in the terminal prompt:

sudo apt install git xz-utils build-essential autoconf flex bison libssl-dev bc libncurses-dev \
python3 python3-setuptools python3-dev python3-yaml python3-jsonschema python3-pyelftools \
swig yamllint libgnutls28-dev

Note

The recommended host machine for building U-Boot is Ubuntu 22.04. Users of Ubuntu 18.04 might need to install Python 3.7 or later. If using the default Python 3.6 that is in Ubuntu 18.04, users might need to install these additional dependencies:

pip install dataclasses pyelftools jsonschema yamllint importlib-resources

3.1.1.1.2. Getting the Source Code

Note

AM62L devices use TF-A BL-1 boot loader to configure LPDDR4 to enable secondary program loader.

The easiest way to get access to the source code is by downloading and installing the Processor SDK Linux. Once installed, the source code is in the SDK at the path <path to tisdk>/board-support. For your convenience the sources also includes git repositories including commit history.

U-Boot sources can also be directly fetched from GIT. The GIT repository URL, branch and commit id is available in Build Information.

3.1.1.1.3. Setup Cross Compile Environment

The cross compile version supported in this release can be found in the release notes for the kernel release.

Before compiling any of the sources referenced in this document, set the cross compiler paths to the toolchains packaged in the Processor SDK [Recommended] as shown below. Refer to Yocto-built SDK Toolchains section for more details on usage.

host# export CROSS_COMPILE_64="${SDK_INSTALL_DIR}/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/aarch64-oe-linux/aarch64-oe-linux-"
host# export SYSROOT_64="${SDK_INSTALL_DIR}/linux-devkit/sysroots/aarch64-oe-linux"
host# export CC_64="${CROSS_COMPILE_64}gcc --sysroot=${SYSROOT_64}"
host# export CFLAGS64="--sysroot=${SYSROOT_64}"
host# export KCFLAGS="--sysroot=${SYSROOT_64}"
host# export LDFLAGS="--sysroot=${SYSROOT_64}"

If the Processor SDK is not installed, the Arm GNU toolchains can be downloaded and setup. Refer to ARM toolchains section for more details on usage.