4.1.3. How to flash eMMC and boot from eMMC UDA
4.1.3.1. Overview
This how to guide allows to prepare and flash the embedded multimedia card (eMMC) device to boot using MMCSD boot, from eMMC UDA in filesystem (FS) mode.
Note
This process will require a working (secure digital) SD card that can boot the device to Linux kernel.
4.1.3.2. Flash eMMC with disk image
Copy the .wic formatted disk image from the SDK installer to target filesystem, boot the device via SD card boot and at Linux prompt, find the eMMC block device as shown here and flash the eMMC as shown below:
root@<machine>:~# ls
tisdk-base-image-<soc>-evm.rootfs.wic.xz
root@<machine>:~# xz -d -k tisdk-base-image-<soc>-evm.rootfs.wic.xz
root@<machine>:~# ls
tisdk-base-image-<soc>-evm.rootfs.wic tisdk-base-image-<soc>-evm.rootfs.wic.xz
root@<machine>:~# umount /dev/mmcblk0*
root@<machine>:~# dd if=tisdk-base-image-<soc>-evm.rootfs.wic of=/dev/mmcblk0
4.1.3.3. Manually flash eMMC device
To boot with MMCSD boot from eMMC UDA in FS mode, the eMMC needs to be prepared before hand.
The recommended process is to flash an SD card with TI SDK image, copy the boot loader binaries
that will be flashed to eMMC in the SD card “boot” partition in emmc/
folder, boot the
board with MMCSD boot from SD (FS mode), and proceed to create disk partitions and flash the
eMMC from Linux.
Create disk partitions
In Linux, create a “boot” partition to store boot loader binaries as shown here and a “root” partition for the foot filesystem (rootfs): as shown here.
Format partitions
For the “boot” partition, format as vfat type as shown here and for the “root” partition, format as ext4 type as shown here.
Flash eMMC UDA
Mount the new “boot” partition and copy the boot loader binaries to the new partition as shown here. Mount the new “root” partition and copy the rootfs to the partition as shown here
4.1.3.4. MMCSD boot configuration from eMMC UDA
Now that we have flashed the eMMC device, reboot the board and stop at u-boot prompt to set configuration for MMCSD boot from UDA.
Enable boot from eMMC UDA
After flashing binaries to eMMC flash, the eMMC device Extended CSD register fields: BUS_WIDTH and PARTITION_CONFIG must be set so ROM will use the correct configuration for MMCSD boot from UDA.
Set by using the mmc bootbus and mmc partconf commands. Go to
Boot from UDA
.
The mmc bootbus command sets the BOOT_BUS_WIDTH field where
mmc bootbus 0 2 0 0
selects x8 (sdr/ddr) buswidth in boot operation mode.The mmc partconf command can be used to configure what hardware partition to boot from. The general syntax is:
$ mmc partconf <dev> [[varname] | [<boot_ack> <boot_partition> <partition_access>]]
Where <dev> is MMC device index.
For more information on these commands, go here.
Boot from UDA
=> mmc partconf 0 1 7 1
=> mmc bootbus 0 2 0 0
Enable warm reset
On eMMC devices, warm reset will not work if EXT_CSD[162] bit is unset since the reset input signal will be ignored. Warm reset is required to be enabled in order for the eMMC to be in a “clean state” on power-on reset so that ROM can do a clean enumeration. To set the EXT_CSD[162] bit, stop at u-boot prompt and run the following command:
=> mmc rst-function 0 1
Warning
This is a write-once field. For more information, refer to the u-boot doc found here.
U-boot environment
The command saveenv is no longer used in TI SDK, thus, the following environment workarounds must be implemented to boot from eMMC UDA.
At u-boot prompt, run the following commands to boot Linux from UDA:
=> setenv mmcdev 0
=> setenv bootpart 0:2
=> boot
Or change the u-boot environment for MMCSD boot to boot completely from eMMC.
First apply the following change in u-boot for any SoC.
diff --git a/board/ti/<soc>/<soc>.env b/board/ti/<soc>/<soc>.env
index 82b9f0741bb..73d59ac425c 100644
--- a/board/ti/<soc>/<soc>.env
+++ b/board/ti/<soc>/<soc>.env
@@ -17,8 +17,8 @@ run_kern=booti ${loadaddr} ${rd_spec} ${fdtaddr}
boot_targets=mmc1 mmc0 usb pxe dhcp
boot=mmc
-mmcdev=1
-bootpart=1:2
+mmcdev=0
+bootpart=0:2
bootdir=/boot
rd_spec=-
Re-build boot loader binaries and copy build outputs to the SD card “boot” partition
and emmc/
folder. Proceed to flash eMMC with these binaries as shown in this
step-by-step guide.
4.1.3.5. Boot from eMMC UDA
Finally we can proceed to change boot mode pins to MMCSD boot from eMMC (port 0) in FS
mode according to TRM, under: Initialization/Boot Mode Pins
and power cycle the
board.