3.6.3. Flash via Fastboot

This application note provides instructions on using Snagfactory tool for flashing.

The Snagfactory tool has two main operations:

  • Snagrecover: Boots the board (recovery) using USB DFU.

  • Snagflash: Flashes binaries to the on-board memory using the Fastboot protocol.

This tool supports flashing multiple boards simultaneously, enhancing efficiency in producion enviroment.

3.6.3.1. Installing Snagfactory

  • Snagfactory tool is hosted here Snagfactory.

  • More info about installation can be found in Snagfactory Readme.

  • Snagfactory also is available on pip.

$ python3 -m pip install --user snagboot
$ python3 -m pip install --user snagboot[gui]

Note

At the time of 11.1 release, the corresponding Snagfactory version was v2.3.

3.6.3.2. Building bootloader binaries for Recovery

For Snagrecover, bootloader images must support DFU boot and fastboot download. In addition to USB DFU fragment config (which enables DFU boot) for the u-boot build, an additional fragment config am6x_a53_snagfactory.config needs to be used, which enables fastboot support in U-Boot and other required configs for snagfactory.

To build bootloader images for recovery using SDK, following change is needed in Rules.make file present in the top level of Linux SDK Installer.

UBOOT_MACHINE_R5=am62ax_evm_r5_defconfig am62x_r5_usbdfu.config

UBOOT_MACHINE_A53=am62ax_evm_a53_defconfig am62x_a53_usbdfu.config am6x_a53_snagfactory.config

Generate the bootloader images using top-level makefile by running following commands on the terminal from the top-level of the Linux SDK installer.

$ make u-boot_clean
$ make u-boot
$ make u-boot_stage

Save the bootloader binaries generated in a separate directory. These bootloader images will be used for recovery and to start flashing the images. The bootloader images after make can be found in board-support/built-images.

For more details regarding USB DFU refer USB Device Firmware Upgrade (DFU).

Note

CONFIG_FASTBOOT_BUF_SIZE is defined in am6x_a53_snagfactory.config and specifies the maximum buffer size for flashing files. Its value must be equal or greater than the largest file size being flashed. If smaller, non-sparse images will not flash correctly due to issues with chunked processing.

3.6.3.3. Connections

  • Power off the EVM and set up the boot mode switches to boot from USB DFU.

SW2-11001100
SW3-00000000
  • Power on the board.

  • Optionally you can also connect host PC to board via UART to read the console logs.

3.6.3.3.1. How to use Snagfactory

Comprehensive instructions for installation of the Snagfactory tool are here:

SnagFactory GUI Tool Configuration and Device Flashing Procedure

The tool currently supports MMC and MTD backends for flashing images.

Note

SnagFactory GUI tool is a prerequisite for this procedure.

The following steps outline the process for configuring and flashing a device by using the SnagFactory GUI tool.

../../../_images/snagfactory.png

Step 1: Launch SnagFactory GUI Tool

  • Launch the SnagFactory GUI tool to begin the configuration and device flashing process.

$ snagfactory

Step 2: Select Configuration File Option

  • Upon launch, the SnagFactory GUI tool will present the option to add a configuration file. Select the conf option to proceed with loading the configuration file.

Step 3: Load YAML Configuration File

  • Load the YAML configuration file for the platform. This file has the necessary settings and parameters for the device flashing process.

Step 4: Flash the Device

  • Once you load the YAML configuration file, the SnagFactory GUI tool will flash the device with the specified configuration.

The example configuration files for emmc and ospi-nand and ospi-nor are as follows.

For reference, the ospi-nor.yaml file for am62p platform can be as follows:

boards:
  0451:6165: am62p
soc-models:
  am62p-firmware:
    tiboot3:
      path: "<path_to_boot_binaries>/tiboot3.bin"
    tispl:
      path: "<path_to_boot_binaries>/tispl.bin"
    u-boot:
      path: "<path_to_boot_binaries>/u-boot.img"
  am62p-tasks:
  - eraseblk-size: 0x40000
    fb-buffer-addr: 0x82000000
    fb-buffer-size: 0x7000000
    target-device: nor0
  - task: run
    args:
      - "oem_run:mtd list"
      - "oem_run:setenv mtdids nor0=nor0"
  - task: mtd-parts
    args:
      - name: ospi.tiboot3
        size: 0x80000
      - name: ospi.tispl
        size: 0x200000
      - name: ospi.u-boot
        size: 0x400000
  - task: flash
    args:
      - image: "<path_to_flash_binaries>/tiboot3.bin"
        part: ospi.tiboot3
      - image: "<path_to_flash_binaries>/tispl.bin"
        part: ospi.tispl
      - image: "<path_to_flash_binaries>/u-boot.img"
        part: ospi.u-boot

For reference, the ospi-nand.yaml file for am62xx-lp platform can be as follows:

boards:
  0451:6165: am625
soc-models:
  am625-firmware:
    tiboot3:
      path: "<path_to_boot_binaries>/tiboot3.bin"
    tispl:
      path: "<path_to_boot_binaries>/tispl.bin"
    u-boot:
      path: "<path_to_boot_binaries>/u-boot.img"
  am625-tasks:
  - eraseblk-size: 0x40000
    fb-buffer-addr: 0x82000000
    fb-buffer-size: 0x7000000
    target-device: spi-nand0
  - task: run
    args:
      - "oem_run:mtd list"
      - "oem_run:setenv mtdids spi-nand0=spi-nand0"
  - task: mtd-parts
    args:
      - name: ospi_nand.tiboot3
        size: 0x80000
      - name: ospi_nand.tispl
        size: 0x200000
      - name: ospi_nand.u-boot
        size: 0x400000
      - name: ospi_nand.env
        size: 0x40000
      - name: ospi_nand.env.backup
        size: 0x40000
      - name: ospi_nand.rootfs
        size: 0x5fc0000
        start: 0x2000000
      - name: ospi_nand.phypattern
        start: 0x7fc0000
        size: 0x40000
  - task: flash
    args:
      - image: "<path_to_flash_binaries>/tiboot3.bin"
        part: ospi_nand.tiboot3
      - image: "<path_to_flash_binaries>/tispl.bin"
        part: ospi_nand.tispl
      - image: "<path_to_flash_binaries>/u-boot.img"
        part: ospi_nand.u-boot

For reference, the emmc.yaml file for am62p platform can be as follows:

boards:
  "0451:6165": "am62p"
soc-models:
  am62p-firmware:
      tiboot3:
        path: "<path_to_boot_binaries>/tiboot3.bin"
      tispl:
        path: "<path_to_boot_binaries>/tispl.bin"
      u-boot:
        path: "<path_to_boot_binaries>/u-boot.img"
  am62p-tasks:
    - target-device: mmc0
      fb-buffer-addr: 0x82000000
      fb-buffer-size: 0x7000000
    - task: gpt
      args:
        - name: rootfs
          size: 1G
    - task: reset
    - task: flash
      args:
        - image: "<path_to_flash_binaries>/tiboot3.bin"
          image-offset: 0x0
          part: "hwpart 1"
        - image: "<path_to_flash_binaries>/tispl.bin"
          image-offset: 0x80000
          part: "hwpart 1"
        - image: "<path_to_flash_binaries>/u-boot.img"
          image-offset: 0x280000
          part: "hwpart 1"
        - image: "<path_to_flash_binaries>/rootfs.ext4"
          part: "rootfs"

Snagboot Command-line Configuration and Device Flashing Procedure

Snagrecover uses vendor-specific ROM code mechanisms to initialize external RAM and run U-Boot, without modifying any non-volatile memories.

$ snagrecover -s am625 -F "{'tiboot3': {'path': 'tiboot3.bin'}}" -F "{'tispl': {'path': 'tispl.bin'}}" -F "{'u-boot': {'path': 'u-boot.img'}}"

Snagflash communicates with U-Boot to flash system images to non-volatile memories, using either DFU, UMS or Fastboot.

$ snagflash -P fastboot-uboot -p 0451:6165 -i