3.3.3. CPUIdle

Overview

The cpuidle framework consists of two key components:

A governor that decides the target C-state of the system. A driver that implements the functions to transition to target C-state. The idle loop is executed when the Linux scheduler has no thread to run. When the idle loop is executed, current ‘governor’ is called to decide the target C-state. Governor decides whether to continue in current state/ transition to a different state. Current ‘driver’ is called to transition to the selected state.

Standby Mode

On AM62Ax platforms, “Standby” mode is implemented through the Linux CPUIdle framework. Standby is the default low-power state that the system enters automatically when idle, using the WFI (Wait For Interrupt) C-state. This power-saving mechanism activates whenever the system is “just sitting idle” without requiring any special configuration or activation from the user.

When your device appears inactive, it is actually cycling in and out of this standby state many times per second, seamlessly managing power while remaining responsive.

Enable Standby

In order to enable Standby the k3-am62x-sk-lpm-standby.dtso overlay should be applied. Refer to How to enable DT overlays for more details. More information on what the overlay does is in the Linux Device Tree Implementation section.

Standby Implementation Architecture

For AM62Ax, the Standby implementation involves a multi-layer architecture:

  1. Linux CPUIdle Framework: - Determines when to place CPUs into idle states based on system activity - Uses governors (like the menu governor) to predict how long CPUs will be idle - Invokes platform-specific drivers to transition to appropriate C-states

  2. ARM Generic CPUIdle Driver: - Implements the Linux CPUIdle driver interface for ARM platforms - Communicates with TF-A through PSCI SMC (Secure Monitor Call) interface

  3. PSCI Interface in Linux: - Provides a standardized method for the kernel to request power management operations - Translates Linux-side requests into PSCI calls to TF-A

  4. TF-A PSCI Implementation: - Runs in secure world (EL3) - Implements the PSCI specification - Provides platform-specific handlers via the plat_psci_ops structure

When your system goes idle, the following sequence occurs:

  • Linux idle loop detects no runnable tasks

  • CPUIdle governor selects the appropriate C-state (“stby” for these platforms)

  • CPUIdle driver communicates with TF-A via the PSCI interface

  • TF-A’s PSCI implementation validates the requested power state through validate_power_state()

  • TF-A executes the cpu_standby() handler from plat_psci_ops

  • The actual WFI instruction is executed within the TF-A’s standby handler

  • On interrupt: CPU automatically exits WFI state

  • Control returns to Linux

This automated process happens continuously during system operation, seamlessly transitioning between active and idle states to save power whenever possible.

Standby vs. Deep Sleep: Understanding the Difference

It’s important to distinguish between the lightweight “standby” provided by CPUIdle and deeper sleep states:

  • CPUIdle Standby (WFI): - Processor-level power saving only - Very fast entry and exit (microseconds) - Occurs automatically hundreds of times per second - No user intervention required - All peripherals remain operational - Perfect for normal “idle” periods

  • Deep Sleep Modes: - System-wide power saving - Slower entry and exit (milliseconds to seconds) - Requires explicit software requests - May require peripheral reconfiguration - Suitable for extended inactive periods

Source Location

Linux Side:

  • drivers/cpuidle/cpuidle-arm.c - ARM CPU idle driver

  • drivers/cpuidle/dt_idle_states.c - Device tree parsing for idle states

  • drivers/cpuidle/cpuidle.c - Core CPUIdle framework

  • kernel/sched/idle.c - Kernel idle loop implementation

  • drivers/firmware/psci.c - PSCI interface to TF-A

TF-A Side (not part of Linux kernel):

  • plat/ti/k3/common/k3_psci.c - PSCI implementation for K3 platforms

Linux Device Tree Implementation

In order to implement Standby in Linux, an idle-states node has to be added and then referenced by the CPU node. The k3-am62x-sk-lpm-standby.dtso can be used as a reference.

idle-states {
         entry-method = "psci";

         CPU_SLEEP_0: stby {
                 compatible = "arm,idle-state";
                 idle-state-name = "standby";
                 arm,psci-suspend-param = <0x00000001>;
                 entry-latency-us = <100>;
                 exit-latency-us = <50>;
                 min-residency-us = <1000>;
         };
 };

The entry-latency-us, exit-latency-us, and min-residency-us properties are explained in depth here. The min-residency-us can be fine tuned to change the minimum amount of time Linux is in idle which can change the power savings.

Driver Usage

CPUIdle works automatically once enabled in the kernel, with no user intervention required. The CPUIdle framework statistics can be accessed through the sysfs interface:

# ls -l /sys/devices/system/cpu/cpu0/cpuidle/
drwxr-xr-x    2 root     root             0 Jan  1 00:01 state0
drwxr-xr-x    2 root     root             0 Jan  1 00:01 state1

# ls -l /sys/devices/system/cpu/cpu0/cpuidle/state1/
-r--r--r--    1 root     root         4096 Jan  1 00:02 desc
-r--r--r--    1 root     root         4096 Jan  1 00:02 latency
-r--r--r--    1 root     root         4096 Jan  1 00:02 name
-r--r--r--    1 root     root         4096 Jan  1 00:02 power
-r--r--r--    1 root     root         4096 Jan  1 00:02 time
-r--r--r--    1 root     root         4096 Jan  1 00:02 usage

To view the current C-state statistics:

# cat /sys/devices/system/cpu/cpu0/cpuidle/state1/name
stby
# cat /sys/devices/system/cpu/cpu0/cpuidle/state1/usage
6245738