10. ROS-GST Plugins

TI ROS-GST plugins provides an optimized bridge between ROS 2 and GStreamer framework.

10.1. Build Plugins

Please follow the LINK to setup Docker for ROS 2 on the target.

Once the Docker setup is done on target, use the following to build the GStreamer plugins.

root@docker:~/j7ros_home/ros_ws$ colcon build --base-paths /opt/robotics_sdk/ros2 --packages-select ti_ros_gst_plugins --cmake-force-configure

The libraries for the plugins can be found under $COLCON_PREFIX_PATH/ti_ros_gst_plugins/

10.2. Inspect Plugins

Inspect all available ROS-GST plugins

root@docker: gst-inspect-1.0 $COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins/libros_gst_plugins.so

Inspect specific ROS-GST plugins

root@docker: gst-inspect-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins/ tirosimgsrc

10.3. Plugins

10.3.1. tirosimgsrc

This plugin can subscribe to ROS Image or CompressedImage(jpeg) topic and put the received msg to GStreamer or TIOVX buffer.

There are two ways to define caps for the plugin

  • Explicitly define caps as property, shown in example below (This is necessary for CompressedImage(jpeg) msg)

  • Let first ROS msg set the caps automatically (Works only for Image msg)

You can use example rosbag file provided to publish msg, or you can you any other source

root@docker: ros2 bag play $WORK_DIR/data/ros_bag/zed1_2020-11-09-18-01-08/ --loop --topic /camera/left/image_raw

In another terminal run the pipeline to receive the msg being published to the topic.

# tirosimgsrc->display

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins/ tirosimgsrc ros-topic=/camera/left/image_raw caps="video/x-raw,width=1280,height=720,format=UYVY" ! kmssink driver-name=tidss sync=false
# tirosimgsrc->AI->display

root@docker: export MODEL_DIR=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416/

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins/ \
tirosimgsrc ros-topic=/camera/left/image_raw ! tiovxdlcolorconvert ! video/x-raw,format=NV12 ! tiovxmultiscaler name=split_01 \
\
split_01. ! queue ! tiovxdlpreproc model=$MODEL_DIR out-pool-size=4 ! application/x-tensor-tiovx ! tidlinferer target=1  model=$MODEL_DIR ! post_0.tensor \
\
split_01. ! queue ! video/x-raw, width=1280, height=720 ! post_0.sink \
\
tidlpostproc name=post_0 model=$MODEL_DIR viz-threshold=0.5 display-model=true ! queue ! mosaic_0. \
\
tiovxmosaic name=mosaic_0 target=1 \
src::pool-size=4 sink_0::startx="<320>" sink_0::starty="<150>" sink_0::widths="<1280>" sink_0::heights="<720>" \
! video/x-raw,format=NV12, width=1920, height=1080 ! queue ! tiperfoverlay ! kmssink driver-name=tidss sync=false

10.3.2. tirossink

This plugin can publish specific ROS msg based on sink caps from gst pipeline. You can also specify optional property ros-msg-type. If not define, the plugin will pick appropriate message type based on the caps automatically.

Currently supported msgs:

  • sensor_msgs/Image

  • sensor_msgs/CompressedImage

  • std_msgs/String

  • custom_msgs/Detection2D

10.3.2.1. sensor_msgs/Image

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins/ videotestsrc ! video/x-raw,width=1280,height=720,format=NV12,framerate=30/1 ! tirossink ros-topic=image_raw

10.3.2.2. sensor_msgs/CompressedImage

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins/ videotestsrc ! video/x-raw,width=1280,height=720,format=NV12,framerate=30/1 ! jpegenc ! image/jpeg ! tirossink ros-topic=image_jpeg
root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins/ videotestsrc ! video/x-raw,width=1280,height=720,format=NV12,framerate=30/1 ! pngenc ! image/png ! tirossink ros-topic=image_png

10.3.2.3. std_msgs/String

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins/ multifilesrc location=x.txt ! text/x-raw ! tirossink ros-topic=string

10.3.2.4. custom_msgs/Detection2D

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins v4l2src device=/dev/video-usb-cam0 io-mode=2 ! image/jpeg, width=1280, height=720 ! jpegdec ! \
tiovxdlcolorconvert ! video/x-raw, format=NV12 ! \
tiovxmultiscaler ! video/x-raw, width=416, height=416 ! \
tiovxdlpreproc model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416  out-pool-size=4 ! application/x-tensor-tiovx ! \
tidlinferer target=1  model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416 ! post_0.tensor \
tidlpostproc name=post_0 model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416 viz-threshold=0.6 \
\
post_0.text ! queue ! text/x-raw ! tirossink ros-topic=Det2D ros-msg-type=detection2d

10.3.2.5. custom_msgs/Detection2D & sensor_msgs/Image

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins v4l2src device=/dev/video-usb-cam0 io-mode=2 ! image/jpeg, width=1280, height=720 ! jpegdec ! \
tiovxdlcolorconvert ! video/x-raw, format=NV12 ! \
tiovxmultiscaler name=split_01 \
split_01. ! queue ! video/x-raw, width=416, height=416 ! \
tiovxdlpreproc model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416  out-pool-size=4 ! application/x-tensor-tiovx ! \
tidlinferer target=1  model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416 ! post_0.tensor \
\
split_01. ! queue ! video/x-raw, width=1280, height=720 ! \
post_0.sink \
\
tidlpostproc name=post_0 model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416 viz-threshold=0.6 \
\
post_0.src ! queue ! video/x-raw ! tirossink ros-topic=Image ros-msg-type=image \
post_0.text ! queue ! text/x-raw ! tirossink ros-topic=Det2D ros-msg-type=detection2d

10.3.2.6. custom_msgs/Detection2D & sensor_msgs/CompressedImage

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins v4l2src device=/dev/video-usb-cam0 io-mode=2 ! image/jpeg, width=1280, height=720 ! jpegdec ! \
tiovxdlcolorconvert ! video/x-raw, format=NV12 ! \
tiovxmultiscaler name=split_01 \
split_01. ! queue ! video/x-raw, width=416, height=416 ! \
tiovxdlpreproc model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416  out-pool-size=4 ! application/x-tensor-tiovx ! \
tidlinferer target=1  model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416 ! post_0.tensor \
\
split_01. ! queue ! video/x-raw, width=1280, height=720 ! \
post_0.sink \
\
tidlpostproc name=post_0 model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416 viz-threshold=0.6 \
\
post_0.src ! queue ! video/x-raw ! jpegenc ! tirossink ros-topic=CompressedImage ros-msg-type=compressed-image-jpeg \
post_0.text ! queue ! text/x-raw ! tirossink ros-topic=Det2D ros-msg-type=detection2d

10.4. Example AI pipeline

[SK] On the target,

root@docker: gst-launch-1.0 --gst-plugin-path=$COLCON_PREFIX_PATH/ti_ros_gst_plugins/lib/ti_ros_gst_plugins v4l2src device=/dev/video-usb-cam0 io-mode=2 ! image/jpeg, width=1280, height=720 ! jpegdec ! \
tiovxdlcolorconvert ! video/x-raw, format=NV12 ! tee name=tee_split \
\
tee_split. ! queue ! tirossink ros-topic=camera/image_rect_nv12 \
\
tee_split. ! queue ! tiovxmultiscaler ! video/x-raw, width=416, height=416 ! \
tiovxdlpreproc model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416  out-pool-size=4 ! application/x-tensor-tiovx ! \
tidlinferer target=1  model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416 ! post_0.tensor \
tidlpostproc name=post_0 model=/opt/model_zoo/ONR-OD-8200-yolox-nano-lite-mmdet-coco-416x416 viz-threshold=0.6 \
\
post_0.text ! queue ! text/x-raw ! tirossink ros-topic=vision_cnn/tensor ros-msg-type=detection2d

[Visualization on Ubuntu PC]

ros2 launch ti_viz_nodes rviz_objdet_cnn_launch.py width:=1280 height:=720 approx_time_sync:=True