2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM62A installer provides everything needed as discussed below to create the embedded system from “scratch” :
- Platform/board-support software and configuration files for Linux
- U-Boot and Kernel sources and configuration files
- An ARM cross-compiling toolchain as well as other host binaries and components
- A Yocto/OE compliant filesystem and sources for example applications
- A variety of scripts and Makefiles to automate certain tasks
- Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
- Reference Examples, benchmarks
2.1.2. Licensing¶
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
- Linux Manifest: “/docs/software_manifest.html”
2.1.3. Release 08.06.00¶
Released on February 2023
2.1.3.1. What’s new¶
Processor SDK Linux AM62A Release has following new features:
- AM62A: Initial Platform Support (GP, HS-FS, HS-SE with default Boot Experience on HS-FS)
- U-Boot: OSPI NAND with UBIFS, C7x and R5 Early boot, DFU Flashing, QoS Optimization for DSS and CSI load
- ATF: v2.8+
- Kernel: SD/eMMC, SDIO, GPIO, OSPI NAND, USB host and device mode, CSI Support with OV5640, IMX219, IMX390 and OV2312 Sensors, RTC, ePWM, CPSW 3G, IPC R5, IPC C7x, Mailbox, HWspinlock, VPU, SA3UL, Display( HDMI), Wave521 Video Encode and Decode, McASP audio output and capture, MCRC
2.1.4. Build Information¶
2.1.4.1. U-Boot¶
u-boot
2.1.4.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
2.1.4.3. Yocto¶
meta-processor-sdk
meta-ti
meta-arago
2.1.5. Issues Tracker¶
2.1.5.1. Linux Known Issues¶
Record ID | Title | Platform | Workaround |
---|---|---|---|
LCPD-29423 | AM62A: OV2312: Occassional IR frames in RGB channel | am62axx_sk-fs | PR with a workaround has been opened, Contacted sensor manufacturer for root-cause and proper fix. |
LCPD-28950 | CSI2 Multi-capture channel 0 not working | am62axx_sk-fs | |
LCPD-29589 | AM62x CPSW: PPS example not enabled by default | am62axx_sk-fs | |
LCPD-32459 | am62a Intermittent Boot Failure on RT-Linux | am62axx_sk-fs | |
LCPD-24456 | Move IPC validation source from github to git.ti.com | am62axx_sk-fs | |
LCPD-32356 | AM62x: tcrypt doesn’t use sa2ul for SHA256/512 or any other alg | am62axx_sk-fs | |
LCPD-29588 | CPSW documentation: Time Sync Router no longer firewalled | am62axx_sk-fs | |
LCPD-28672 | CPSW: Add more details about driver config | am62axx_sk-fs | |
LCPD-32790 | AM62A: VPU: Module load/unload in loop fails after bootup | am62axx_sk-fs | |
LCPD-32728 | AM62x, AM62a: Doc: Update HS FS Migration Guide | am62axx_sk-fs,am62axx_sk-se | |
LCPD-32353 | SBL remote core images does not fit the partition table defined by LINUX for serial NAND | am62axx_sk-fs | |
LCPD-29113 | Test gap: Linux support for CSI2 virtual channel/multiple camera support | am62axx_sk-fs | |
LCPD-32793 | Continous noise heard while playing audio file on am62a SK board | am62axx_sk-fs | |
LCPD-32344 | AM62: McASP recording causes CPU freezes | am62axx_sk-fs | |
LCPD-29943 | AM64x: Upstream: Add boot mode switch settings | am62axx_sk-fs,am62axx_sk-se |