2.3. Yocto Layer Configuration

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>


The following config files are located in the yocto-build/configs/processor-sdk-linux directory.

Config File

Description

Supported machines

processor-sdk-linux-11_01_02_01.txt

Processor SDK Linux 11_01 Release

am57xx-evm, am57xx-hs-evm