2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the configs/
directory of the configs directory. The yocto config can also be
downloaded directly from the SDK release page.
Config File | Description | Supported machines |
---|---|---|
psdkla-07_01_00.txt | Processor SDK Linux 07_01_00 Release | j7-evm, j7200-evm, am65xx-evm |