2.3. Yocto Layer Configuration

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>

The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.

Config File

Description

Supported machines/platforms

processor-sdk-scarthgap-11.02.05.02-config.txt

Processor SDK 11.02.05.02 Release

am335x-evm, am437x-evm, am65xx-hs-evm

processor-sdk-scarthgap-11.02.08.02-config.txt

Processor SDK 11.02.08.02 Release

am64xx-evm, am62xx-evm, am62xx-lp-evm, am62xxsip-evm, am62lxx-evm, am62pxx-evm, am62dxx-evm