3.1.2.4. SD, eMMC and USB
The following guide shows how to flash and boot from storage media like the embedded multimedia card (eMMC), secure digital (SD) card, and USB storage devices. While this is a step-by-step guide, it is in no way extensive and does not cover all the per-platform corner-cases. For any issues/questions on this guide, please reach out to: Help e2e.
3.1.2.4.1. MMC
3.1.2.4.1.1. Listing MMC devices
Usually in all the platforms there will be one or two MMC instances of which one would be SD and the other would be eMMC. The index of them can vary from one class of platforms to the other. For a given platform, the device number: mmcdev=[0:1] can be found in the following way:
=> mmc list
OMAP SD/MMC: 0 (SD)
The device number “0” is for SD, here eMMC is not enumerated.
3.1.2.4.1.2. Selecting MMC device and paritions
To selct an MMC device in u-boot, the command: mmc dev could be used. The general syntax is:
=> mmc dev [dev] [partition]
The following lists examples and their explanation for each MMC device and partitions according to the example in: Listing MMC devices.
=> mmc dev 0 # select SD
3.1.2.4.1.3. View MMC partition contents
This section assumes an SD card or eMMC was prepared previously to boot the device.
Note
For eMMC, typically, the device ships without a partition table If there is a need to create a partition in UDA (to flash the rootfs), please go to: create partition in UDA and format the partition: formatting eMMC partition before proceeding to look at the eMMC partition contents.
To verify partitions in any MMC device from u-boot prompt, use the command: mmc part. If the partitions are formatted with a file system type that is supported by u-boot, you can view the contents of the MMC partition as show below:
=> ls mmc 0:1
7700992 zImage
112421 am437x-idk-evm.dtb
118979 am437x-sk-evm.dtb
122333 am43x-epos-evm.dtb
extlinux/
158859 MLO
814184 u-boot.img
717 uEnv.txt
84299 am437x-gp-evm.dtb
8 file(s), 1 dir(s)
=> ls mmc 0:2 boot
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 4096 dtb
7700992 zImage
Where the general syntax is:
$ ls <interface> [<dev[:partition]> [directory]]
3.1.2.4.1.4. Flash and boot SPL from eMMC
In some cases it is desirable to write MLO and u-boot.img
as raw images to the MMC device rather than load them from a filesystem.
In that case, the command mmc write can be used to flash
the MMC device.
In this example, mmc dev 0 selects an eMMC device that was enumerated. In
the following example, flash the eMMC boot0 HW partition, loading the binaries from
SD and assuming the files: MLO and u-boot.img exist on the SD card
first (boot) partition:
=> mmc dev 0
=> mmc rescan
=> mmc dev 1 1
=> fatload mmc 0 ${loadaddr} MLO
=> mmc write ${loadaddr} 0x0 0x300
=> fatload mmc 0 ${loadaddr} u-boot.img
=> mmc write ${loadaddr} 0x300 0x400
To flash the eMMC boot0 HW partition from network tftp:
=> setenv autoload no
=> dhcp
=> mmc dev 1 1
=> tftp ${loadaddr} MLO
=> mmc write ${loadaddr} 0x0 0x300
=> tftp ${loadaddr} u-boot.img
=> mmc write ${loadaddr} 0x300 0x400
To flash the eMMC UDA HW partition from SD: Flash each binary at specific offsets chosen to not overwrite the partition table on the device. Assuming that the files exist on the SD card.
=> mmc dev 0
=> mmc rescan
=> mmc dev 1
=> fatload mmc 0 ${loadaddr} MLO
=> mmc write ${loadaddr} 0x100 0x100
=> mmc write ${loadaddr} 0x200 0x100
=> fatload mmc 0 ${loadaddr} u-boot.img
=> mmc write ${loadaddr} 0x300 0x400
=> fatload mmc 0 ${loadaddr} rootfs.ext4
=> mmc write ${loadaddr} 0x1000 ...rootfs.ext4 size in bytes divided by 512, in hex...
3.1.2.4.1.4.1. eMMC boot configuration
We also need to configure the eMMC to boot from boot0 HW partition using the bootbus and partconf commands. The bootbus command sets the eMMC into dual data rate mode with a bus width of 8 to match with the bus configuration supported by the Boot ROM. The partconf command gives access to the boot0 HW partition during boot operation. Note that these configurations are limited to boot operation and the eMMC can be set to its highest speed mode once boot operation is complete. All these are non-volatile configurations that need to be done once per eMMC/board .
=> mmc bootbus 1 2 0 2
=> mmc partconf 1 1 1 0
=> mmc rst-function 1 1
3.1.2.4.1.5. Flashing an MMC device using USB-DFU
To see the list of available places to write to (in DFU terms, altsettings) list the
MMC partitions with mmc part command, run printenv dfu_alt_info_mmc
or printenv dfu_alt_info_emmc to see how they are mapped and exposed to
dfu-util.
=> mmc part
Partition Map for MMC device 0 -- Partition Type: DOS
Partition Start Sector Num Sectors Type
1 63 144522 c Boot
2 160650 1847475 83
3 2024190 1815345 83
=> printenv dfu_alt_info_mmc
dfu_alt_info=boot part 0 1;rootfs part 0 2;MLO fat 0 1;u-boot.img fat 0 1;uEnv.txt fat 0 1"
Note
The above command: mmc part lists the partitions in the current selected device. Switch to a different MMC device with mmc dev, refer to Selecting MMC device and paritions.
This means that you can tell dfu-util to write anything to any of:
boot
rootfs
MLO
u-boot.img
uEnv.txt
And that the MLO, u-boot.img and uEnv.txt files are to be
written to a FAT filesystem.
To start DFU on the target on the first MMC device:
=> setenv dfu_alt_info ${dfu_alt_info_mmc}
=> dfu 0 mmc 0
On boards like AM57x GP EVM or BeagleBoard x15, where the second USB instance is used as USB client, the dfu command becomes:
=> dfu 1 mmc 0
Then on the host PC to write MLO to an existing boot partition:
$ sudo dfu-util -D MLO -a MLO
On the host PC to overwrite the current boot partition contents with a new created on the host FAT filesystem image:
$ sudo dfu-util -D fat.img -a boot
3.1.2.4.1.6. Flashing an SD card from a host PC
This section assumes that you have flashed an SD card using the script “create-sdcard.sh” packaged in the installer or have made a compatible layout manually. In this case, you will need to copy the boot images:
MLOu-boot.img
to the SD card boot partition. At this point, the device can boot to u-boot prompt.
3.1.2.4.2. USB
3.1.2.4.2.1. Configuring USB in Host Mode
Configuring USB in host mode documentation is pending for AM437x, please reach out to: Help e2e for additional information.
3.1.2.4.2.2. Flash and boot SPL from USB storage
Booting to U-Boot prompt from USB storage is supported. The following are the steps to be followed:
In U-Boot the USB controller can be used in either host or peripheral mode.
Build the bootloader images using the “am43xx_evm_usbhost_boot_defconfig”. For instructions to build the bootloader images please refer to Build U-Boot.
Create a FAT32 partition with boot flag enabled on the USB storage device.
Copy the bootloader images(MLO, u-boot.img) into the above created partition.
Set the boot mode switches to USB host boot mode (For boot switch details refer to the Initialization/Functional Description/Booting chapter of TRM.)
Connect the USB Mass storage device with the bootloader images and boot up the board.
The board should now boot to u-boot prompt.
3.1.2.4.2.3. Boot Linux from USB storage
Booting Linux from USB storage documentation is pending for AM437x, please reach out to: Help e2e for additional information.