3.2.2.2. Audio

3.2.2.2.1. Introduction

The audio subsystem present on various TI SoCs consists of two major components:

  1. Multi-channel Audio Serial Port (McASP) - Provides a full-duplex serial interface between the host processor and external audio peripherals like codecs over industry-standard protocols like Inter-IC sound (I2S).

  2. System DMA engine - Provides McASP with direct access to system memory to read audio samples from (for playback) or store audio samples to (for capture).

Along with the above, most TI EVMs and SKs have line input/output jack(s) wired to an on-board codec that can convert between the analog signals and the digital protocol supported by McASP.

3.2.2.2.2. Software Architecture

All the hardware components are exposed to userspace applications using the Linux ALSA (Advanced Linux Sound Architecture) framework, which allows control and configuration of the hardware through common APIs. For more details check the links below.

Within the kernel there are separate drivers for each component. For each board a sound-card instance is created, usually using the sound {} device tree node, that links together various components like different McASP instances to a codec or an HDMI bridge.

../../../../_images/audio-asoc-arch.png

3.2.2.2.3. McASP Configuration

TI EVMs include a default McASP configuration in the device tree that defines the sound topology connecting McASP to the onboard codec(s). For custom designs using a different sound topology—such as different codec connections or a different codec—the McASP configuration parameters described in this section can be modified accordingly in the device tree.

The Multichannel Audio Serial Port (McASP) is a highly configurable audio interface that supports various audio protocols including I2S, TDM, and S/PDIF, and a flexible clocking scheme, which allows for complete independence between the receive and transmit ports.

McASP serializers are connected to data pins, referred to as AXR pins. The name stands for “Audio Transmit/Receive” (AXR), reflecting the fact that any McASP data pin can be configured to function as either an input or an output. As such, the terms “serializer” and “AXR pin” are used interchangeably throughout this documentation.

3.2.2.2.3.1. Device Tree Properties

McASP nodes are typically defined in the SoC-level device tree (.dtsi) first with base properties like compatible, reg, interrupts, and dmas, which stay the same regardless of audio configuration.

Board-level device trees then customize the McASP configuration using the properties below. Together they form the complete McASP node definition.

The following table briefly describes the McASP-specific properties configured in board-level device trees:

Property

Type

Required

Description

op-mode

uint32

Yes

Operation mode:
• 0 for I2S/TDM mode
• 1 for DIT mode (Transmitter-only mode for self-encoding formats like S/PDIF)

tdm-slots

uint32

Yes, for I2S/TDM mode

Number of TDM slots for TX (and RX if tdm-slots-rx not specified). Range: 2-32.
Ignored in DIT mode.

auxclk-fs-ratio

uint32

No 1

A fixed multiplier to sampling rate (𝑓s) for a given AUXCLK frequency for TX (and RX if auxclk-fs-ratio-rx not specified).
1 If not specified, dividers are calculated from .set_sysclk via the ASoC machine driver. (For common machine driver such as simple-audio-card or audio-graph-card, this is set via the system-clock-frequency = <> property in the DAI link).
Only applicable when McASP is the master which produces the bit clock.
See Configuration Guidelines for details on usage and calculation.

serial-dir

uint32 array

Yes

Serializer pin configuration.
For each AXR pin:
0 = Inactive,
1 = TX,
2 = RX.
Must include all AXR pins available on the McASP instance.

ti,async-mode

boolean

No

Enables independent TX and RX clocking, allowing different sample rates (𝑓s) and bits per frame for playback and capture.
Ignored in DIT mode.

tdm-slots-rx

uint32

No

Number of TDM slots for RX, allowing independent RX slot count. Range: 2-32.
Requires ti,async-mode.

auxclk-fs-ratio-rx

uint32

No

Multiplier to sampling rate for a given AUXCLK frequency for RX.
Requires ti,async-mode.

tx-num-evt

uint32

No

WFIFO threshold for TX. Enables TX FIFO buffering when non-zero. Disabled by default.

rx-num-evt

uint32

No

RFIFO threshold for RX. Enables RX FIFO buffering when non-zero. Disabled by default.

Note

In the latest K3 family of SoCs (Sitara™ AM6x, Jacinto™ J4x platforms etc.), McASP FIFOs are disabled by default to achieve low latency, since K3 DMA already provides internal buffering.
Enabling McASP FIFOs is generally not required and should be considered for specific use cases that need additional buffering at the McASP level, such as:
• Scenarios with slow DMA throughput
• High DDR bandwidth utilization where additional buffering helps system stability
• Applications requiring extra data buffering to compensate for overall system latency

For more detail, refer to davinci-mcasp-audio.yaml and davinci-mcasp-audio.txt in the Linux kernel source.

3.2.2.2.3.2. Capabilities Overview

The McASP driver supports multiple audio protocols and operational modes:

Operation Modes:

  • I2S/TDM Mode (op-mode = 0)

    • Supports 2 to 32 TDM slots (channels)

    • Full-duplex operation (simultaneous TX and RX)

    • Can operate in synchronous or asynchronous mode

  • DIT Mode (op-mode = 1)

    • Transmit-only operation

    • Hardware-generated S/PDIF encoding

    • The tdm-slots, ti,async-mode properties are ignored

    • Only inactive or TX serializers (values 0, 1) should be configured in serial-dir

Clock Modes:

  • Synchronous Mode (default): TX and RX share the same bit clock and frame sync signals, requiring identical sample rates and bits per frame for both directions

    • Suited for simple, single-codec designs where ADC and DAC bit clocks and frame sync need to be synchronized

  • Asynchronous Mode (ti,async-mode): Independent TX and RX clocking, allowing different sample rates, bits per frame, and TDM slot counts for playback and capture

    • Enables simultaneous playback and capture with independent audio settings

    • Allows flexibility in multi-sound topology designs with various ASoC codec-class drivers connected to the same McASP instance

Important

To fully support asynchronous mode, the codec driver must also support independent clocking for playback/capture and should not impose such restrictions on ASoC framework.
For instance, .symmetric_rate should not be set in the codec driver’s snd_soc_dai_driver struct. Otherwise, opening streams with different audio settings will fail with errors similar to the following:
[  146.186314]  davinci-mcasp.0-pcmdevice-codec: ASoC: unmatched rate symmetry: 2b20000.au
dio-controller:44100 - soc_pcm_params_symmetry:48000
[  146.187012]  davinci-mcasp.0-pcmdevice-codec: ASoC: error at __soc_pcm_hw_params on dav
inci-mcasp.0-pcmdevice-codec: -22
arecord: set_params:1456: Unable to install hw params:
...

Key Features:

  • Multiple serializers (up to 16) for multi-channel audio

  • Configurable McASP FIFO buffering (tx-num-evt, rx-num-evt)

  • Fixed clock generation with auxclk-fs-ratio or dynamic machine driver sysclk settings

  • Support for master and slave clock modes (via DAI link configuration)

3.2.2.2.3.3. Configuration Scenarios

The examples below show typical board-level McASP configurations. Base properties like compatible, reg, interrupts, and dmas are inherited from the SoC-level dtsi file and are not shown here.

I2S/TDM Mode - Synchronous, Stereo (2 slots)

For stereo audio (2 TDM slots) with synchronized TX/RX clocking:

 /* Example from AM62x-SK (k3-am62x-sk-common.dtsi) */
 &mcasp1 {
    status = "okay";
    #sound-dai-cells = <0>;

    pinctrl-names = "default";
    pinctrl-0 = <&main_mcasp1_pins_default>;

    op-mode = <0>;          /* MCASP_IIS_MODE */
    tdm-slots = <2>;
    auxclk-fs-ratio = <256>;
    serial-dir = <  /* 0: INACTIVE, 1: TX, 2: RX */
          1 0 2 0
          0 0 0 0
          0 0 0 0
          0 0 0 0
    >;
};

I2S/TDM Mode - Synchronous, Multiple TX Serializers

For stereo audio (2 TDM slots) with multiple TX serializers and auxclk-fs-ratio (synchronized TX/RX clocking):

/* Example from J721S2 (k3-j721s2-common-proc-board.dts) */
&mcasp4 {
   status = "okay";
   #sound-dai-cells = <0>;

   pinctrl-names = "default";
   pinctrl-0 = <&mcasp4_pins_default>;

   op-mode = <0>;          /* MCASP_IIS_MODE */
   tdm-slots = <2>;
   auxclk-fs-ratio = <256>;
   serial-dir = <    /* 0: INACTIVE, 1: TX, 2: RX */
      0 2 1 1
      0 0 0 0
      0 0 0 0
      0 0 0 0
   >;
};

I2S/TDM Mode - Asynchronous (Independent TX/RX)

For I2S/TDM mode with asynchronous clocking, enabling independent TX and RX configurations with different slot counts and sample rates. This contrasts with the synchronous I2S/TDM modes above where TX and RX share the same clocking:

/* Example from AM62D-EVM (k3-am62d2-evm.dts) */
&mcasp2 {
   status = "okay";
   #sound-dai-cells = <0>;

   pinctrl-names = "default";
   pinctrl-0 = <&main_mcasp2_pins_default>;

   auxclk-fs-ratio = <2177>;
   op-mode = <0>;          /* MCASP_IIS_MODE */
   tdm-slots = <2>;        /* DAC Codec configured for stereo playback */
   tdm-slots-rx = <4>;     /* ADC Codec configured for 4-channel capture */
   ti,async-mode;
   serial-dir = <    /* 0: INACTIVE, 1: TX, 2: RX */
         1 1 0 1
         1 0 0 0
         0 0 0 0
         0 0 2 0
   >;
};

DIT Mode (S/PDIF)

For S/PDIF digital audio output (transmit-only):

/* Example from OMAP4 device (omap4-l4-abe.dtsi) */
&mcasp0 {
   status = "okay";
   #sound-dai-cells = <0>;

   pinctrl-names = "default";
   pinctrl-0 = <&main_mcasp0_pins_default>;

   op-mode = <1>;    /* MCASP_DIT_MODE */
   serial-dir = < 1 >;
};

3.2.2.2.3.4. Configuration Guidelines

This section provides rules and guidelines when configuring certain McASP device tree properties.

auxclk-fs-ratio

This property defines the ratio between the AUXCLK (reference clock) and the sampling rate, as a means to statically configure its internal clock dividers. Giving a hint to the driver to pick the specific sampling rate whenever possible at runtime.

Alternatively, a fixed clock source frequency can be specified via the DAI-link property system-clock-frequency = <> or via a custom machine driver’s .set_sysclk() callback, allowing the driver to dynamically calculate dividers for any McASP-supported sampling rate.

Either or both properties may be defined. But at least one must be provided: auxclk-fs-ratio to specify the clock divider, or system-clock-frequency to specify the reference clock frequency directly.

When using auxclk-fs-ratio, calculate the ratio as follows:

For example, given a desired sampling rate of 44.1kHz with a 96MHz AUXCLK, the auxclk-fs-ratio would be: \(96000000 / 44100 = 2177\). This ratio is also applicable to other standard sampling rates McASP supports, as long as the produced bit clock is within acceptable tolerance.

The same applies to auxclk-fs-ratio-rx.

Refer to the Runtime Behavior section below for tolerance calculation details.

serial-dir

The serial-dir array size must match the hardware (e.g., 16 AXR pins for McASP0 means array must have 16 entries). Each McASP instance may have up to 16 AXR pins, please refer to device-specific data sheet and TRM.

serial-dir = <  /* 0: INACTIVE, 1: TX, 2: RX */
      1 0 2 0  /* AXR0-3:  TX, Inactive, RX, Inactive */
      0 0 0 0  /* AXR4-7:  All inactive */
      0 0 0 0  /* AXR8-11: All inactive */
      0 0 0 0  /* AXR12-15: All inactive */
>;

3.2.2.2.3.5. Codec Integration

The McASP configuration described above defines the hardware interface. To create a functional audio device, the McASP node needs to be connected to codec class driver(s) via a sound card definition in the device tree.

The simple-audio-card is a generic machine driver and establishes Digital Audio Interface (DAI) links that connect the McASP (CPU-side) to codec(s). These DAI links operate within the ASoC framework, which constitutes part of the ALSA stack. Most TI EVMs use simple-audio-card for its simplicity, though audio-graph-card or custom machine drivers are also supported. All DAI link properties McASP relies on are part of the generic ASoC framework, not specific to any particular machine driver.

The DAI link configuration provides the following intrinsics to the McASP driver:

  • Link McASP instance(s) to codec instance(s)

  • Mapping of McASP serializers to DAI links

    • e.g., McASP assumes the first TX AXR pin is mapped to the first playback-enabled DAI link and outputs data to the first available TX TDM slot; see Channel Mapping

  • Master/slave clocking roles for bit clock and frame sync signals

    • If McASP is the master, system-clock-direction-out must be declared in the CPU DAI for McASP to generate clocks

  • Data alignment format

    • e.g., “dsp_a”, “dsp_b”, “i2s”

  • Polarity of bit clock and frame sync signals via bitclock-inversion and frame-inversion

  • Optional dai-link properties:

    • system-clock-frequency

    • dai-tdm-slot-width

    • dai-tdm-slot-num

    • dai-tdm-slot-tx-mask

    • dai-tdm-slot-rx-mask

Attention

Due to ASoC and driver limitations, the data alignment format must remain the same for every DAI link connected to the same McASP node, even in asynchronous mode where the hardware is capable of having independent playback and capture settings.

3.2.2.2.3.5.2. Audio Card Examples

Single Codec

For simple stereo configurations with one codec, a single DAI link suffices:

sound0 {
   compatible = "simple-audio-card";
   simple-audio-card,name = "AM62x-SKEVM";
   simple-audio-card,format = "i2s";

   simple-audio-card,cpu {
      sound-dai = <&mcasp1>;
   };

   simple-audio-card,codec {
      sound-dai = <&tlv320aic3106>;
   };
};

In this single codec configuration:

  • ti,async-mode should be disabled (synchronous mode) in McASP device tree node since playback and capture share the same codec and require identical clock settings

Multiple Codecs

When using multiple codecs, define separate DAI links for each codec. The following syntax allows separate configurations for each DAI link:

/* Example from AM62D-EVM (k3-am62d2-evm.dts) */
sound0 {
   compatible = "simple-audio-card";
   simple-audio-card,name = "AM62D2-EVM";

   /* First DAI, McASP in master mode */
   simple-audio-card,dai-link@0 {
      format = "dsp_a";
      bitclock-master = <&master0>;
      frame-master = <&master0>;

      master0: cpu {
            sound-dai = <&mcasp2>;
            system-clock-direction-out;
      };

      codec@0 {
            sound-dai = <&pcm6240>;
      };
   };

   /* Second DAI, McASP in master mode */
   simple-audio-card,dai-link@1 {
      format = "dsp_a";
      bitclock-master = <&master1>;
      frame-master = <&master1>;

      master1: cpu {
            sound-dai = <&mcasp2>;
            system-clock-direction-out;
      };

      codec@1 {
            sound-dai = <&tad5212_dac1>;
            playback-only;
      };
   };

   /* Additional dai-link@2, @3, @4 for more codecs... */
};

In this multi-codec configuration:

  • Each DAI link connects the same McASP instance to different codecs and maps serializers/AXRs accordingly

  • It is recommended to enable ti,async-mode in the McASP device tree node to allow more flexibility with independent TX/RX clocking

  • The bitclock-master and frame-master properties specify which device (CPU or codec) drives the bit clock and frame sync signals

  • system-clock-direction-out is required for McASP to generate clocks, which is required when McASP is driving the signals in master mode

  • Since McASP is in master mode, auxclk-fs-ratio should be defined in the McASP node, otherwise system-clock-frequency must be set in the DAI link to provide a fixed clock source

For more information on DAI link configuration and ASoC machine drivers, refer to ALSA links in the Additional Information section below.

3.2.2.2.3.6. Runtime Behavior

The McASP driver makes dynamic runtime decisions when handling audio streams, including serializer activation, channel-to-slot mapping, and supported audio formats. These behaviors are determined by the interaction between hardware capabilities and parameters requested by userspace through the ALSA framework.

Note

The runtime behaviors described in this section apply to I2S/TDM mode (op-mode = 0) only. DIT mode (op-mode = 1) has fixed S/PDIF encoding behavior per specification.

3.2.2.2.3.6.1. Channel Mapping

When a playback or capture stream is opened, the ALSA framework passes the requested number of audio channels from the userspace application to the McASP driver.

The driver activates TX or RX serializers (AXR pins) in the order they appear in the serial-dir device tree property. For each serializer, the driver maps channels to available TDM slots sequentially. If dai-tdm-slot-tx-mask or dai-tdm-slot-rx-mask are configured, disabled slots are skipped. This process continues across multiple serializers until all requested channels are mapped. Unused TDM slots and AXR pins remain inactive.

The total TDM slot count on the bus (frame sync period) is always preserved as defined by tdm-slots or tdm-slots-rx, regardless of how many channels are actively used.

If the requested channels exceed the available capacity (\(active\_serializers \times slots\_per\_serializer\)), the driver rejects the stream with an error.

3.2.2.2.3.6.2. Sample Rate and Bit Depth

Note

This section only pertains to McASP configured as the bit clock master. When McASP is in slave mode, it accepts whatever combinations the codec provides without imposing constraints.

When a stream is opened and McASP is in master mode, the driver evaluates which sample rate and bit depth combinations can be supported based on its ability to generate the required bit clock frequency within ±1000 ppm tolerance (0.1%).

The driver uses auxclk-fs-ratio (if defined) to calculate the expected reference clock frequency as rate × ratio for each sampling rate, and/or uses a fixed clock source frequency from system-clock-frequency/.set_sysclk() for all rates. In both cases, it calculates dividers to determine which bit clock frequencies can be achieved within tolerance.

\(error_{ppm} = \frac{actual\_freq - target\_freq}{target\_freq} \times 10^6\)

Only combinations that can be accurately generated are provided as supported formats, and ALSA subsequently selects the best configuration for the userspace application.

To support a specific sample rate and bit depth combination, ensure that:

  • The auxclk-fs-ratio property or machine driver’s .set_sysclk() configuration allows the McASP to generate the required bit clock frequency within tolerance

  • The codec supports the desired combination

  • If the source audio format differs, one may configure explicit resampling via ~/.asoundrc or /etc/asound.conf ALSA config file in userspace.

3.2.2.2.4. Generic commands and instructions

Most of the boards have simple audio setup which means we have one sound card with one playback and one capture PCM. To list the available sound cards and PCMs for playback:

aplay -l

To list the available sound cards and PCMs for capture:

arecord -l

For McASP-based sound card, each DAI link instance is represented as a separate subdevice.

In most cases -Dplughw:0,0 is the device we want to use for audio but in case we have several audio devices (onboard + USB for example) one needs to specify which device to use for audio:

-Dplughw:omap5uevm,0 will use the onboard audio on OMAP5-uEVM board.

To play audio on card0’s PCM0 and let ALSA to decide if resampling is needed:

aplay -Dplughw:0,0 <path to wav file>

To record audio to a file:

arecord -Dplughw:0,0 -t wav <path to wav file>

To test full duplex audio (play back the recorded audio w/o intermediate file):

arecord -Dplughw:0,0 | aplay -Dplughw:0,0

To request specific audio format to be used for playback/capture take a look at the help of aplay/arecord. For example, one can specify the format with -f, the sampling rate with -r, or the number of channels with -c. In this case, one should open the hw device (not the plughw) via -Dhw:0,0. For example, record 48KHz, stereo 16bit audio:

arecord -Dhw:0,0 -fdat -t wav record_48K_stereo_16bit.wav

Or to record 96KHz, stereo 24bit audio:

arecord -Dhw:0,0 -fS24_LE -c2 -r96000 -t wav record_96K_stereo_24bit.wav

It is a good practice to save the mixer settings found to be good and reload them after every boot (if your distribution is not doing this already)

Set the mixers for the board with amixer, alsamixer
alsactl -f board.aconf store

After booting up the board it can be restored with a single command:

alsactl -f board.aconf restore

3.2.2.2.5. Board-specific instructions

AM43x-EPOS-EVM

The board uses tlv320aic3111 codec connected through McASP1 [AXR0 for playback, AXR1 for Capture] for audio. The board features internal stereo speakers and two 3.5mm jack for Headphone and Mic In

Kernel config

Device Drivers  --->
  Sound card support  --->
    Advanced Linux Sound Architecture  --->
      ALSA for SoC audio support  --->
        Audio support for Texas Instruments SoCs  --->
          <*> Multichannel Audio Serial Port (McASP) support
        CODEC drivers  --->
          <*> Texas Instruments TLV320AIC31xx CODECs
        <*>   ASoC Simple sound card support

User space

Note

Before audio playback ALSA mixers must be configured for either Headphone or Speaker output. The audio will not work with incorrect mixer configuration!

To play audio through headphone jack run:

amixer sset 'DAC' 127
amixer sset 'HP Analog' 66
amixer sset 'HP Driver' 0 on
amixer sset 'HP Left' on
amixer sset 'HP Right' on
amixer sset 'Output Left From Left DAC' on
amixer sset 'Output Right From Right DAC' on

To play audio through internal speakers run:

amixer sset 'DAC' 127
amixer sset 'Speaker Analog' 127
amixer sset 'Speaker Driver' 0 on
amixer sset 'Speaker Left' on
amixer sset 'Speaker Right' on
amixer sset 'Output Left From Left DAC' on
amixer sset 'Output Right From Right DAC' on

To capture audio from both microphone channels run:

amixer sset 'MIC1RP P-Terminal' 'FFR 10 Ohm'
amixer sset 'MIC1LP P-Terminal' 'FFR 10 Ohm'
amixer sset 'ADC' 40
amixer cset name='ADC Capture Switch' on

If the captured audio has low volume you can try higher values for ‘Mic PGA’ mixer, for instance:

amixer sset 'Mic PGA' 50

Note: The codec has only one channel ADC so the captured audio is dual channel mono signal.

AM437x-GP-EVM

The board uses tlv320aic3106 codec connected through McASP1 [AXR2 for playback, AXR3 for Capture] for audio. The board features two 3.5mm jack for Headphone and Line In.

Kernel config

Device Drivers  --->
  Sound card support  --->
    Advanced Linux Sound Architecture  --->
      ALSA for SoC audio support  --->
        Audio support for Texas Instruments SoCs  --->
          <*> Multichannel Audio Serial Port (McASP) support
        CODEC drivers  --->
          <*> Texas Instruments TLV320AIC3x CODECs
        <*>   ASoC Simple sound card support

User space

The hardware defaults are correct for audio playback, the routing is OK and the volume is ‘adequate’ but in case the volume is not correct:

amixer -c AM437xGPEVM sset PCM 90                            # Master Playback volume

Playback to Headphone only:

amixer -c AM437xGPEVM sset 'Left HP Mixer DACL1' on               # HP Left route enable
amixer -c AM437xGPEVM sset 'Right HP Mixer DACR1' on              # HP Right route enable
amixer -c AM437xGPEVM sset 'Left Line Mixer DACL1' off            # Line out Left disable
amixer -c AM437xGPEVM sset 'Right Line Mixer DACR1' off           # Line out Right disable
amixer -c AM437xGPEVM sset 'HP DAC' 90                            # Adjust HP volume

Record from Line In:

amixer -c AM437xGPEVM sset 'Left PGA Mixer Line1L' on             # Line in Left enable
amixer -c AM437xGPEVM sset 'Right PGA Mixer Line1R' on            # Line in Right enable
amixer -c AM437xGPEVM sset 'Left PGA Mixer Mic3L' off             # Analog mic Left disable
amixer -c AM437xGPEVM sset 'Right PGA Mixer Mic3R' off            # Analog mic Right disable
amixer -c AM437xGPEVM sset 'PGA' 40                               # Adjust Capture volume

3.2.2.2.6. Potential issues

In case of XRUN (under or overrun)

The underrun can happen when an application does not feed new samples in time to alsa-lib (due CPU usage). The overrun can happen when an application does not take new captured samples in time from alsa-lib.
There could be several reasons for XRUN to happen, but it usually points to system latency issues connected to CPU utilization or latency caused by the storage device.
Things to try:
  • Increase the buffer size (ALSA buffer and period size)

  • Try to cache the file to be played in memory

  • Try to use application which uses threads for interacting with ALSA and with the filesystem

3.2.2.2.7. Additional Information

  1. ALSA SoC Project Homepage

  2. ALSA Project Homepage

  3. ALSA User Space Library

  4. Using ALSA Audio API Author: Paul Davis

Software Help

  1. Tools and Techniques for Audio Debugging

  2. Interfacing DRA7xx Audio to Analog Codecs

Audio hardware codecs

  1. TLV320AIC31 - Low-Power Stereo CODEC with HP Amplifier

  2. TLV320AIC3104 - Low-Power Stereo CODEC with HP Amplifier

  3. TLV320AIC3111 - Low-Power Stereo CODEC with Embedded miniDSP and Stereo Class-D Speaker Amplifier

  4. TLV320AIC3106 - Low-Power Stereo Audio CODEC

McASP Documentation

  1. McASP Hardware Design Guide