5.2.7. How to Fix Y2K38 Issue
5.2.7.1. What is the Y2K38 Issue?
The Y2K38 issue is a bug which prevents a date from exceeding 03:14:07 UTC on January 19, 2038, on 32-bit systems. This is because the structures used to store the date experience an integer overflow when the date is set beyond the mentioned one. This causes the system to crash.
For more information, see: https://en.wikipedia.org/wiki/Year_2038_problem
There are new data structures that are used on 32-bit systems to store date/time in longer fields, thereby avoiding the overflow and the crash. However, since setting and displaying date/time uses multiple software components (such as the kernel, glibc etc), all code on a filesystem must be Y2K38-compliant (i.e. all code must be using the new data structures and functions) for the filesystem to be Y2K38-friendly. If any piece of software uses the older structures and functions, it makes the whole filesystem vulnerable.
To understand how the problem was fixed in Scarthgap filesystem, refer: https://static.sched.com/hosted_files/osseu2024/8b/EOSS%20Vienna%202024%20-%20Surviving%20Y2038.pdf
5.2.7.2. Building a Y2K38-friendly Image
In SDK 9.3, TI’s 32-bit platforms are still based on Kirkstone filesystem, which is NOT Y2K38-friendly. The Y2K38 issue is fixed in OE-core Scarthgap, on which the next release will be based.
Until then, if a Y2K38-friendly filesystem is required, obtain a tisdk-thinlinux-image from the latest
cicd.scarthgap.x:
https://software-dl.ti.com/cicd-report/linux/index.html?section=platform&platform=am335x
The above images are based on the 6.6 Kernel and Scarthgap filesystem, and thus has the Y2K38 issue fixed.
Note
While the above images are Y2K38-friendly, it must be ensured that even the code introduced to it from other sources is Y2K38-friendly. Any code that is not Y2K38-friendly will break the Y2K38-compatibility of the filesystem. Thus it is important to be intentional about writing Y2K38-friendly code, and to test this code to ensure that the final image remains Y2K38-friendly.
To build a Y2K38-friendly image on the 6.6 Kernel and Scarthgap filesystem baseline, follow the “Build Instructions” section present in the above link.