2.3. Yocto Layer Configuration
Processor SDK uses oe-layersetup configuration files to initialize the Yocto build environment. Configure your build with the following command:
$ ./oe-layertool-setup.sh -f <config>
Replace <config> with one of the configuration files listed below.
The oe-layersetup git repository
contains the following configuration files in the configs/processor-sdk directory.
Config File |
Description |
Supported machines/platforms |
|---|---|---|
|
Processor SDK 11.02.05.02 Release |
am335x-evm |