3.2.4.17. USB MUSB
Quick Start Guide
This section is a quick guide on how to start using usb ports on TI platform with supplied pre-built binaries. Please refer to USB Quick Start
Introduction
The USB User’s Guide provides information about
Overview of USB hardware and software
Supported linux driver features for USB host and device mode of operation
The Linux USB configuration through menuconfig. Please refer to USB configuration
Hardware Overview
USBSS Overview
The USB subsystem includes
Two instances of USB (Mentor Graphic’s USB2.0 OTG) controllers. Each MUSB controller supports USB 1.1 and USB 2.0 standard.
CPPI 4.1 compliant DMA controller sub-module with 30 RX and 30 TX simultaneous DMA channels
CPPI 4.1 DMA scheduler
CPPI Queue Manager module with 92 queues for queuing/dequeuing packets
Interfaces to the CPU via 3 OCP interfaces
Master OCP HP interface for the DMA (for data transfers)
Master OCP HP interface for the Queue manager (to manage CPPI descriptors)
Slave OCP MMR interface (for CPU to access USBSS/MUSB registers)
Signals the standard Charge Pump (part of EVM BOM) for VBUS 5V generation
MUSB Controller Overview
The salient features of the MUSB USB2.0 OTG controller are:
High/full speed operation as USB peripheral.
High/full/low speed operation as Host controller.
Compliant with OTG spec.
15 Transmit and 15 Receive Endpoints other than the mandatory Control Endpoint 0.
Double buffering support in FIFO.
Support for high bandwidth Isochronous transfer
32 Kilobytes of Endpoint FIFO RAM for USB packet buffering.
Interfaced with CPPI4.1 DMA controller with 15 Rx and 15 Tx channels (for each usb controller).
Defer interrupt enable feature is supported for each packet descriptor of cppi-dma.
Software Overview
Mentor graphics controller driver (or MUSB driver)
The MUSB driver is implemented on top of Mentor controller IP which supports all the speeds (High, Full and Low). AM33XX USBOTG subsytem uses CPPI 4.1 DMA for all the transfers. The musb driver conforms to linux usb framework and supports both PIO and DMA mode of operation. The musb host controller driver (HCD) binds the controller hardware to linux usb core stack. The musb device or gadget controller driver binds the controller hardware and specific gadget driver (filestorage, cdc/rndis etc).
Linux USB Stack Architecture
As shown in the figure, linux usb stack is a layered architecture, with musb controller at the lowest layer, the musb host/device controller driver binds the musb controller hardware to linux usb stack framework. The CPPI4.1 DMA controller driver is responsible for transmit/receive of packets over the musb endpoints.
Driver Features List
The Mentor USB driver can be built as module or built-in to kernel
Support both PIO and DMA mode (The DMA mode not applicable for control endpoint)
Support two instances musb controller in otg mode (both usb0 and usb1 controller in otg mode. This will allow host or device operation on each port simultaneously.
The driver supports the following features for USB Host (AM33XX)
Host Mode Feature |
AM33xx |
---|---|
HUB class support |
Yes |
Yes |
|
Yes |
Table:
The driver supports the following features for USB Gadget (AM33XX)
Gadget Mode Feature |
AM33xx |
---|---|
Yes |
|
Yes |
|
Yes |
Table:
The driver supports the following features for Dual host/gadget (AM33xx)
Dual Mode Feature |
AM33x |
---|---|
Yes |
Table:
Not verified features of AM33xx
Not verified features |
am33x |
---|---|
Wifi support |
Not verified |
Serial device |
Not verified |
Table:
Known limitations
musb_am335x.ko can’t be removed (and we don’t allow that to happen) to workaround a known hwmod issue.
References
For more details about EVM, please refer to EVM reference manual.
The Mentor USB driver can be built as module or built into kernel. For more information refer to USB configuration