3.7.11. QT Graphics Framework

Qt is a powerful C++ toolkit for writing cross-platform graphics applications, enabling a single code base to run predictably and perform well on Windows and embedded platforms,

Please refer https://www.qt.io/ for additional details on Qt.

The PSDK target file system includes the pre-built Qt libraries under /usr/lib and a rich set of QT demo applications under /usr/share/qt5/examples.

3.7.11.1. Demos

Demos using the Null Window System / KMS / DRM / EGLFS are provided with Qt. By default EGLFS will use the eglfs_kms backend.

$ /usr/share/qt5/examples/opengl/hellogles3/hellogles3 -platform eglfs
$ /usr/share/qt5/examples/opengl/2dpainting/2dpainting -platform eglfs
$ /usr/share/qt5/examples/opengl/paintedwindow/paintedwindow -platform eglfs

The default eglfs_kms configuration file for Qt5 is located at /etc/qt5/eglfs_kms_cfg.json.

Please note that EGLFS backend is not smart enough to select a display device automatically. One must be specified in the config file using the device key. If one is not specified, /dev/dri/card0 will be used, which can either point at the GPU or the Display device depending on the order in which the devices were initialized. We recommend using the /dev/dri/by-path/* path for a persistent device path. If an incorrect device was chosen, an error like the following can appear: Failed to create display device (err=19).

For more information about Qt’s EGLFS and using Qt5 in embedded applications see:

3.7.11.2. QT QPA

The QT5 within PSDK is prebuilt with Wayland enabled and therefore wayland-egl is the default QPA. Hence all QT applications should be run on top of Weston. To run QT application without Weston, the user can use -platform option to specify the desired QPA as linuxfb or eglfs.

Note

The linuxfb inteface is deprecated and requires switching the display into legacy fb mode.

For example:

$ /usr/share/qt5/examples/opengl/2dpainting/2dpainting -platform eglfs

3.7.11.3. Running QT Applications with the Weston IVI shell

To run the QT application with ivi-shell, set the QT_WAYLAND_SHELL_INTEGRATION environment variable to ivi-shell.

$ export QT_WAYLAND_SHELL_INTEGRATION=ivi-shell