4.3.2. Predictive Maintenance Demo

4.3.2.1. Introduction

Predictive Maintenance (PdM) promises to achieve levels of efficiency and safety on the factory floor never seen before in the current established best practices for systems and processes. Machine downtime is one of the biggest challenges on the production line. The current method of MRO (maintain, repair, operate) is far from what the optimum level of production can be. With predictive maintenance, once data is coming from equipment in real-time (or near real-time depending on application needs), advanced analytics are used to identify asset reliability risks that could impact business operations. By applying machine learning and analytics to operational data generated by critical assets to gain a better understanding of asset performance, companies can act on these insights as part of a continuous improvement process.

Predictive maintenance employs advanced analytics on the machine data collected from end sensor nodes to draw meaningful insights that more accurately predict machine failures. It is comprised of three steps: sense, compute and act. Data is collected from sensors that are already available in machines, by adding NEW sensors, or by using control inputs. Depending upon the machine types and the required failure analysis, different sensor signals – such as temperature, sound, magnetic field, current, voltage, ultrasonic, vibration – are analyzed to predict the failure. The predicted information from sensor data analysis is used to generate an event, work order and notification. The sensor data is also used to visualize the machine’s overall operating condition. An action is taken when the event reports an anomaly, a machine that is nearing the end of its useful life, or when wear and tear is detected in machine parts.

The following are the advantages of predictive maintenance using analytics:

  • Detects incipient failures and breakdowns in early stages and facilitates early repair

  • Establishes shelf life of asset and assesses product warranty

  • Maintains inventory and tabs on spare parts

  • Explores hypothetical scenarios

  • Early notification and alerts to field operators and improves safety standards

  • Prevents unnecessary downtime in production processes

  • Maximizes lifecycle of equipment

  • Enables product innovation . new features, services and pricing models

Some of the examples of predictive maintenance from real-life scenario includes:

  • Find defective bearings long before defects are visually seen

  • Find misalignment between two rotating pieces of equipment

  • Recognize when fans become unbalanced

  • Identify when bearings need lubrication

  • Tell when an electrical connection needs to be tightened

  • Alert when oil is contaminated or in need of replacement

An overview video for predictive maintenance can be found from predictive maintenance overview training.

Processor SDK Linux now provides a predictive maintenance demo which leverages Recurrent Neural Network (RNN) for anomaly detection over motor drive control. The sections below describes the demo in details, including the system model for anomaly detection with RNN, the workflow of developing the PdM demo with step by step instructions, the benchmarking results, and the PdM demo deliverables from Processor SDK Linux.

4.3.2.2. Anomaly detection system model with RNN

In addition to Convolutional Neural Network (CNN), recently RNN emerged as high-quality universal approximation method for time series. It is becoming more effective with many desktop tools supported by GPU acceleration.

For anomaly detection, a system model is established to predict the output from the input for the normal scenario. If prediction of the output values is good, the system model acts as a high-accuracy approximation of the physical system. With this system model, if there are significant and continuous prediction errors, it indicates anomalies are happening.

../../../_images/system-model.png

Fig. 4.6 System model for anomaly detection with RNN

4.3.2.3. Workflow for developing the PdM demo

The figure below illustrates the workflow for developing the PdM demo. It begins with acquiring data that describes the physical system in a range of healthy and faulty conditions. The data can be from sensors, or generated from a physical model. Then, the acquired data will go through some pre-processing, such as down-sampling to reduce the data dimension. After that, it comes to the stage of developing the model. For PdM, the model can be either a detection model for condition monitoring (e.g., anomaly detection) or a prediction model for prognostics (e.g., estimating the remaining useful life). The model development requires identifying appropriate condition indicators and then training a model to interpret these condition indicators. This is likely an iterative process, as you try different models and indicators and tune the model parameters such as the number of RNN layers and nodes. The last step is to deploy the model and integrate the solution into a system for machine monitoring and maintenance at the edge devices.

../../../_images/develop-pdm-workflow.png

Fig. 4.7 Workflow for developing the PdM demo

In the following subsections, details are provided for the individual steps of this workflow using the anomaly detection for motor drive as the example.

4.3.2.3.1. Sensor data acquisition

In our PdM anomaly detection demo, the sensor data are originating from motor drive TI design. In this TI design, AM437x IDK (running Processor SDK RTOS, PRU-ICSS EtherCAT Slave, and PRU-ICSS Industrial Drives) is conducting motor control. It also receives the feedback about the phase current measurement and the position measurement. On the other hand, AM437x IDK acts as Ethercat slave and communicates with TwinCAT master on a host machine for setting the target velocity, target position, and etc.

To acquire the sensor data in real-time, high-speed (921600 baud rate) UART is implemented to send out the two phase currents (2 bytes each), and the motor position (4 bytes) with sampling rate of 10KHz. To get continuous sensor data, PyAutoGUI is employed to achieve automated control of TwinCAT, so that the motor can repeatedly move from position 1 to position 2, and then from position 2 back to position 1.

../../../_images/data-acquisition-motor-drive.png

Fig. 4.8 Sensor data acquisition from motor drive

4.3.2.3.2. Sensor data pre-processing

For the sensor data with a frequency of 10KHz, simple pre-processing of low-pass filtering and down-sampling to 50Hz is done to reduce the high frequency noise. After that, normalization is done for the down-sampled sensor data.

Depending on the application, some Other preprocessing techniques can be applied, such as FFT, high order statistics, and wavelets.

4.3.2.3.3. Offline training to establish the model

To establish the RNN model, offline desktop training in MATLAB is done with the two down-sampled phase currents. The RNN topology contains a single Long Short-Term Memory (LSTM) layer, and a Fully Connected (FC) layer. There are 31 hidden nodes for the LSTM layer, and 31 inputs and 2 outputs for the FC layer. This is a simple RNN model, which is specified to avoid overfitting and control the computation load. The trained model is in Open Neural Network Exchange (ONNX) format. The last layer, regression layer, is the output layer used for prediction.

../../../_images/training-RNN.png

Fig. 4.9 Offline training RNN model with LSTM and FC layers

The RNN model is trained with the normal scenario data: motor moves with velocity of 100 degree per second from 45 degree to 270 degree and back to 45, and so on so forth. With a single training sequence about 50s long, the training with Matlab on a desktop PC is completed in less than three minutes.

Some other open source tools, such as Keras/Tensor Flow, Pytorch, can also be used for the training.

4.3.2.3.4. Deploy and integration

After getting the model, the last step is to deploy the model and integrate it for anomaly detection at the edge.

Build RNN inference library

To establish the RNN inference library implementing the LSTM and FC layers, our initial solution is using python scripts to convert the ONNX model into CPP header file, which contains the initialized data structures with all the weights information. The python scripts supports N stacked LSTM layers, plus one FC layer. The generated CPP header is then compiled with the LSTM library to create the ARMv7 object file with the initialization and processing APIs.

../../../_images/rnn-inference-lib.png

Fig. 4.10 Build RNN inference library

Real time anomaly detection at the edge

With the RNN inference library, we build the Linux user space application running on Arm to perform anomaly detection. The figure below shows the call flow of the anomaly detection. The two phase currents are received in real-time from the motor control application running on AM4 IDK. Then, low pass filtering and down-sampling are applied to the phase currents, followed by normalization. After that, RNN prediction is done upon the pre-processed phase currents, using the RNN inference library built above. The predicted phase currents are then de-normalized, and compared with the actual phase currents to calculate the prediction error. The prediction errors at the beginning for the normal scenario are used for calibration: the maximal prediction error in this stage is scaled with a ratio larger than 1 to be the anomaly detection threshold. After that, the prediction error will be used to report anomalies: if the prediction is larger than the threshold found in the calibration stage, then anomaly is reported.

../../../_images/anomaly-detection.png

Fig. 4.11 Real time anomaly detection

4.3.2.4. Deliverables from Processor SDK Linux

Processor SDK Linux provides an out of box PdM demo from Matrix GUI. It also supports re-building the demo from the top-level Makefile. Python-based conversion tool is also provided to convert an ONNX model into CPP header file.

4.3.2.4.1. Out of box demo with with pre-recorded sensor data

The PdM demo for anomaly detection is provided from Matrix GUI under Analytics submenu - PdM Anomaly Detection with RNN.

../../../_images/pdm-in-matrix-gui.png

Fig. 4.12 PdM anomaly detection demo in Matrix GUI

For this out of box demo, pre-recorded sensor data (/usr/share/ti/examples/pdm/normal100-anomaly150-normal100.log) is used as the testing sequence, as shown in the demo scripts (/usr/bin/runPdmAnomalyDetection.sh). This testing sequence starts with the normal scenario data, i.e., motor moves with velocity of 100 degree per second from 45 degree to 270 degree and back to 45, and so on so forth. To create anomalies, the motor moves with a higher velocity of 150 degree per second after some time. The figure below shows the Qt GUI display of the demo. The left-side panel shows the real-time sensor input: the two phase currents in blue and green, and the motor position in orange. The right-side panel shows the detection results: the blue line is the anomaly detection threshold found from the calibration, the orange line draws the prediction error, while the red line draws the time period of the detected anomaly.

../../../_images/pdm-qt-gui-anomaly-detection.png

Fig. 4.13 Anomaly detection demo display

Filesystem of Processor SDK Linux also packages two more pre-recorded testing sequences (under /usr/share/ti/examples/pdm/), for some other anomalies.

  • normal270-anomaly170-normal270.log: motor moving from 45 degree to a different (170 instead of 270) degree.

  • normal45-270-v100-with-friction2-iter10-15.log: hand-pressing the coupler between the motor and the encoder to add more friction.

4.3.2.4.2. Support rebuilding the demo from top-level Makefile

The source of the PdM demo for real-time inference is available at pdm-anomaly-detection git rep. The source is also bundled with Processor SDK Linux installer, under the example-applications directory:

[plsdk_install_dir]/example-applications/pdm-anomaly-detection-1.0

Rebuilding of the demo can be done via the top-level Makefile of Processor SDK Linux:

cd [plsdk_install_dir]
make pdm-anomaly-detection

After the compilation is completed, the demo binary can be found at [plsdk_install_dir]/example-applications/pdm-anomaly-detection-1.0/RnnPdmAnomalyDetection.

4.3.2.4.3. ONNX model conversion tool

Python scripts are provided in the PdM demo source under the model folder to convert ONNX model to CPP header file with initialized data structures. It supports N stacked LSTM layers plus on fully connected layer as the last layer.

Before running the scripts, install the python packages below if this has not been done earlier.

sudo apt install python-pip
pip install numpy pandas scipy onnx

Then, run the command below to do the conversion:

cd pdm-anomaly-detection/model or pdm-anomaly-detection-1.0/model
python ./make_header.py -m ./[onnx-model-file]

The output CPP header file is called LSTM_model.h which is placed under the same model folder.

4.3.2.5. Benchmarking for anomaly detection with RNN

To conduct benchmarking for the RNN based anomaly detection, two threads are used with Qt/QML display not in the picture.

  • thread 1: main processing thread with RNN prediction and anomaly detection

  • thread 2: parsing thread to read senor data

Linux clock_gettime() function is used for reading the time:

clock_gettime(CLOCK_REALTIME, &ts0);

/* Run LSTM network for prediction */
runLstm(lstm_in1, lstm_in2, &lstm_out1, &lstm_out2);

clock_gettime(CLOCK_REALTIME, &ts1);
ns_lstm = (ts1.tv_sec-ts0.tv_sec) * 1000000000 + ts1.tv_nsec-ts0.tv_nsec;

Two benchmarking points are used:

  • Pre-processing: low-pass filtering and down-sampling to reduce 200 samples to 1 sample

  • RNN prediction (LSTM + FC) on 1 sample

Average compute time per sample:

  • RNN prediction: 0.083ms

  • Pre-processing: 0.014ms

  • Total (RNN prediction and pre-processing): 0.097ms

With a sampling rate 50Hz, RNN based anomaly detection consumes around 0.5% of CPU running at 1GHz, showing a low computation load.