2.1. Release Notes

2.1.1. Overview

The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.

To simplify the end user experience, Processor SDK Linux AM64x installer provides, everything needed to create the embedded system from “scratch”, with...

  • Platform/board-support software and configuration files for Linux
  • U-Boot and Kernel sources and configuration files
  • An ARM cross-compiling toolchain as well as other host binaries and components
  • A Yocto/OE compliant filesystem and sources for example applications
  • A variety of scripts and Makefiles to automate certain tasks
  • Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
  • Reference Examples, benchmarks

2.1.2. Licensing

Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.

  • Linux Manifest: “/docs/software_manifest.htm”

2.1.3. Release 08.00.00

Released on August 2021

What’s New

Processor SDK Linux AM64x Release has following new features:

  • First release on 2021 LTS 5.10 kernel, 2021.01 U-Boot
  • Support for DFU boot in SPL bootloader
  • Support for ICSS-G Dual EMAC/PRUETH
  • Support for ECAP, MCAN, ePWM, SA2UL, WDT drivers
  • Unified DDR driver for AM64
  • ATF 2.5, OPTEE 3.12
  • WiFi out of box demo for AM64x SK
  • Matrix GUI LED demo for AM64 EVM and SK
  • Yocto build support for all the demo components including benchmark demo
  • Toplevel Makefile in the installer for building BSP components

2.1.4. Build Information

2.1.4.1. U-Boot

Head Commit: 53e79d0e89f975eeb874366dd9a92f68b3a599d1 defconfigs: am65x_hs_evm: Sync HS and non-HS defconfigs
Repo: git://git.ti.com/ti-u-boot/ti-u-boot.git
Branch: 08.00.00.004

2.1.4.2. Kernel

Linux Kernel

Head Commit: 4c2eade9f722838b0e457650368cba1c6c7483c2 Merged TI feature rpmsg into ti-linux-5.10.y
Branch: ti-linux-5.10.y
Kernel defconfig: ti_sdk_arm64_release_defconfig

Real Time (RT) Linux Kernel

Head Commit: 0701a5b58c943909a38be9df38a3b4bdd8234340 Merged TI feature ti_linux_base_rt into ti-rt-linux-5.10.y
Branch: ti-rt-linux-5.10.y
Kernel defconfig: ti_sdk_arm64_rt_release_defconfig

2.1.4.3. Yocto

meta-ti

Head Commit: 15f3d4a3c3773294f1cdb66a88744930941a892e ti-rtos-firmware: Add soft link to the rtos firmware binaries
Branch: dunfell

meta-arago

Head Commit: ae47bd7fbea2776a4f8792f20c493d7959ee2f54 iproute2: upgrade to 5.10
Branch: dunfell

meta-processor-sdk

Head Commit: ea2e8505fdf9948c0e2881af9dacb07e801c9037 recipes-ti: ti-tisdk-makefile: Remove evse-hmi snippet
Branch: dunfell

2.1.5. Issues Tracker

2.1.5.1. Issues opened in previous releases that were closed on this release

Record ID Platform Title
LCPD-21538 am64xx-evm PCI-EP MSI tests are failing am64xx-evm
LCPD-21516 WIC file generated does not include tiboot3.bin am64xx-evm
LCPD-21510 USB devices attached to am64xx-evm are not enumerated am64xx-evm
LCPD-21509 AM64x Core Benchmarks degrades on some runs am64xx-evm
LCPD-20721 AM64-sk: Memtester failures am64xx-sk
LCPD-20626 am64x-sk: mmc list command does not return anything am64xx-sk
LCPD-20163 am64xx fails to boot when using the mmcmode custom build am64xx-evm
LCPD-20162 Degraded performance when running IET tests over eth1 am64xx-evm
LCPD-20130 am64xx PCIe-EP test failing due to a NULL pointer exception am64xx-evm
LCPD-20106 USBDEVICE ping from DUT to host fails when packet_count=470 am64xx-evm,j7200-evm

2.1.5.2. Issues found and closed on this release that may be applicable to prior releases

Record ID Title Platform
LCPD-22854 am64xx crypto tests fail due to tcrypt am64xx-evm,am64xx-sk
LCPD-22842 am64xx ethernet CPSW3g tests faile due to queue 0 not increasing am64xx-evm
LCPD-22514 Broken USB MSC boot on AM642-EVM am64xx-evm
LCPD-22488 AM64 inconsistent promiscuous mode visibility am64xx-evm,j721e-idk-gw,j7200-evm
LCPD-22358 U-Boot: am642/am654/j72xx: ethernet address fixup is broken am64xx-evm,am654x-evm,j721e-evm,j7200-evm
LCPD-22281 U-Boot hangs with ‘LPDDR4_StartTest: FAIL’ error when starting on am64xx-evm am64xx-evm
LCPD-22240 2021.00 uboot on am64xx-evm - dhcp does not work am64xx-evm
LCPD-22048 U-Boot: J7/AM64: DDR driver size is bloated up am64xx-evm,j721e-idk-gw

2.1.5.3. SDK Known Issues

Record ID Platform Title Workaround
LCPD-20038 am64xx-evm OPTEE test applications are missing from rootfs  

2.1.5.4. U-Boot Known Issues

Record ID Platform Title Workaround
LCPD-23026 am64xx-evm USB MSC Boot: USB controller not visible from u-boot  
LCPD-23024 am64xx-evm PSDK-DOC: UBoot: USB host boot info is out of date  
LCPD-23020 am64xx-evm am64xx-evm: U-Boot PHY autonegotiation failed 2 out of 100 times  
LCPD-22841 am64xx-evm,j721e-idk-gw,j7200-evm j7200 Watchdog Timer test is failing  
LCPD-21962 am64xx-evm U-Boot documentation discrepancies  
LCPD-20131 am64xx-evm,j721e-idk-gw,j7200-evm Uboot fails to enumerate devices attached to a usb hub on the first ‘usb reset’ call Re-run usb reset command

2.1.5.5. Linux Kernel Known Issues

Record ID Platform Title Workaround
LCPD-22931 am64xx-evm,am64xx-sk,am654x-evm,am654x-idk,dra72x-evm RemoteProc documentation missing  
LCPD-22920 am64xx-evm AM64x Linux IPC documentation is insufficient / out-of-date  
LCPD-22913 am64xx-evm,j721e-idk-gw,j7200-evm USBDEV ACM NCM enumeration fails on the device side  
LCPD-22912 am64xx-evm am64xx-evm SMP dual core test fails sporadically  
LCPD-22892 am64xx-evm,am654x-evm,am654x-idk icssg: due to FW bug both interfaces has to be loaded always  
LCPD-22852 am64xx-evm AM64x: ICSSG ping with 16384 size shows high packet loss  
LCPD-22834 am64xx-evm am64xx-evm stress boot test files  
LCPD-22789 am64xx-evm cdns-usb3: g_mass_storage and g_ether fails on some boards  
LCPD-22534 am64xx-evm,am654x-evm,j721e-idk-gw,j7200-evm Ipsec aes128 TCP test failure  
LCPD-22319 am64xx-evm,j7200-evm OpenSSL performance test data out of bounds  
LCPD-22215 am64xx-evm PCIE NVM card stops enumerating on am64xx after some time  
LCPD-20705 am64xx-evm USB stick attached to PCIe USB card is not enumerated  
LCPD-20558 am64xx-sk OSPI UBIFS tests failing on am64xx-sk  
LCPD-20105 am64xx-evm AM64x: Kernel: ADC: RX DMA channel request fails  
LCPD-20061 am64xx-evm Occasional PHY error during during TSN Time-Aware Shaper execution  
LCPD-20006 am64xx-evm AM64x: remoteproc may be stuck in the start phase after a few times of stop/start  
LCPD-18854 am64xx-evm,dra71x-evm,dra76x-evm ov5640 sensor capture fails for raw format capture