2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Linux provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:
Bootloaders & Filesystems
SDK Installer
Setup Scripts
Makefiles
WLAN support (Wilink 8)
Code Composer Studio
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor SDK Linux GPLv3 Disclaimer.
2.1.3. Documentation¶
Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.
Software Manifest: Provides license information on software included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs
.EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Release 08.00.00¶
Released August 2021
What’s New
Processor SDK 8.0 Release has following new features:
First release on 2021 LTS 5.10 kernel, 2021.01 U-Boot
AM65: ICSS-G PRUETH
ATF 2.5, OPTEE 3.12
2.1.5. Supported Platforms¶
See here for a list of supported platforms and links to more information.
2.1.6. Build Information¶
2.1.6.1. U-Boot¶
2.1.6.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
Generic Kernel Release Notes
2.1.6.3. Yocto¶
meta-ti
meta-arago
2.1.7. Issues Tracker¶
2.1.7.1. Issues opened in previous releases that were closed on this release¶
Record ID |
Summary |
---|---|
LCPD-21334 |
Convert ti,j721e-gpio to yaml |
LCPD-20623 |
AM654x UART boot failing to boot |
LCPD-21536 |
AM654x - Display port tests fail due to tidss not found |
LCPD-21297 |
Upstream: remoteproc/pru: Fix multiple issues in firmware event mapping |
LCPD-19873 |
Pings not received by DUT over Ethernet VLAN |
2.1.7.2. Issues found and closed on this release that may be applicable to prior releases¶
Record ID |
Summary |
---|---|
LCPD-22979 |
firmware links are missing in /lib/firmware directory for K3 |
LCPD-22784 |
am654x-evm fails to load boot images over UART |
LCPD-22914 |
HS EVMs fail to boot |
LCPD-22304 |
am654x boot fails with latest baseboard dtb’s |
LCPD-22300 |
/dev/hwrng missing on K3 platforms |
LCPD-22188 |
j721e and am65 hs fails to build on 2021.01 uboot |
LCPD-22792 |
EFI is disabled |
LCPD-22358 |
U-Boot: am642/am654/j72xx: ethernet address fixup is broken |
LCPD-22344 |
crypto: sa2ul: crypto self-tests fail to allocate des3 algos |
LCPD-22342 |
crypto: sa2ul: Fix a number of leaks in failure paths in probe |
LCPD-22318 |
CRYPTO_S_PERF testcases are missing CONFIG_CRYPTO_DEV_SA2UL arg in 2021.00 |
LCPD-22306 |
GFX: Fix RT kernel build failure for SGX |
LCPD-22282 |
U-Boot: reset to default env fails in 2021 LTS |
LCPD-22239 |
2021.00 idk and pcie dtbs are missing for am654 |
2.1.7.3. Errata workarounds¶
Record ID |
Summary |
Workaround |
ErrataID |
---|---|---|---|
LCPD-17788 |
PCI-Express: GEN3 (8GT/s) Operation Not Supported. |
i2104 |
|
LCPD-17783 |
USB: USB2PHY Charger Detect is enabled by default without VBUS presence |
i2075 |
|
LCPD-19447 |
DSS: Disabling a layer connected to Overlay may result in synclost during the next frame |
i2097 |
|
LCPD-14579 |
DSS : DSS Does Not Support YUV Pixel Data Formats |
i2000 |
2.1.7.4. SDK Known Issues¶
Record ID |
Summary |
Workaround |
---|---|---|
LCPD-23006 |
PVR driver fails to detect SGX core on AM65x SR1.0 |
Remove graphics driver from filesystem (/lib/modules/5.10.41-g4c2eade9f7/extra/pvrsrvkm.ko) |
LCPD-19948 |
Yocto: stream recipe is incorrect |
|
LCPD-19858 |
OE: OPTEE label used in SDK is old and wrong |
|
LCPD-18908 |
GLMark2 fails for am65x |
|
LCPD-18270 |
Ivi shell test fails. Lib ivi-controller.so and other components are missing from the file system |
|
LCPD-17449 |
libasan_preinit.o is missing in devkit |
|
LCPD-17413 |
QT Webengine-based browser: the mouse does not work within the web page with QPA EGLFS |
|
LCPD-17412 |
QT5 Webengine-based browser crashing with any resize operation |
|
LCPD-13817 |
Qt5 Webengine-based broswer does not work on AM654x with pagesize = 64k |
|
LCPD-13816 |
Chromium-wayland broswer does not work on AM654x with page size = 64k |
2.1.7.5. U-Boot Known Issues¶
Record ID |
Summary |
Workaround |
---|---|---|
LCPD-22975 |
AM654x: 1Ghz & beyond caused boot hang on SR2.0 |
|
LCPD-17770 |
U-Boot: Fix order of MCU R5 shutdown depending on cluster mode |
|
LCPD-16524 |
Need to adjust RMW bit when using enabling ECC |
None |
LCPD-14843 |
U-boot should support default settings for netboot |
None |
LCPD-16696 |
U-Boot does not recognize SD-Card after re-insert/change |
|
LCPD-15873 |
There is no dtbo in u-boot for PCIe x1 + usb3 daughter card |
None |
2.1.7.6. Linux Kernel Known Issues¶
Record ID |
Summary |
Workaround |
---|---|---|
LCPD-23055 |
AM654x: DFU Boot fails |
|
LCPD-17471 |
device hang when restarting crashed R5F |
|
LCPD-13653 |
am65x-evm could not boot from MMC/SD when MMC/SD is backup boot mode |
No workaround |
LCPD-22962 |
IPC performance- IPC_S_FUNC_PRU_ECHO test failing |
|
LCPD-16534 |
remoteproc/k3-r5f: PDK IPC echo_test image fails to do IPC in remoteproc mode on second run |
None |
LCPD-22892 |
icssg: due to FW bug both interfaces has to be loaded always |
|
LCPD-19924 |
[AM65xx] ICSS-G TCP receive throughput degraded |
|
LCPD-19923 |
[AM65x] Linux reboot command fails |
|
LCPD-19861 |
ICSSG: Unregistered multicast MAC packets are still visible in non-promiscuous mode |
|
LCPD-19859 |
ETH ICSSG netperf benchmark returns lower performance than expected |
|
LCPD-19580 |
am654- unable to select a mode (sdhci?) |
|
LCPD-18665 |
Am65x Pg2: Board cannot do soft reboot when booting from SD card |
|
LCPD-18289 |
pcie-usb tests sometimes fail |
|
LCPD-18228 |
PCI PM runtime suspend is not increasing |
|
LCPD-17908 |
ICSSG: dual-emac: udp packets ocassionally sent out of order on egress |
|
LCPD-17800 |
CPSW: Master/Slave resolution failed message seen at console |
|
LCPD-15540 |
uvc-gadget results in segmentation fault |
|
LCPD-13938 |
PCIe EP read/write/copy test failed with larger sizes |
|
LCPD-13936 |
Uboot dhcp timeout 1 of 100 times |
|
LCPD-13603 |
One board could not boot rootfs from more than one SDHC card |
|
LCPD-13445 |
Seldom kernel oops triggered by prueth_netdev_init |
|
LCPD-22534 |
Ipsec aes128 TCP test failure |
|
LCPD-19929 |
Industrial protocols documentation |
|
LCPD-18860 |
isolcpus in the command line is not honored |
|
LCPD-18684 |
syscalls sync failures: fdatasync03, fsync04, sync03, syncfs01, sync_file_range02 |
|
LCPD-18258 |
IPSEC perfomance failures |
|
LCPD-17798 |
2020 LTS: INTA/INTR smp_affinity failure and IRQ allocation issues. |
|
LCPD-17777 |
AES HW is not exercised |
|
LCPD-17673 |
No software documentation for the Timer module |
|
LCPD-16845 |
OPP freq update in DT impacts only cluster0 |
|
LCPD-13410 |
Reboot command is not operational |
|
LCPD-22953 |
v4l2 cal compliance test fails |
|
LCPD-22952 |
alsa_amixer_volumesetting fails |
|
LCPD-22951 |
Alsa test fails - no soundcards found |
|
LCPD-22950 |
Alsa speaker test fails |
|
LCPD-22949 |
Audio interactive test fails |
|
LCPD-22947 |
Alsa performance test fails |
|
LCPD-18297 |
AM6: OV5640: 176x144 does not work |
|
LCPD-15819 |
tidss: the driver should reject dual-display setup, as it is not supported |
|
LCPD-20014 |
remoteproc: TX_PRU: IRQ vring, IRQ kick not found error message on console |
|
LCPD-22931 |
RemoteProc documentation missing |
|
LCPD-22959 |
UART Read/Write tests at baud rate 115200 fails |
|
LCPD-23012 |
DRM universal planes - Could not get DRM master permission |
|
LCPD-23009 |
CAL capture test- No capture device of type cal found |
|
LCPD-23008 |
AM65xx - display port scenario not enabled |
|
LCPD-23007 |
k3-am654-evm-hdmi.dtbo file is missing in CoreSDK for am654x |
|
LCPD-22955 |
DSS scaling and cropping tests fails- kms_props not supported |
|
LCPD-22954 |
DRM Stress Test fails |
2.1.7.7. RT Linux Kernel Known Issues¶
Record ID |
Summary |
Workaround |
---|---|---|
LCPD-6663 |
[RT] Kmemleak is buggy and boot is crashed randomly |
|
LCPD-22238 |
RT linux build sometimes fails to boot - might be related to remoteproc2 |
2.1.8. Change Requests¶
ID |
Head Line |
Original Fix Version |
New Fix Version |
---|---|---|---|
JACINTOREQ-1431 |
Descope all non ETHERNET functionality inside PRU-ICSS subsystem |
08.00.00 |
None |
2.1.9. Installation and Usage¶
The Software Developer’s Guide provides instructions on how to setup up your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications and Code Composer Studio.
2.1.10. Host Support¶
The Processor SDK is developed, built and verified on Ubuntu 16.04 and 18.04. Details on how to create a virtual machine to load Ubuntu are described in this page.
Note
Processor SDK Installer is 64-bit, and installs only on 64-bit host machine. Support for 32-bit host is dropped as Linaro toolchain is available only for 64-bit machines