2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layersetup.sh -f <config>
The following config files are located in the configs/
directory of the configs directory. The yocto config can also be
downloaded directly from the AM65x SDK release page.
Config File | Description | Supported machines |
---|---|---|
processor-sdk-linux-07_00_01.txt | Processor SDK Linux 07_00_01 Release | am65xx-evm |