3.2.2.10. PRP Offload

Introduction

HSR (High-availability Seamless Redundancy) framework in Linux supports HSR and PRP (Parallel Redundancy Protocol) modes of redundancy by using 2 ports. It also allows to offload the below functionalities of PRP mode to the underlying hardware/device:

  • hsr-tag-ins-offload: Add PRP trailer to the frame

  • hsr-dup-offload: Duplicate the outgoing PRP frame

  • hsr-tag-rm-offload: Remove PRP trailer from the frame

The Programmable Real-time Unit and Industrial Communication Subsystem (PRU-ICSS) PRP firmware supports offloading of all above functionalities saving overhead from the driver.

Note

The offload of functionality hsr-fwd-offload should also be enabled for correct driver configuration.

The below script sets up a PRP interface with all possible offload functionalities enabled

#!/bin/sh

#For non offload - sh prp_setup.sh prp_sw <INTF_A> <INTF_B> <PRP_INTF_IP_ADDR>
#For offload - sh prp_setup.sh prp_hw <INTF_A> <INTF_B> <PRP_INTF_IP_ADDR>

if [ "$#" != "4" ]
then
      echo "$0 <prp_sw/prp_hw> <intf1> <intf2> <ip addr>"
      exit
fi

if [ "$1" != "prp_sw" ] && [ "$1" != "prp_hw" ]
then
      echo "$0 <prp_sw|prp_hw>"
      exit
fi

if=prp0

ifa=$2
ifb=$3

ip=$4
mac=$(ifconfig "$ifa" | grep ether | cut -d " " -f 10)

echo "ip=$ip"
echo "if=$if"
echo "mac=$mac"
echo "slave-a=$ifa"
echo "slave-b=$ifb"

ip link set $if down
ip link delete $if  2> /dev/null

ip link set $ifa down
ip link set $ifb down
sleep 1

if [ "$1" = "prp_hw" ]
then
      echo "Available offload features for $ifa: "
      ethtool -k "$ifa" | grep hsr
      ethtool -K "$ifa" hsr-fwd-offload on
      ethtool -K "$ifa" hsr-dup-offload on
      ethtool -K "$ifa" hsr-tag-ins-offload on
      ethtool -K "$ifa" hsr-tag-rm-offload on
      echo "Enabled offload features for $ifa: "
      ethtool -k "$ifa" | grep hsr

      echo "Available offload features for $ifb: "
      ethtool -k "$ifb" | grep hsr
      ethtool -K "$ifb" hsr-fwd-offload on
      ethtool -K "$ifb" hsr-dup-offload on
      ethtool -K "$ifb" hsr-tag-ins-offload on
      ethtool -K "$ifb" hsr-tag-rm-offload on
      echo "Enabled offload features for $ifb: "
      ethtool -k "$ifb" | grep hsr
fi

ip link set dev "$ifa" address "$mac"
ip link set dev "$ifb" address "$mac"

ip link add name $if type hsr slave1 "$ifa" slave2 "$ifb" supervision 45 proto 1

sleep 3

ip addr add "$ip"/24 dev $if
ip link set $if up
ip link set $ifa up
ip link set $ifb up
sleep 1

To create PRP interface with IP address 192.168.1.10 using eth1 and eth2, run the script by passing the arguments as below

sh prp_setup.sh prp_hw eth1 eth2 192.168.1.10

Multicast Filtering

All multi-cast addresses not registered will be filtered out.

Multicast Add/Delete

Multicast MAC address can be added/deleted using ip maddr commands or Linux socket ioctl SIOCADDMULTI/SIOCDELMULTI.

Show multicast address

Show current list of multicast address for the PRP interface

ip maddr show dev <prp_intf>

Example:

# ip maddr show dev prp0
7:      prp0
         link  33:33:00:00:00:01 users 3
         link  01:80:c2:00:00:0e users 3 static
         link  01:80:c2:00:00:03 users 3 static
         link  01:80:c2:00:00:00 users 3 static
         link  01:00:5e:00:00:01 users 3
         link  33:33:ff:1e:a0:a8 users 3
         link  01:00:5e:00:00:fb users 3
         link  33:33:00:00:00:fb users 3
         inet  224.0.0.251
         inet  224.0.0.1
         inet6 ff02::fb
         inet6 ff02::1:ff1e:a0a8
         inet6 ff02::1
         inet6 ff01::1

Add multicast address

Add a multicast address

ip maddr add <multicast_mac_addr> dev <prp_intf>

Example: To add a multicast address and display the list in PRP and slave ports

# ip maddr add 01:80:c4:00:00:0e dev prp0
# ip maddr show dev prp0
7:      prp0
         link  33:33:00:00:00:01 users 3
         link  01:80:c2:00:00:0e users 3 static
         link  01:80:c2:00:00:03 users 3 static
         link  01:80:c2:00:00:00 users 3 static
         link  01:00:5e:00:00:01 users 3
         link  33:33:ff:1e:a0:a8 users 3
         link  01:00:5e:00:00:fb users 3
         link  33:33:00:00:00:fb users 3
         link  01:80:c4:00:00:0e users 3 static
         inet  224.0.0.251
         inet  224.0.0.1
         inet6 ff02::fb
         inet6 ff02::1:ff1e:a0a8
         inet6 ff02::1
         inet6 ff01::1

# ip maddr show dev eth1
5:      eth1
         link  33:33:00:00:00:01 users 3
         link  01:00:5e:00:00:01 users 3
         link  01:80:c2:00:00:0e users 4 static
         link  01:80:c2:00:00:03 users 4 static
         link  01:80:c2:00:00:00 users 4 static
         link  33:33:ff:1e:a0:a8 users 3
         link  33:33:00:00:00:fb users 3
         link  01:00:5e:00:00:fb users 2
         link  01:80:c4:00:00:0e users 2
         inet  224.0.0.1
         inet6 ff02::fb
         inet6 ff02::1:ff1e:a0a8
         inet6 ff02::1 users 2
         inet6 ff01::1

# ip maddr show dev eth2
6:      eth2
         link  33:33:00:00:00:01 users 3
         link  01:00:5e:00:00:01 users 3
         link  01:80:c2:00:00:0e users 4 static
         link  01:80:c2:00:00:03 users 4 static
         link  01:80:c2:00:00:00 users 4 static
         link  33:33:ff:1e:a0:a7 users 2
         link  33:33:00:00:00:fb users 3
         link  33:33:ff:1e:a0:a8 users 2
         link  01:00:5e:00:00:fb users 2
         link  01:80:c4:00:00:0e users 2
         inet  224.0.0.1
         inet6 ff02::fb
         inet6 ff02::1:ff1e:a0a7
         inet6 ff02::1 users 2
         inet6 ff01::1

Delete multicast address

Delete a multicast address

ip maddr del <multicast_mac_addr> dev <prp_intf>

Example: To delete an added multicast address and dislay the list of PRP and slave intefaces.

# ip maddr del 01:80:c4:00:00:0e dev prp0
# ip maddr show dev prp0
7:      prp0
         link  33:33:00:00:00:01 users 3
         link  01:80:c2:00:00:0e users 3 static
         link  01:80:c2:00:00:03 users 3 static
         link  01:80:c2:00:00:00 users 3 static
         link  01:00:5e:00:00:01 users 3
         link  33:33:ff:1e:a0:a8 users 3
         link  01:00:5e:00:00:fb users 3
         link  33:33:00:00:00:fb users 3
         inet  224.0.0.251
         inet  224.0.0.1
         inet6 ff02::fb
         inet6 ff02::1:ff1e:a0a8
         inet6 ff02::1
         inet6 ff01::1

# ip maddr show dev eth1
5:      eth1
         link  33:33:00:00:00:01 users 3
         link  01:00:5e:00:00:01 users 3
         link  01:80:c2:00:00:0e users 4 static
         link  01:80:c2:00:00:03 users 4 static
         link  01:80:c2:00:00:00 users 4 static
         link  33:33:ff:1e:a0:a8 users 3
         link  33:33:00:00:00:fb users 3
         link  01:00:5e:00:00:fb users 2
         inet  224.0.0.1
         inet6 ff02::fb
         inet6 ff02::1:ff1e:a0a8
         inet6 ff02::1 users 2
         inet6 ff01::1

# ip maddr show dev eth2
6:      eth2
         link  33:33:00:00:00:01 users 3
         link  01:00:5e:00:00:01 users 3
         link  01:80:c2:00:00:0e users 4 static
         link  01:80:c2:00:00:03 users 4 static
         link  01:80:c2:00:00:00 users 4 static
         link  33:33:ff:1e:a0:a7 users 2
         link  33:33:00:00:00:fb users 3
         link  33:33:ff:1e:a0:a8 users 2
         link  01:00:5e:00:00:fb users 2
         inet  224.0.0.1
         inet6 ff02::fb
         inet6 ff02::1:ff1e:a0a7
         inet6 ff02::1 users 2
         inet6 ff01::1

Multicast Filtering for VLAN Interfaces

Multicast filtering for VLAN interfaces is also supported.

Show current list of multicast address for the PRP VLAN interface

ip maddr show dev <prp_vlan_intf>

Example:

# ip maddr show dev prp0.5

Add multicast address for the PRP VLAN interface

ip maddr add <multicast_mac_addr> dev <prp_vlan_intf>

Example:

# ip maddr add 01:80:c4:00:00:0e dev prp0.5

Delete multicast address for the PRP VLAN interface

ip maddr del <multicast_mac_addr> dev <prp_vlan_intf>

Example:

# ip maddr del 01:80:c4:00:00:0e dev prp0.5

PTP Support

For PTP support over PRP, see HSR and PRP PTP support.

Performance

This section describes the throughput and CPU usage metrics in the offload case

Setup

A sample test setup is as shown below

../../../../../_images/AM64_PRP_Setup.jpg

Test Procedure

  1. Connect the LAN cables between the DANP DUTs as shown in the setup image

  2. Execute the commands to setup and create PRP interface

    sh prp_setup.sh prp_hw <INTF_A> <INTF_B> <PRP_INTF_IP_ADDR>
    
  3. Confirm ping across all Nodes

    1. Node A < - - > Node B

    2. Node B < - - > Node C

    3. Node C < - - > Node A

  4. Disconnect one of the cable for a node and retry

  5. Monitor the CPU usage on DUTs

    mpstat -P ALL 1
    
  6. Run iperf3 server on Node C

    iperf3 -s
    
  7. Run iperf3 client on Node A for 60 secs

    iperf3 -c -t60 <Node_C_IP_Addr>
    

Througput at Node A

Table 3.4 Throughput performance

Sender

Receiver

610 Mbits/sec

605 Mbits/sec