3.2.2.9. PRP Offload
Introduction
HSR (High-availability Seamless Redundancy) framework in Linux supports HSR and PRP (Parallel Redundancy Protocol) modes of redundancy by using 2 ports. It also allows to offload the below functionalities of PRP mode to the underlying hardware/device:
hsr-tag-ins-offload: Add PRP trailer to the frame
hsr-dup-offload: Duplicate the outgoing PRP frame
hsr-tag-rm-offload: Remove PRP trailer from the frame
The Programmable Real-time Unit and Industrial Communication Subsystem (PRU-ICSS) PRP firmware supports offloading of all above functionalities saving overhead from the driver.
Note
The offload of functionality hsr-fwd-offload should also be enabled for correct driver configuration.
The below script sets up a PRP interface with all possible offload functionalities enabled
#!/bin/sh
#For non offload - sh prp_setup.sh prp_sw <INTF_A> <INTF_B> <PRP_INTF_IP_ADDR>
#For offload - sh prp_setup.sh prp_hw <INTF_A> <INTF_B> <PRP_INTF_IP_ADDR>
if [ "$#" != "4" ]
then
echo "$0 <prp_sw/prp_hw> <intf1> <intf2> <ip addr>"
exit
fi
if [ "$1" != "prp_sw" ] && [ "$1" != "prp_hw" ]
then
echo "$0 <prp_sw|prp_hw>"
exit
fi
if=prp0
ifa=$2
ifb=$3
ip=$4
mac=$(ifconfig "$ifa" | grep ether | cut -d " " -f 10)
echo "ip=$ip"
echo "if=$if"
echo "mac=$mac"
echo "slave-a=$ifa"
echo "slave-b=$ifb"
ip link set $if down
ip link delete $if 2> /dev/null
ip link set $ifa down
ip link set $ifb down
sleep 1
if [ "$1" = "prp_hw" ]
then
echo "Available offload features for $ifa: "
ethtool -k "$ifa" | grep hsr
ethtool -K "$ifa" hsr-fwd-offload on
ethtool -K "$ifa" hsr-dup-offload on
ethtool -K "$ifa" hsr-tag-ins-offload on
ethtool -K "$ifa" hsr-tag-rm-offload on
echo "Enabled offload features for $ifa: "
ethtool -k "$ifa" | grep hsr
echo "Available offload features for $ifb: "
ethtool -k "$ifb" | grep hsr
ethtool -K "$ifb" hsr-fwd-offload on
ethtool -K "$ifb" hsr-dup-offload on
ethtool -K "$ifb" hsr-tag-ins-offload on
ethtool -K "$ifb" hsr-tag-rm-offload on
echo "Enabled offload features for $ifb: "
ethtool -k "$ifb" | grep hsr
fi
ip link set dev "$ifa" address "$mac"
ip link set dev "$ifb" address "$mac"
ip link add name $if type hsr slave1 "$ifa" slave2 "$ifb" supervision 45 proto 1
sleep 3
ip addr add "$ip"/24 dev $if
ip link set $if up
ip link set $ifa up
ip link set $ifb up
sleep 1
To create PRP interface with IP address 192.168.1.10 using eth1 and eth2, run the script by passing the arguments as below
sh prp_setup.sh prp_hw eth1 eth2 192.168.1.10
Multicast Filtering
All multi-cast addresses not registered will be filtered out.
Multicast Add/Delete
Multicast MAC address can be added/deleted using ip maddr commands or Linux socket ioctl SIOCADDMULTI/SIOCDELMULTI.
Show multicast address
Show current list of multicast address for the PRP interface
ip maddr show dev <prp_intf>
Example:
# ip maddr show dev prp0
7: prp0
link 33:33:00:00:00:01 users 3
link 01:80:c2:00:00:0e users 3 static
link 01:80:c2:00:00:03 users 3 static
link 01:80:c2:00:00:00 users 3 static
link 01:00:5e:00:00:01 users 3
link 33:33:ff:1e:a0:a8 users 3
link 01:00:5e:00:00:fb users 3
link 33:33:00:00:00:fb users 3
inet 224.0.0.251
inet 224.0.0.1
inet6 ff02::fb
inet6 ff02::1:ff1e:a0a8
inet6 ff02::1
inet6 ff01::1
Add multicast address
Add a multicast address
ip maddr add <multicast_mac_addr> dev <prp_intf>
Example: To add a multicast address and display the list in PRP and slave ports
# ip maddr add 01:80:c4:00:00:0e dev prp0
# ip maddr show dev prp0
7: prp0
link 33:33:00:00:00:01 users 3
link 01:80:c2:00:00:0e users 3 static
link 01:80:c2:00:00:03 users 3 static
link 01:80:c2:00:00:00 users 3 static
link 01:00:5e:00:00:01 users 3
link 33:33:ff:1e:a0:a8 users 3
link 01:00:5e:00:00:fb users 3
link 33:33:00:00:00:fb users 3
link 01:80:c4:00:00:0e users 3 static
inet 224.0.0.251
inet 224.0.0.1
inet6 ff02::fb
inet6 ff02::1:ff1e:a0a8
inet6 ff02::1
inet6 ff01::1
# ip maddr show dev eth1
5: eth1
link 33:33:00:00:00:01 users 3
link 01:00:5e:00:00:01 users 3
link 01:80:c2:00:00:0e users 4 static
link 01:80:c2:00:00:03 users 4 static
link 01:80:c2:00:00:00 users 4 static
link 33:33:ff:1e:a0:a8 users 3
link 33:33:00:00:00:fb users 3
link 01:00:5e:00:00:fb users 2
link 01:80:c4:00:00:0e users 2
inet 224.0.0.1
inet6 ff02::fb
inet6 ff02::1:ff1e:a0a8
inet6 ff02::1 users 2
inet6 ff01::1
# ip maddr show dev eth2
6: eth2
link 33:33:00:00:00:01 users 3
link 01:00:5e:00:00:01 users 3
link 01:80:c2:00:00:0e users 4 static
link 01:80:c2:00:00:03 users 4 static
link 01:80:c2:00:00:00 users 4 static
link 33:33:ff:1e:a0:a7 users 2
link 33:33:00:00:00:fb users 3
link 33:33:ff:1e:a0:a8 users 2
link 01:00:5e:00:00:fb users 2
link 01:80:c4:00:00:0e users 2
inet 224.0.0.1
inet6 ff02::fb
inet6 ff02::1:ff1e:a0a7
inet6 ff02::1 users 2
inet6 ff01::1
Delete multicast address
Delete a multicast address
ip maddr del <multicast_mac_addr> dev <prp_intf>
Example: To delete an added multicast address and dislay the list of PRP and slave intefaces.
# ip maddr del 01:80:c4:00:00:0e dev prp0
# ip maddr show dev prp0
7: prp0
link 33:33:00:00:00:01 users 3
link 01:80:c2:00:00:0e users 3 static
link 01:80:c2:00:00:03 users 3 static
link 01:80:c2:00:00:00 users 3 static
link 01:00:5e:00:00:01 users 3
link 33:33:ff:1e:a0:a8 users 3
link 01:00:5e:00:00:fb users 3
link 33:33:00:00:00:fb users 3
inet 224.0.0.251
inet 224.0.0.1
inet6 ff02::fb
inet6 ff02::1:ff1e:a0a8
inet6 ff02::1
inet6 ff01::1
# ip maddr show dev eth1
5: eth1
link 33:33:00:00:00:01 users 3
link 01:00:5e:00:00:01 users 3
link 01:80:c2:00:00:0e users 4 static
link 01:80:c2:00:00:03 users 4 static
link 01:80:c2:00:00:00 users 4 static
link 33:33:ff:1e:a0:a8 users 3
link 33:33:00:00:00:fb users 3
link 01:00:5e:00:00:fb users 2
inet 224.0.0.1
inet6 ff02::fb
inet6 ff02::1:ff1e:a0a8
inet6 ff02::1 users 2
inet6 ff01::1
# ip maddr show dev eth2
6: eth2
link 33:33:00:00:00:01 users 3
link 01:00:5e:00:00:01 users 3
link 01:80:c2:00:00:0e users 4 static
link 01:80:c2:00:00:03 users 4 static
link 01:80:c2:00:00:00 users 4 static
link 33:33:ff:1e:a0:a7 users 2
link 33:33:00:00:00:fb users 3
link 33:33:ff:1e:a0:a8 users 2
link 01:00:5e:00:00:fb users 2
inet 224.0.0.1
inet6 ff02::fb
inet6 ff02::1:ff1e:a0a7
inet6 ff02::1 users 2
inet6 ff01::1
Multicast Filtering for VLAN Interfaces
Multicast filtering for VLAN interfaces is also supported.
Show current list of multicast address for the PRP VLAN interface
ip maddr show dev <prp_vlan_intf>
Example:
# ip maddr show dev prp0.5
Add multicast address for the PRP VLAN interface
ip maddr add <multicast_mac_addr> dev <prp_vlan_intf>
Example:
# ip maddr add 01:80:c4:00:00:0e dev prp0.5
Delete multicast address for the PRP VLAN interface
ip maddr del <multicast_mac_addr> dev <prp_vlan_intf>
Example:
# ip maddr del 01:80:c4:00:00:0e dev prp0.5
Performance
This section describes the throughput and CPU usage metrics in the offload case
Setup
A sample test setup is as shown below
Test Procedure
Connect the LAN cables between the DANP DUTs as shown in the setup image
Execute the commands to setup and create PRP interface
sh prp_setup.sh prp_hw <INTF_A> <INTF_B> <PRP_INTF_IP_ADDR>Confirm ping across all Nodes
Node A < - - > Node B
Node B < - - > Node C
Node C < - - > Node A
Disconnect one of the cable for a node and retry
Monitor the CPU usage on DUTs
mpstat -P ALL 1Run iperf3 server on Node C
iperf3 -sRun iperf3 client on Node A for 60 secs
iperf3 -c -t60 <Node_C_IP_Addr>
Througput at Node A
Sender |
Receiver |
610 Mbits/sec |
605 Mbits/sec |