4.1.5. Program MMC boot media
4.1.5.1. Overview
This documentation provides the steps for building flasher image with initramfs-based boot support and programming the MMC device via CPSW Ethernet connection to a Linux host PC. This solution will work with a completely blank board / SK and can be used as a base to create a custom production programming solution.
To achieve this goal the following is required:
Use the SDK to build a separate “flasher” image which can be transferred from the host PC via Ethernet to program the MMC-SD device.
4.1.5.2. What is Needed
The most current Processor SDK for Linux installed on the host Linux PC used for development
SK-AM64B or AM64-EVM board and an ethernet cable to connect the board to the host PC
A 12V and 5V power supply compatible with the AM64-EVM and SK-AM64B respectively.
A Serial Debug Cable is recommended to monitor U-Boot outputs
An image to flash. This can be derived from the SDK mentioned above
A Linux Filesystem small enough to be peripheral booted, with the functionality needed to do the necessary flashing operation. This can be derived from the SDK mentioned above
A Linux host PC to transfer the binary files
A configured TFTP Server
A SD card with pre-built U-Boot images from SDK
4.1.5.3. Configure tftp
Steps to configure a TFTP Server on host PC can be found in TFTP Server
4.1.5.4. Preparing the Flasher Image
First we need to create the flasher image with smaller filesystem on the host PC.
4.1.5.4.1. Prepare a rootfs
Navigate to <Processor-SDK>/filesystem
Refer to prerequisites and steps for Yocto build for an Ubuntu host: Host Setup - Ubuntu (Recommended).
After the Yocto enviroment is setup, use the below step to build the Initramfs Image:
MACHINE=<machine> bitbake -k tisdk-tiny-initramfs
The bitbake command mentioned in the last line above builds the tisdk-tiny-initramfs
cpio which can be located at deploy-ti/images/am64xx-evm
.
4.1.5.4.2. Prepare Kernel with baked-in initramfs
Navigate to your linux repository to build flasher Image
cd <PSDK_PATH>/board-support/linux-[ver]/
Build device defconfig file
make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- defconfig ti_arm64_prune.config
Make a backup copy of
.config
called.config.orig
Edit the current Kernel config using menuconfig as follows:
make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- menuconfig
Set CONFIG_INITRAMFS_SOURCE =
path to cpio/tisdk-tiny-initramfs-am64xx-evm.cpio
Select General setup:
Scroll down to Initial RAM Filesystem and RAM Disk (initramfs/initrd) support and Select it:
Move down a line to Initramfs source file(s). Select it and fill in the location of the files:
![../../../_images/menuconfig.png](../../../_images/menuconfig.png)
Exit menuconfig and save the new configuration.
4.1.5.4.3. Build the Kernel
Compile the
zImage
make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- Image
Copy
arch/arm64/boot/Image
to/tftpboot
4.1.5.5. Target Images
Populate pre-built U-Boot images from SDK into TFTP folder
Note
We can use the prebuilt U-Boot images as-is with no modifications needed
Populate bootloaders into the TFTP home directory
Copy
tiboot3.bin
,tispl.bin
andu-boot.img
files fromProcessor-SDK/board-support/prebuilt-images/am64xx-evm/
to the~/tftpboot
directory
Populating rootfs into the TFTP home directory.
Download the default bootable SD card image (WIC file) available on the release page as
tisdk-default-image-machine.wic.xz
Copy wic image to root directory
/tftpboot
4.1.5.6. Program the Flash
Now that the flash image has been created we can now flash the SK
Note
In SK the TFTP server must be properly configured to transfer the flash image.
Connect SK to Linux host machine via Serial Debugging Cable
Open an active console window to monitor bootup messages
Connect ethernet cable to board
Boot the board in SD boot mode and “strike any key” to halt U-Boot at prompt
Enter the following commands
setenv serverip <SERVER_IP> dhcp
For creating eMMC boot partiton refer here
For writing bootloaders into eMMC boot partition
mmc dev 0 1
tftp ${loadaddr} tiboot3.bin
mmc write ${loadaddr} 0x0 0x400
tftp ${loadaddr} tispl.bin
mmc write ${loadaddr} 0x800 0x1000
tftp ${loadaddr} u-boot.img
mmc write ${loadaddr} 0x1800 0x2000
To give the ROM access to the boot partition, the following commands must be used for the first time:
mmc partconf 0 1 1 1
mmc bootbus 0 2 0 0
Enter command to boot Linux using initramfs image from TFTP server
run findfdt tftp ${loadaddr} Image tftp ${fdtaddr} ${name_fdt} booti ${loadaddr} - ${fdtaddr}
Enter the following command on Host PC’s Linux shell to transfer the wic image
tftp -b 1468 -g -r tisdk-default-image-am64xx-evm.wic.xz <SERVER_IP>
Flash the image into MMC-SD
dd if=tisdk-default-image-am64xx-evm.wic.xz of=/dev/mmcblk1
Now reboot the board with SD boot mode and verify that it boots successfully