3. Building Debian Images
3.1. Introduction
Building a Debian Image requires:
Generating a chroot environment for the target architecture (Arm), if the host environment is on x86.
Installing all the necessary packages
Customizing configuration scripts if needed
Building Bootloader
Flashing the generated RootFS and Boot binaries to SD Card
There are several opensource tools available for generating the RootFS in a chroot environment. Such as debootstrap (now deprecated), mmdebstrap (complex), bdebstrap (simple wrapper on top of mmdebstrap).
ti-bdebstrap is a set of scripts that builds upon the bdebstrap
tool to create custom Debian images for TI platforms. This includes creating the bdebstrap
chroot environment itself, installing essential and useful TI and non-TI packages, setting up the configuations, Building the U-Boot etc.
In other words, ti-bdebstrap
offers users an easy way to create a full-fledged Debian image for supported TI platforms, using a single command. Once the image is built, the user can directly flash it onto a SD card.
TI currently supports building Debian Bookworm Images for AM62Px, AM62x and AM64x platforms.
3.2. Usage
3.2.1. Get Scripts
The scripts are hosted at https://github.com/TexasInstruments/ti-bdebstrap
To clone the repository, run:
git clone https://github.com/TexasInstruments/ti-bdebstrap.git
3.2.2. Repository Structure
ti-bdebstrap
├── build.sh
├── builds.toml
├── configs
│ ├── bdebstrap_configs
│ │ ├── am62-bookworm.yaml
│ │ ├── am62p-bookworm.yaml
│ │ ├── am64-bookworm.yaml
│ ├── bsp_sources.toml
│ └── machines.toml
├── LICENSE
├── README.md
├── scripts
│ ├── build_bsp.sh
│ ├── build_distro.sh
│ ├── common.sh
│ └── setup.sh
├── target
│ └── files for target configs
build.sh
: the “main” script that the user should run to generate Debian images.
configs/
: contains details, configuration options and values for machines, bsp_sources and distro-variants (see below for details).
scripts/
: contains helper scripts for build.sh
.
target/
: contains files for target configs, like weston.service
for the weston target.
builds.toml
: contains list of all valid builds along with their definitions (see below for details).
3.2.3. Build Configurations
A build config
represents an image with certain values for the machine
, bsp_version
and distro_variant
parameters.
The builds.toml
file contains a list of all valid builds in the builds[]
list. Each build
is then defined underneath.
Values of machine
, bsp_version
and distro-variant
must be defined in configs/machines.toml
, configs/bsp_sources.toml
and configs/bdebstrap_configs/<distro-variant>.yaml
files. If any of these is missing, the build will fail.
So long as you conform to the rule above, you may also define your own builds.
3.2.4. Building Images
All valid builds are listed in the builds.toml
file. To build an image, one of these must be chosen and supplied to the build.sh
command. build.sh
commences the build process.
The images are finally stored in the build/
directory. Each build also produces a log file inside log/
.
Building images using ti-bdebstrap
involves the following steps:
install the pre-requisite packages
get the scripts using
git clone
run the
build.sh
script and with required build config as argument.flashing the image into a SD card
3.2.5. Install Pre-requisite Packages
First, ensure that your repositories are up-to-date:
sudo apt update
Then, install packages as follows:
sudo apt install -y \
pigz expect pv \
binfmtc binfmt-support \
qemu-user qemu-user-static qemu-system-arm \
debian-archive-keyring bdebstrap \
build-essential autoconf automake \
bison flex libssl-dev \
bc u-boot-tools swig python3-pyelftools
Ensure that all packages were correctly installed using:
sudo apt install --fix-broken
Finally, install toml-cli
:
pip3 install toml-cli
Note
Since the build script is run as root user, toml-cli should also be installed with sudo for root user to be able to access it.
Note
The scripts internally handle toolchain downloads based on Host architecture. So the same steps can be followed on both arm and x86_64 hosts.
3.2.6. Building the Image
Note
If you are behind a proxy, since the build is run with sudo, make sure to set the proxy for root user (preferably in /etc/environment
).
To build an image, you need to run the build.sh
script:
sudo ./build.sh <build-name>
The <build-name>
must be one present inside builds.toml
file.
After the build, the RootFS, Boot partition and bsp_sources are stored in build/<build-name>
. The logs will be stored in logs/<build-name>.log
.
Example: to build for am62-bookworm-09.02.01.010
, run:
sudo ./build.sh am62-bookworm-09.02.01.010
The RootFS, Boot partition and bsp_sources are then stored in build/am62-bookworm-09.02.01.010
. The build log is saved as logs/am62-bookworm-09.02.01.010.log
.
3.2.7. Generate an SD Card Image
This step can be skipped if you do not want to share the generated Image with anyone and want to proceed with testing with an SD card.
To generate an SD Card Image with the generated RootFS and Boot partition files, run:
./create-wic.sh <build-name>
Example: to build for am62-bookworm-09.02.01.010
, run:
./create-wic.sh am62-bookworm-09.02.01.010
The wic image is generated under build/am62-bookworm-09.02.010
. This can be used to flash an SD card using standard tools like balena-etcher.
3.2.8. Flash Image to SD Card using Script
To flash the SD card without generating a wic image, use the create-sdcard.sh
script. Run it using the below command and follow with the prompts.
sudo ./create-sdcard.sh <build-name>
For example, if the image is am62-bookworm-09.02.01.010, type:
sudo ./create-sdcard.sh am62-bookworm-09.02.01.010
This script will partition the SD Card and copy the contents of RootFS and Boot partitions that are generated to the SD Card.