3.7. OP-TEEΒΆ

Overview

OP-TEE is a Trusted Execution Environment (TEE) designed as companion to a non-secure Linux kernel running on Arm; Cortex-A cores using the TrustZone technology. OP-TEE implements TEE Internal Core API v1.1.x which is the API exposed to Trusted Applications and the TEE Client API v1.0, which is the API describing how to communicate with a TEE. Those APIs are defined in the GlobalPlatform API specifications.

Getting the OP-TEE Source Code

$ git clone https://github.com/OP-TEE/optee_os.git

Getting Security Dev Tool

$ git clone git://git.ti.com/security-development-tools/core-secdev-k3.git -b master
$ export TI_SECURE_DEV_PKG=`pwd`/core-secdev-k3

Building OP-TEE

on GP
$ make CROSS_COMPILE64=aarch64-linux-gnu- PLATFORM=k3-am65x CFG_ARM64_core=y
on HS
$ make CROSS_COMPILE64=aarch64-linux-gnu- PLATFORM=k3-am65x CFG_ARM64_core=y
$ {TI_SECURE_DEV_PKG}/scripts/secure-binary-image.sh ./out/arm-plat-k3/core/tee-pager_v2.bin ./out/arm-plat-k3/core/tee-pager_v2.bin.signed