2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM64x installer provides, everything needed to create the embedded system from “scratch”, with...
- Platform/board-support software and configuration files for Linux
- U-Boot and Kernel sources and configuration files
- An ARM cross-compiling toolchain as well as other host binaries and components
- A Yocto/OE compliant filesystem and sources for example applications
- A variety of scripts and Makefiles to automate certain tasks
- Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
- Reference Examples, benchmarks
2.1.2. Licensing¶
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
- Linux Manifest: “/docs/software_manifest.htm”
- App/Demos Manifest: “/sitara-apps/Processor_SDK_manifest.html”
2.1.3. Release 07.03.00¶
Released on March 2021
What’s New
Processor SDK Linux AM64x Release has following new features:
This release integrates benchmark examples built on top of RTOS, NO-RTOS and Linux platform software. Refer to highlights per subsystem for more detailed information.
Benchmark Demo:
- Benchmark_demo with GUI (A53/Linux) working for all 4 R5F/NO-RTOS cores with u-boot based SD card boot
- 4-ch IPC RPMsg_char functional between R5F/NO-RTOS and A53/Linux
- Benchmarking R5F apps such as CFFT, FIR and FOC with profile/cycle counts
Platform SW/board-support
- Integrated with latest tools and Platform SW releases
Dependent component Release notes
Refer below component release notes for complete feature-set and further details
- For Linux Kernel, u-boot & DTB [Use Link]
- For RTOS/NO-RTOS source (MCU+ SDK) [Use Link]
- For Industrial Protocols (ECAT) [Use Link]
- For Industrial Drives (EnDAT,HDSL) [Use Link]
Known Issues
- None
Issues Fixed
- This is the first release of Processor SDK Linux AM64X.