2.2. Yocto Layer Configuration

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>

The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.

Config File

Description

Supported machines/platforms

processor-sdk-scarthgap-chromium-11.00.09.04-config.txt

Processor SDK 11.00.09.04 Release

am62xx-evm, am62xx-lp-evm, beagleplay-ti

processor-sdk-scarthgap-11.00.09.04-config.txt

Processor SDK 11.00.09.04 Release

am62xx-evm, am62xx-lp-evm, beagleplay-ti

processor-sdk-scarthgap-selinux-11.00.09.04-config.txt

Processor SDK 11.00.09.04 Release

am62xx-evm, am62xx-lp-evm, beagleplay-ti

The oe-layersetup configuration, as defined in processor-sdk-scarthgap-chromium-11.00.09.04-config.txt, is used for configuring the meta layers in the yocto SD card image available on AM62x-SDK-Download-page.