3.6.5. Flash via UART
This tool uses UART as the transport or interface to send the file to flash to the EVM.
The UART Flash tool is part of MCU+SDK installer and can be downloaded from AM62x-SDK-Download-page.
Detailed instructions on using the tool can be found in MCU+SDK docs.