2.1. Release Notes

2.1.1. Overview

The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.

To simplify the end user experience, Processor SDK Linux AM62x installer provides everything needed as discussed below to create the embedded system from “scratch” :

  • Platform/board-support software and configuration files for Linux

  • U-Boot and Kernel sources and configuration files

  • An ARM cross-compiling toolchain as well as other host binaries and components

  • A Yocto/OE compliant filesystem and sources for example applications

  • A variety of scripts and Makefiles to automate certain tasks

  • Other components needed to build an embedded system that don’t fit neatly into one of the above buckets

  • Reference Examples, benchmarks

This release supports High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide

2.1.2. Licensing

Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.

  • Linux Manifest: <PSDK_PATH>/docs/software_manifest.html

2.1.3. Release 10.01.10.04

Released on December 2024

2.1.3.1. What’s new

Processor SDK Linux AM62X Release has following new features:

Component version:

  • Kernel 6.6.58

  • RT Kernel 6.6.58-rt45

  • U-Boot 2024.04

  • Toolchain GCC 13.3

  • ATF 2.11+

  • OPTEE 4.4.0

  • Graphics DDK 24.1

  • TIFS Firmware v10.01.08

  • DM Firmware 10.01.00.10

  • Yocto scarthgap 5.0

2.1.4. Build Information

2.1.4.1. U-Boot

u-boot

Head Commit: 29d0c23d67ee7b88e46fe1753cd020e2b04c2ef6 arm: mach-k3: common: Print TIFS context save addr on resume
uBoot Version: 2024.04
uBoot Description: RC Release 10.01.10
Clone: git://git.ti.com/ti-u-boot/ti-u-boot.git
Branch: ti-u-boot-2024.04
uBoot Tag: 10.01.10

2.1.4.2. TF-A

Head Commit: 58b25570c9ef91753b14c2103f45f4be9dddb696 Merge “feat(ti): implement DM_MANAGED suspend” into integration
Branch: master
Tag: 2.11+

2.1.4.3. OP-TEE

Head Commit: 8f645256efc0dc66bd5c118778b0b50c44469ae1 Update CHANGELOG for 4.4.0
Branch: master
Tag: 4.4.0

2.1.4.4. ti-linux-firmware

Head Commit: 1eaf07dc4ec5cdeb98078f17a9d4635e88f43f75 ti-dm: Update display sharing firmware for am62px
Branch: ti-linux-firmware
Tag: 10.01.10

2.1.4.5. Kernel

Linux Kernel

Head Commit: a7758da17c2807e5285d6546b6797aae1d34a7d6 driver core: fw_devlink: Stop trying to optimize cycle detection logic
Kernel Version: 6.6.58
Kernel Description: RC Release 10.01.10
Repo: git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git
Branch: ti-linux-6.6.y
Tag: 10.01.10
use-kernel-config=defconfig
config-fragment=kernel/configs/ti_arm64_prune.config

Real Time (RT) Linux Kernel

Head Commit: c79d7ef3a56ff61dd83d5527520b419a4f0e32e2 Merge branch ‘ti-linux-6.6.y-cicd’ of https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel into ti-rt-linux-6.6.y-cicd
Kernel Version: 6.6.58-rt45
Kernel Description: RC Release 10.01.10-rt
Repo: git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git
Branch: ti-rt-linux-6.6.y
Tag: 10.01.10-rt
use-kernel-config=defconfig
config-fragment=config-fragment=kernel/configs/ti_arm64_prune.config kernel/configs/ti_rt.config

2.1.4.6. Yocto

meta-ti

Head Commit: 50acaea23568f72121020a97bf13869770929cb7 CI/CD Auto-Merger: cicd.scarthgap.202412030400
Clone: git://git.yoctoproject.org/meta-ti
Branch: scarthgap
Release Tag: 10.01.10

meta-arago

Head Commit: 2b1f8572ac54cd64ca5d5b40e344bb32b00a05f5 CI/CD Auto-Merger: cicd.scarthgap.202412030400
Clone: git://git.yoctoproject.org/meta-arago
Branch: scarthgap
Release Tag: 10.01.10

meta-tisdk

Head Commit: fcd7661087b0dd5b5b57d30ba0d45f2698e962f8 Jailhouse: Update SRCREV for 10.01.10 tag
Branch: scarthgap
Release Tag: 10.01.10.04

meta-edgeai

Head Commit: 4cba875d5173dee6b4ca34bd41d5a8b47891e0c7 ti-tidl: Update concerto SRC_REV
Date: 2024-12-04 12:21:41 -0600
Branch: scarthgap
Release Tag: 10.01.10.04

Important

meta-edgeai layer is not applicable in case of SK-AM62-SIP (i.e. am62xxsip-evm)

2.1.5. Issues Tracker

Note

  • Release Specific Issues including details will be published through Software Incident Report (SIR) portal

  • Further Information can be found at SIR Portal

2.1.5.1. Errata Resolved

Record ID

Title

EXT_EP-12128

USB2 PHY locks up due to short suspend

EXT_EP-12123

USART: Erroneous clear/trigger of timeout interrupt

EXT_EP-12124

BCDMA: RX Channel can lockup in certain scenarios

EXT_EP-12125

i2327: RTC: Hardware wakeup event limitation

2.1.5.2. Errata Open

Record ID

Title

EXT_EP-12114

MMCSD: HS200 and SDR104 Command Timeout Window Too Small

2.1.5.3. Issues Resolved

Record ID

Title

EXT_EP-12108

audit for potential bugs with 6.6.44 stable merge

EXT_EP-12098

Uboot docs: document renaming tiboot3-<evm>.bin file

EXT_SITMPUSW-29

TI Debian SDK: Docker not working

EXT_SITMPUSW-31

IPC Firmwares missing from base images.

EXT_EP-12061

Single Link LVDS is broken with 10.0

EXT_EP-12103

PHY configs not restored after suspend-resume

EXT_EP-12058

rcu_preempt self-detected stall on CPU while running DSS usecases

EXT_EP-12102

Linux: AM62 USB interoperability broken as LPM is enabled

EXT_EP-12062

OSPI NAND Flash write issues with SK-AM62-LP

EXT_EP-12083

GPIO doesn’t maintain state during suspend/resume

EXT_EP-12096

AM62*: CAN: mcu_mcan0 regression

EXT_EP-12094

AM62x: incorrect PRUSS clock ID in device tree

EXT_EP-12093

GPIO glitch observed while resuming from DeepSleep

EXT_EP-12056

8250_omap: incorrect handling of dma->rx_running flag

EXT_EP-12086

copying files to eMMC causes kernel crash

SITSW-5794

TISCI Messages from A53_4 are not receiving a response

SITSW-4773

DM is ignoring the exact flags sent in TISCI message

SYSFW-5992

Unable to set exact pixel clock for OLDI LCD display / HDMI Pixel clock

SYSFW-6426

Ownership of a firewall region can be transferred to an invalid host

SYSFW-6432

Set device API doesn’t return Error when PD is in transition state

SYSFW-7571

Device IDs higher than 255 does not work with set device constraint API

SYSFW-7602

RTC count value not getting updated after DeepSleep exit

SYSFW-7614

Unable to configure DSS clock below 15.625MHz

SYSFW-7617

LPM mode selection logic does not check for constraints on all the hosts/devices

SYSFW-7739

LPM constraint messages received by TIFS not forwarded to DM

SYSFW-7740

Only the last latency constraint value passed from a host considered in LPM selection

EXT_SITMPUSW-32

SDK Makefile: Fix logic to pick key directory for mkimage

2.1.5.4. Issues Open

Record ID

Title

EXT_EP-12111

Linux SDK v10.0: TI-added support for W25N01JW SPI NAND breaks other existing Flash support

EXT_EP-12075

U-boot gets stuck when DDR size changed to 512 MB

EXT_EP-12051

AM64x: Linux hangs on repetitive probe/removal of gadget zero

EXT_EP-12066

CPSW EST schedule triggers netdev watchdog

EXT_EP-12065

CPSW Ethernet EST schedule is not taken down on link down

EXT_EP-12071

sdk-doc: missing SK-AM64B information in CDNS3 USB page

EXT_EP-12076

copying files to eMMC triggers cqe error

EXT_EP-12074

ti-rpmsg-char: Squash resource leaks

EXT_EP-12072

misleading GPMC message in kernel log

EXT_EP-12112

Add Timer PWM documentation and other infrastructure as needed

EXT_EP-12060

AM64x: Lower core count on variant devices no supported

EXT_EP-12081

AM62x: Make “Debugging SPL” doc specific to AM62x

SYSFW-7622

DeepSleep resume failure when RTC wake is set for 1 second

SYSFW-7781

Get device API does not return error when the LPSC is in transition state

SYSFW-7887

DeepSleep fails if entered immediately after bootup

SYSFW-7884

There is an additional divide by 4 on all clocks of WKUP/MCU GPIO clock mux

SYSFW-7898

Switching between MCU-Only and DeepSleep mode fails after some iterations