3.9.7. QT Graphics Framework
Qt is a powerful C++ toolkit for writing cross-platform graphics applications, enabling a single code base to run predictably and perform well on Windows and embedded platforms,
Please refer https://www.qt.io/ for additional details on Qt.
The PSDK target file system includes the pre-built Qt libraries under
/usr/lib
and a rich set of QT demo applications under
/usr/share/qt5/examples
.
3.9.7.1. Demos
Demos using the Null Window System / KMS / DRM / EGLFS are
provided with Qt. By default EGLFS will use the eglfs_kms
backend.
$ /usr/share/qt5/examples/opengl/hellogles3/hellogles3 -platform eglfs
$ /usr/share/qt5/examples/opengl/2dpainting/2dpainting -platform eglfs
$ /usr/share/qt5/examples/opengl/paintedwindow/paintedwindow -platform eglfs
The default eglfs_kms
configuration file for Qt5 is located at
/etc/qt5/eglfs_kms_cfg.json
.
For more information about Qt’s EGLFS and using Qt5 in embedded applications see:
3.9.7.2. QT QPA
The QT5 within PSDK is prebuilt with Wayland enabled and therefore
wayland-egl is the default QPA. Hence all QT applications should be run
on top of Weston. To run QT application without Weston, the user can use
-platform
option to specify the desired QPA as linuxfb
or eglfs
.
Note
The linuxfb
inteface is deprecated and requires switching the display
into legacy fb mode.
For example:
$ /usr/share/qt5/examples/opengl/2dpainting/2dpainting -platform eglfs
3.9.7.3. Running QT Applications with the Weston IVI shell
To run the QT application with ivi-shell, set the
QT_WAYLAND_SHELL_INTEGRATION
environment variable to ivi-shell.
$ export QT_WAYLAND_SHELL_INTEGRATION=ivi-shell