3.2.2.7. EQEP

Introduction

Linux has support for EQEP (Enhanced Quadature Encoder Pulse). EQEP channels can be used to interface with rotary encoder hardware.

  • AM62x SK: EQEP0: k3-am62x-sk-eqep.dtso

Kernel Configuration

Using menuconfig, enable the following driver:

Device Drivers --->
   <M> Counter support  --->
      <M> TI eQEP counter driver

Note

EQEP driver should be enabled by default as a kernel module in TI Linux kernel.

Features supported in TI SDK

  • position

  • overflow/underflow events

  • direction

  • unit timer

  • latched position

  • edge capture

Using eQEP with SYSFS interface

To check if eQEP is enabled with sysfs interface, check for the existance of the following directory: /sys/bus/counter and run the following command to find the name of counter:

root@am62xx-evm:~# cd /sys/bus/counter/devices
root@am62xx-evm:/sys/bus/counter/devices# cat counter0/name
23200000.counter
root@am62xx-evm:/sys/bus/counter/devices#

The counter name shows this is eQEP0 at base adress 23200000.

Several sysfs attributes are generated by the Generic Counter interface, and reside under the /sys/bus/counter/devices/counterX directory, where X is to the respective counter device id.

Please see the counter sysfs documentation upstream or in TI Linux kernel /Documentation/ABI/testing/sysfs-bus-counter for detailed information on each generic counter interface sysfs attribute.

Through these sysfs attributes, programs and scripts may interact with the Generic Counter paradigm Counts, Signals, and Synapses of respective counter devices.

The following sysfs atributes can be found in /sys/bus/counter/devices/counterX in TI SDK:

  • countY/ceiling

  • countY/count

  • countY/direction

  • countY/enable

  • countY/function

  • countY/latched_count

  • countY/signal0_action

  • countY/signal1_action

  • edge_capture_unit_enable

  • edge_capture_unit_latched_period

  • edge_capture_unit_max_period

  • edge_capture_unit_prescaler

  • latch_mode

  • unit_timer_enable

  • unit_timer_period

  • unit_timer_time

Character device nodes

Counter character device nodes are created under the /dev directory as counterX, where X is the respective counter device id.

$ ls /dev/counter*
/dev/counter0

Counter Events

Please read the generic counter API upstream or in TI Linux kernel /Documentation/driver-api/generic-counter.rst documentation to implement events:

Test eQEP on AM62x SK

../../../../_images/am62x_sk_eqep.jpg ../../../../_images/am62x_sk_rotary_encoder_breakout.jpg

AM62x SK & rotary encoder breakout board

Example Diligent rotary encoder breakout board

The example rotary encoder breakout board used in this example can be found here.

The following is an example for testing eQEP using sysfs interface:

root@am62xx-evm:~# echo 0xff > /sys/bus/counter/devices/counter0/count0/ceiling
root@am62xx-evm:~# cat /sys/bus/counter/devices/counter0/count0/ceiling
255
root@am62xx-evm:~# echo 1 > /sys/bus/counter/devices/counter0/count0/enable
root@am62xx-evm:~# cat /sys/bus/counter/devices/counter0/count0/count
0
root@am62xx-evm:~# cat /sys/bus/counter/devices/counter0/count0/count
92
root@am62xx-evm:~# cat /sys/bus/counter/devices/counter0/count0/count
148
root@am62xx-evm:~# cat /sys/bus/counter/devices/counter0/count0/count
188
root@am62xx-evm:~# cat /sys/bus/counter/devices/counter0/count0/count
252
root@am62xx-evm:~# cat /sys/bus/counter/devices/counter0/count0/count
12

Notice in this example that turning the rotary shaft encoder counterclockwise increases the count until reaching the ceiling, then wraps around to zero and starts again. Also, turning the rotary shaft encoder clockwise decreases the count.