3.2.2.9.3.2. TSN with CPSW¶
3.2.2.9.3.2.1. Introduction¶
TI Common Platform Ethernet Switch (CPSW) supports TSN features such as:
PTP (Precision Time Protocol) [IEEE-1588, IEEE-802.1AS]
EST (Enhancements for Scheduled Traffic) [IEEE-802.1Qbv]
FQTSS / CBS (Credit Based Shaper) [IEEE-802.1Qav]
IET (Interspersing Express Traffic) [IEEE-802.3br, IEEE-802.1Qbu]
Note
All TSN features require CONFIG_TI_AM65_CPTS to be enabled.
Note
Switch based TSN features are supported only with CPSWxg for x >= 3.
3.2.2.9.3.2.2. Documentation and Testing¶
The documentation for each of the TSN features along with the tests are present at:
3.2.2.9.3.2.3. Testing Details¶
The tests have been performed on TI’s J7VCL with CPSW5G in QSGMII/SGMII modes and on TI’s AM625-SK with CPSW3G in RGMII mode.
TI’s AM64-SK with CPSW3G in RGMII mode has been used to assist in the testing process.
TSN testing has been done in MAC mode as well as SWITCH mode.
The test setup and the scripts are documented in this page to help replicate the tests with appropriate changes if required.
The outputs for each of the performed tests have also been documented.
For all the tests, CONFIG_TI_K3_AM65_CPTS has to be enabled in kernel config.
For tuning the TSN features in Switch Mode, refer TSN Switch Tuning Guide