2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM62x installer provides everything needed as discussed below to create the embedded system from “scratch” :
- Platform/board-support software and configuration files for Linux
- U-Boot and Kernel sources and configuration files
- An ARM cross-compiling toolchain as well as other host binaries and components
- A Yocto/OE compliant filesystem and sources for example applications
- A variety of scripts and Makefiles to automate certain tasks
- Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
- Reference Examples, benchmarks
This release supports High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide
2.1.2. Licensing¶
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
- Linux Manifest: “/docs/software_manifest.html”
2.1.3. Release 09.00.00¶
Released on July 2023
2.1.3.1. What’s new¶
Processor SDK Linux AM62x Release has following new features:
- New improved OOB experience
- Jailhouse Hypervisor with various use-cases
- SEVA store (Demo store/Apps Gallery)
- Debian distribution
- Kirkstone filesystem on Yocto based distribution
- Binman Migration across all K3 platforms for Uboot builds
- HS-FS Default Boot Experience for AM62x
- A53 Early Splash-Screen
- Low Power: Deep Sleep on HS-FS, MCU Only mode and more wakeup sources
Major Refresh of component version:
- Kernel 6.1
- U-Boot 2023.04
- Toolchain GCC 11.2
- ATF 2.8+
- OPTEE 3.20
- Graphics DDK 23.1
2.1.4. Build Information¶
2.1.4.1. U-Boot¶
u-boot
2.1.4.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
2.1.4.3. Yocto¶
meta-ti
meta-arago
2.1.5. Issues Tracker¶
2.1.5.1. Issues opened in previous releases that were closed in this release¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-32790 | am62axx_sk-fs | AM62A: VPU: Module load/unload in loop fails after bootup | |
| LCPD-30075 | am62axx_sk-fs,am62axx_sk-se | AM62ax: Enable distro bootcommand | |
| LCPD-29949 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,j721e-idk-gw | [PROD STOP]I2c operations at 100KHz is broken | |
| LCPD-29792 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | am62x: mcspi not functional | |
| LCPD-29589 | am62axx_sk-fs,am62xx-lp-sk,am62xx_lp_sk-fs,am62xx-sk,am62xx_sk-fs,am62xx_sk-se | AM62x CPSW: PPS example not enabled by default | |
| LCPD-29441 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | am62x: kingston emmc fails on AM62x | |
| LCPD-29339 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Processor SDK 8.3 AM62x lacks RT Linux performance numbers | |
| LCPD-29300 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | U-Boot: OSPI-NOR: sf probe shows 0 randomly | |
| LCPD-28950 | am62axx_sk-fs | CSI2 Multi-capture channel 0 not working | |
| LCPD-28764 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | AM62x: Cannot resume from low power mode | |
| LCPD-28688 | am62axx_sk-fs,am62xx-lp-sk,am62xx_lp_sk-fs,am62xx-sk,am62xx_sk-fs,am62xx_sk-se,am64xx-evm,am64xx-sk | AM62x Kernel User Guide: Document AM62x default kernel config | |
| LCPD-28614 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | AM62x: RPMsg client driver sample does not work | |
| LCPD-28415 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | AM62: emmc: Had to disable higherspeeds | |
| LCPD-28414 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | AM62x EVM Devicetree should disable unused MCU peripherals | |
| LCPD-25662 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,j721e-evm,j7200-evm | Remove SGX PVR tools from KS3 devices | |
| LCPD-24691 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,am64xx-evm,j721s2-evm,j721s2_evm-fs,j7200-evm | Kernel: Upstream: Set HIGH_SPEED_EN for MMC1 instance | |
| LCPD-24690 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,am64xx-evm,am64xx-sk,j721s2-evm,j721s2_evm-fs,j7200-evm | Kernel: SDK: Set HIGH_SPEED_EN for MMC1 instance |
2.1.5.2. Issues found and closed in this release that may also be applicable to prior releases¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-34980 | am62axx_sk-fs | Serial Nand flash is not discovered from uboot and kernel | |
| LCPD-34976 | am62axx_sk-se | AM62a: HS-SE : Fails to boot : Firewall Exception | |
| LCPD-34967 | am62axx_sk-fs | AM62a: SD Boot fails with warning “alloc space exhausted” | |
| LCPD-34966 | am62axx_sk-fs,am62xx-lp-sk,am62xx-sk,am62xx_sk-fs,am64xx-evm,am64xx-sk,j721e-evm-ivi,j721e-idk-gw,j721e-sk,j721s2-evm,j784s4-evm | rpmsg_ctrl device mapping errors see with 6.1 kernel | |
| LCPD-34896 | am62xx_lp_sk-fs | AM62x-LP: RT Kernel fails to boot due to PRU | |
| LCPD-34852 | am62xx_sk-se,am64xx-evm,am654x-evm,j721e-idk-gw,j721s2-evm,j7200-evm | Few times payload is packed at size boundary by binman | |
| LCPD-34836 | am62xx_lp_sk-fs | AM62-lp-sk: USB Audio device missing in test farm | |
| LCPD-34686 | am62axx_sk-fs,am64xx-evm | MMC itapdly sel values are not specified in uboot DTS | |
| LCPD-34593 | am62axx_sk-fs,am62xx-sk,am62xx_sk-fs,am64xx-evm,am64xx-hsevm,am654x-evm,am654x-idk,am654x-hsevm,beagleplay-gp | DISTRO BOOT: Not enabled on all Sitara Platforms | |
| LCPD-34519 | am62axx_sk-fs,am62xx-sk,am68_sk-fs,j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm | IPC: IPC_S_FUNC_RPMSG_SAMPLE_CLIENT test failures | |
| LCPD-34378 | am62xx_lp_sk-fs | U-Boot: AM62x document SRAM layout | |
| LCPD-34354 | am62xx-sk,am62xx_sk-fs | Doc: Power Management Arch: Board name misspelled | |
| LCPD-34301 | am62axx_sk-fs,am62xx-lp-sk,am62xx-sk | Enabling clock output on AUDIO_EXT_REFCLK1 pin | |
| LCPD-34131 | am62xx_sk-fs | AM62: Boot inconsistencies on HS FS | |
| LCPD-32945 | am62xx-lp-sk,am62xx_lp_sk-fs,am62xx-sk,am62xx_sk-fs | AM62x USB-DFU Boot is broken in R5 SPL |
2.1.5.3. Errata Workarounds Available in this Release¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-27887 | am62xx-sk,am62xx_sk-fs | i2327: RTC: Hardware wakeup event limitation | None |
| LCPD-27886 | am62axx_sk-fs,am62xx-sk,am64xx-evm,j721e-idk-gw,j7200-evm,j784s4-evm,j784s4-hsevm | USART: Erroneous clear/trigger of timeout interrupt |
2.1.5.4. U-Boot Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-34929 | am62axx_sk-fs | Remoteproc load of C7x from U-boot fails on 9.0 RC3 | |
| LCPD-34398 | am62axx_sk-fs | Uboot: AM62a boot reporting wrong SOC name | |
| LCPD-28503 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,am64xx-evm,am64xx-sk | Need to sync up DTS files between u-boot and kernel for at least AM62x, possibly other boards too |
2.1.5.5. Linux Kernel Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-35056 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | ‘Error: “main_cpsw0_qsgmii_phyinit” not defined’ on AM62x | |
| LCPD-35055 | am62xx-lp-sk,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx-sk,am62xx_sk-fs,am62xx_sk-se | ERROR: reserving fdt memory region failed on AM62x | |
| LCPD-35054 | am62xx_lp_sk-fs,am62xx_lp_sk-se | AM62x LP fitImage boot issue with Yocto images |
|
| LCPD-35043 | am62axx_sk-fs | Doc: VPU performance and capabilities shown incorrectly for AM62Ax | |
| LCPD-35042 | am62xx-sk,am62xx_sk-fs,am62xx_sk-hs4,am62xx_sk-hs5,am62xx_sk-se | Linux: AM62x: OSPI NOR Flash read speed is low (~2.5MBPS) | |
| LCPD-35025 | am62xx_sk-fs | Test gap: Implement automated test for Driver suspend resume | |
| LCPD-35007 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | AM62x: ip adress not assigned by default on AM62x | |
| LCPD-34991 | am62axx_sk-fs | systemd failure with vmalloc overflow error when using fitimage | |
| LCPD-34978 | am62xx-sk,am62xx_sk-fs | AM62x: High tiny-image cpio file size | |
| LCPD-34916 | am62xx-sk,am62xx_sk-fs | AM62x: op-tee with LOG_LEVEL=2 crashes after Deep Sleep | |
| LCPD-34915 | am62xx-sk,am62xx_sk-fs | AM62x: op-tee with HW TRNG crashes after Deep Sleep | |
| LCPD-34912 | am62axx_sk-fs,am62axx_sk-hs4,am62axx_sk-hs5,am62axx_sk-se,am62xx-lp-sk,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx-sk,am62xx_sk-fs,am62xx_sk-hs4,am62xx_sk-hs5,am62xx_sk-se | AM62/AM62Ax: DM does not set correct pixel clock | |
| LCPD-34901 | am62xx-sk,am62xx_sk-fs | AM62: Reset button fails to reset AM625-SK-EVM after wakeup from deep sleep | |
| LCPD-34898 | am62xx-sk,am62xx_sk-fs | AM62x: MCU Only mode: Linux console lockup after ~100 suspend resume cycles | |
| LCPD-34835 | am62axx_sk-fs,am62xx-lp-sk,am62xx-sk,beagleplay-gp | am62/am62a: Add CTRL MMR support for DPI signals on negative edge | |
| LCPD-34833 | am62xx-sk,am62xx_sk-fs | AM62: Wi-Fi not functional after 6.1/kirkstone migration | |
| LCPD-34816 | am62xx-sk,am62xx_sk-fs | rtcwake fails after resuming from Deep Sleep | |
| LCPD-34813 | am62xx-sk,am62xx_sk-fs,am62xx_sk-hs4,am62xx_sk-hs5,am62xx_sk-se | SK-AM62B: Flood of tps6598x_interrupt failed to read events | |
| LCPD-34755 | am62axx_sk-fs | am62a: HDMI related crashes | |
| LCPD-34693 | am62axx_sk-fs,am62xx-sk,am62xx_sk-fs | am62: CPSW TCP bidir tests fail | |
| LCPD-34531 | am62axx_sk-fs,am654x-evm | AM62a: eMMC LTP tests failure | |
| LCPD-34397 | am62xx-sk | usb xhci locks up after multiple Linux reboot | |
| LCPD-34360 | am62axx_sk-fs | Display distorted above certain resolution | |
| LCPD-34242 | am62xx-sk,am62xx_sk-fs,am68_sk-fs,j721s2-evm,j7200-evm,j784s4-evm | GPIO_S_FUNC_DIR_IN_ALL_BANK unit test fails | |
| LCPD-34105 | am62axx_sk-fs,am62axx_sk-hs4,am62axx_sk-hs5,am62axx_sk-se,am62xx-lp-sk,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx-sk,am62xx_sk-fs,am62xx_sk-hs4,am62xx_sk-hs5,am62xx_sk-se | convert uboot’s MDIO driver over to use the driver model | |
| LCPD-32706 | am62xx-sk,am62xx_sk-fs | Display: DRM tests fail inconsistently | |
| LCPD-32351 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | MMCSD: HS200 and SDR104 Command Timeout Window Too Small | If the command requires a timeout longer than 700ms, then the MMC host controller command timeout can be disabled (MMCSD_CON[6] MIT=0x1) and a software implementation may be used in its place. |
| LCPD-28742 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | AM62x: Make “Debugging SPL” doc specific to AM62x | |
| LCPD-28491 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | WiLink not functional with fw_devlink option set to on | |
| LCPD-28448 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Wall time does not account for sleep time | |
| LCPD-28105 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Automated test failure - CPSW failure doing runtime pm | |
| LCPD-28104 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Automated test failure - CPSW test is passing invalid parameters to switch-config | |
| LCPD-25563 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Test: AM62: Linux: Add support for MCAN | |
| LCPD-22715 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,j721e-idk-gw,j721s2-evm,j721s2_evm-fs,j7200-evm | i2232: DDR: Controller postpones more than allowed refreshes after frequency change | Workaround 1: Disable dynamic frequency change by programing DFS_ENABLE |
| LCPD-22319 | am62axx_sk-fs,am62xx-sk,am64xx-evm,j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm | OpenSSL performance test data out of bounds |
2.1.5.6. Linux RT Kernel Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-35056 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | ‘Error: “main_cpsw0_qsgmii_phyinit” not defined’ on AM62x | |
| LCPD-35055 | am62xx-lp-sk,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx-sk,am62xx_sk-fs,am62xx_sk-se | ERROR: reserving fdt memory region failed on AM62x | |
| LCPD-35054 | am62xx_lp_sk-fs,am62xx_lp_sk-se | AM62x LP fitImage boot issue with Yocto images |
|
| LCPD-35043 | am62axx_sk-fs | Doc: VPU performance and capabilities shown incorrectly for AM62Ax | |
| LCPD-35042 | am62xx-sk,am62xx_sk-fs,am62xx_sk-hs4,am62xx_sk-hs5,am62xx_sk-se | Linux: AM62x: OSPI NOR Flash read speed is low (~2.5MBPS) | |
| LCPD-35025 | am62xx_sk-fs | Test gap: Implement automated test for Driver suspend resume | |
| LCPD-34991 | am62axx_sk-fs | systemd failure with vmalloc overflow error when using fitimage | |
| LCPD-34978 | am62xx-sk,am62xx_sk-fs | AM62x: High tiny-image cpio file size | |
| LCPD-34916 | am62xx-sk,am62xx_sk-fs | AM62x: op-tee with LOG_LEVEL=2 crashes after Deep Sleep | |
| LCPD-34915 | am62xx-sk,am62xx_sk-fs | AM62x: op-tee with HW TRNG crashes after Deep Sleep | |
| LCPD-34912 | am62axx_sk-fs,am62axx_sk-hs4,am62axx_sk-hs5,am62axx_sk-se,am62xx-lp-sk,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx-sk,am62xx_sk-fs,am62xx_sk-hs4,am62xx_sk-hs5,am62xx_sk-se | AM62/AM62Ax: DM does not set correct pixel clock | |
| LCPD-34901 | am62xx-sk,am62xx_sk-fs | AM62: Reset button fails to reset AM625-SK-EVM after wakeup from deep sleep | |
| LCPD-34898 | am62xx-sk,am62xx_sk-fs | AM62x: MCU Only mode: Linux console lockup after ~100 suspend resume cycles | |
| LCPD-34897 | am62xx_lp_sk-fs | AM62x-LP: USB failures | |
| LCPD-34835 | am62axx_sk-fs,am62xx-lp-sk,am62xx-sk,beagleplay-gp | am62/am62a: Add CTRL MMR support for DPI signals on negative edge | |
| LCPD-34833 | am62xx-sk,am62xx_sk-fs | AM62: Wi-Fi not functional after 6.1/kirkstone migration | |
| LCPD-34816 | am62xx-sk,am62xx_sk-fs | rtcwake fails after resuming from Deep Sleep | |
| LCPD-34813 | am62xx-sk,am62xx_sk-fs,am62xx_sk-hs4,am62xx_sk-hs5,am62xx_sk-se | SK-AM62B: Flood of tps6598x_interrupt failed to read events | |
| LCPD-34755 | am62axx_sk-fs | am62a: HDMI related crashes | |
| LCPD-34693 | am62axx_sk-fs,am62xx-sk,am62xx_sk-fs | am62: CPSW TCP bidir tests fail | |
| LCPD-34531 | am62axx_sk-fs,am654x-evm | AM62a: eMMC LTP tests failure | |
| LCPD-34516 | am62xx-sk,am62xx_sk-fs,j721s2-evm,j7200-evm,j784s4-evm | USBHOST Audio ltp unit test fails | |
| LCPD-34360 | am62axx_sk-fs | Display distorted above certain resolution | |
| LCPD-34242 | am62xx-sk,am62xx_sk-fs,am68_sk-fs,j721s2-evm,j7200-evm,j784s4-evm | GPIO_S_FUNC_DIR_IN_ALL_BANK unit test fails | |
| LCPD-34105 | am62axx_sk-fs,am62axx_sk-hs4,am62axx_sk-hs5,am62axx_sk-se,am62xx-lp-sk,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62xx-sk,am62xx_sk-fs,am62xx_sk-hs4,am62xx_sk-hs5,am62xx_sk-se | convert uboot’s MDIO driver over to use the driver model | |
| LCPD-32706 | am62xx-sk,am62xx_sk-fs | Display: DRM tests fail inconsistently | |
| LCPD-32351 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | MMCSD: HS200 and SDR104 Command Timeout Window Too Small | If the command requires a timeout longer than 700ms, then the MMC host controller command timeout can be disabled (MMCSD_CON[6] MIT=0x1) and a software implementation may be used in its place |
| LCPD-29332 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | LPM Demo not Working on Linux RT | |
| LCPD-28742 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | AM62x: Make “Debugging SPL” doc specific to AM62x | |
| LCPD-28491 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | WiLink not functional with fw_devlink option set to on | |
| LCPD-28448 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Wall time does not account for sleep time | |
| LCPD-28105 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Automated test failure - CPSW failure doing runtime pm | |
| LCPD-28104 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Automated test failure - CPSW test is passing invalid parameters to switch-config | |
| LCPD-25563 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se | Test: AM62: Linux: Add support for MCAN | |
| LCPD-22715 | am62xx-sk,am62xx_sk-fs,am62xx_sk-se,j721e-idk-gw,j721s2-evm,j721s2_evm-fs,j7200-evm | i2232: DDR: Controller postpones more than allowed refreshes after frequency change | Workaround 1: Disable dynamic frequency change by programing DFS_ENABLE = 0 |
| LCPD-22319 | am62axx_sk-fs,am62xx-sk,am64xx-evm,j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm | OpenSSL performance test data out of bounds |
2.1.5.7. Linux SDK Known Issues¶
| Record ID | Platform | Title | Workaround |
|---|---|---|---|
| LCPD-34978 | am62xx-sk,am62xx_sk-fs | AM62x: High tiny-image cpio file size | |
| LCPD-35083 | am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se | AM62: PRU rpmsg samples echo sample FW are not getting installed | MACHINE=am62xx-evm bitbake pru-icss; install the ipk on the targetfs; opkg install pru-icss-rpmsg-echo_6.2.0-r1.0_am62xx_evm.ipk |