2.2. Yocto Layer ConfigurationΒΆ

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>

The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.

Config File Description Supported machines/platforms
processor-sdk-08.06.00-config.txt Processor SDK 08.06.00.42 Release am62xx-evm