2.2. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.
Config File | Description | Supported machines/platforms |
---|---|---|
processor-sdk-08.03.00.19-config.txt | Processor SDK 08.03.00.19 Release | am62xx-evm |